Maker.io main logo

NeoPixel Sprite Weather Display

87

2023-03-21 | By Adafruit Industries

License: See Original Project

Courtesy of Adafuit

Guide by Liz Clark

Overview

With all of the weather API's and display options, it can be ‎overwhelming to decide which approach to take when building a ‎weather display. This project takes the less is more, or smol is more, ‎approach.‎

You can use the tiny yet mighty 5x5 NeoPixel Grid BFF add-on board ‎with a QT Py ESP32-S2 to display the current weather conditions and ‎temperature. The CircuitPython code is using the Open-Meteo API to ‎fetch current weather data. Open-Meteo is a free and open-source ‎weather API that does not require an API key, making it fast to get ‎started with.‎

display_1

The current weather condition is shown with a 5x5 sprite on the ‎NeoPixel Grid. There are sprites for sunny, partly cloudy, clouds, rain, ‎thunderstorms and snow with day and night versions for each.‎

sprite_2

The current temperature scrolls across the display after showing the ‎sprite. The color of the text changes depending on the temperature. ‎Lower temperatures are represented with cooler colors (green, blue, ‎and purple) and higher temperatures are represented with warmer ‎colors (yellow, orange, and red).‎

scroll_3

Prerequisite Guides

Adafruit QT Py ESP32-S2

Adafruit 5x5 NeoPixel Grid BFF

How To Solder Headers

Parts

CircuitPython

CircuitPython is a derivative of MicroPython designed to simplify ‎experimentation and education on low-cost microcontrollers. It ‎makes it easier than ever to get prototyping by requiring no upfront ‎desktop software downloads. Simply copy and edit files on ‎the CIRCUITPY drive to iterate.‎

CircuitPython QuickStart

Follow this step-by-step to quickly get CircuitPython running on your ‎board.‎

Download the latest version of CircuitPython for this board via ‎circuitpython.org

Click the link above to download the latest CircuitPython UF2 file.‎

Save it wherever is convenient for you.‎

download_4

board_5

Plug your board into your computer, using a known-good data-sync ‎cable, directly, or via an adapter if needed.‎

Click the reset button once (highlighted in red above), and then click ‎it again when you see the RGB status LED(s) (highlighted in green ‎above) turn purple (approximately half a second later). Sometimes it ‎helps to think of it as a "slow double-click" of the reset button.‎

For this board, tap reset and wait for the LED to turn purple, and as ‎soon as it turns purple, tap reset again. The second tap needs to ‎happen while the LED is still purple.‎

Once successful, you will see the RGB status LED(s) turn green ‎‎(highlighted in green above). If you see red, try another port, or if ‎you're using an adapter or hub, try without the hub, or different ‎adapter or hub.‎

If double-clicking doesn't work the first time, try again. Sometimes it ‎can take a few tries to get the rhythm right!‎

A lot of people end up using charge-only USB cables and it is very ‎frustrating! Make sure you have a USB cable you know is good for ‎data sync.‎

If after several tries, and verifying your USB cable is data-ready, you ‎still cannot get to the bootloader, it is possible that the bootloader is ‎missing or damaged. Check out the Install UF2 Bootloader page for ‎details on resolving this issue.‎

You will see a new disk drive appear called QTPYS2BOOT.‎

‎Drag the adafruit_circuitpython_etc.uf2 file to QTPYS2BOOT.‎

disk_6‎ ‎‎

 

The BOOT drive will disappear, and a new disk drive ‎called CIRCUITPY will appear.‎

That's it!‎

boot_7

Create Your settings.toml File

If you've worked on WiFi projects with CircuitPython before, you're ‎probably familiar with the secrets.py file. This file is a Python file that ‎is stored on your CIRCUITPY drive that contains all of your secret ‎WiFi information, such as your SSID, SSID password and any API keys ‎for IoT services. ‎

As of CircuitPython 8.0.0-beta.6, there is support for ‎a settings.toml file. Similar to secrets.py, the settings.toml file ‎separates your sensitive information from your main code.py file. ‎

settings.toml File Example

Here is an example on how to format your settings.toml file.‎

Download File

Copy Code
# Comments are supported
CIRCUITPY_WIFI_SSID="guest wifi"
CIRCUITPY_WIFI_PASSWORD="guessable"
CIRCUITPY_WEB_API_PORT=80
CIRCUITPY_WEB_API_PASSWORD="passw0rd"
test_variable="this is a test"
thumbs_up="\U0001f44d"

In a settings.toml file, it's important to keep these factors in mind:‎

  • Strings are wrapped in double quotes; ex: "your-string-here"

  • Integers are not quoted and may be written in decimal with ‎optional sign ( +1, -1, 1000) or hexadecimal (0xabcd)‎

    • Floats, octal (0o567) and binary (0b11011) are not supported

  • Use \u escapes for weird characters, \x and \ooo escapes are not ‎available in .toml files

    • Example: \U0001f44d for thumbs up emoji ‎and \u20ac for € (EUR sign)

  • Unicode emoji, and non-ASCII characters, stand for themselves ‎as long as you're careful to save in "UTF-8 without BOM" format‎ ‎ ‎‎

‎When your settings.toml file is ready, you can save it in your text ‎editor with the .toml extension.‎

settings_8

Accessing Your settings.toml Information ‎in code.py

In your code.py file, you'll need to import the os library to access ‎the settings.toml file. Your settings are accessed with ‎the os.getenv() function. You'll pass your settings entry to the ‎function to import it into the code.py file.‎

Download File

Copy Code
import os

print(os.getenv("test_variable"))

code_9

In the upcoming CircuitPython WiFi examples, you'll see how ‎the settings.toml file is used for connecting to your SSID and ‎accessing your API keys.‎

Code the Weather Display

Once you've finished setting up your QT Py ESP32-S2 with ‎CircuitPython, you can access the code and necessary libraries by ‎downloading the Project Bundle.‎

To do this, click on the Download Project Bundle button in the ‎window below. It will download as a zipped folder.‎

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2022 Liz Clark for Adafruit Industries
# SPDX-License-Identifier: MIT

import os
import ssl
import time
import board
import wifi
import socketpool
import fontio
import neopixel
import simpleio
from adafruit_display_text.bitmap_label import Label
from adafruit_bitmap_font import bitmap_font
from displayio import Bitmap
from rainbowio import colorwheel
from adafruit_ticks import ticks_ms, ticks_add, ticks_diff
import adafruit_requests
from weather_codes import weather_codes

# minimum expected temperature
min_temp = 0
# maximum expected temperature
max_temp = 100
# first daylight hour
daytime_min = 7
# last daylight hour
daytime_max = 17
# latitude
lat = 42.36
# longitude
long = -71.06
# temp unit for API request
temperature_unit = "fahrenheit"
# temp unit for display
temp_unit = "F"

# API request to open-meteo
weather_url = "https://api.open-meteo.com/v1/forecast?"
# pass latitude and longitude
weather_url  = "latitude=%d&longitude=%d&timezone=auto" % (lat, long)
# pass temperature_unit
weather_url  = "&current_weather=true&temperature_unit=%s&windspeed_unit=mph" % temperature_unit

#  connect to SSID
wifi.radio.connect(os.getenv('CIRCUITPY_WIFI_SSID'), os.getenv('CIRCUITPY_WIFI_PASSWORD'))

pool = socketpool.SocketPool(wifi.radio)
requests = adafruit_requests.Session(pool, ssl.create_default_context())

def get_the_weather():
    # make the API request
    response = requests.get(weather_url)
    # packs the response into a JSON
    response_as_json = response.json()
    print()
    # prints the entire JSON
    print(response_as_json)
    print()
    # gets current weather code
    w = int(response_as_json['current_weather']['weathercode'])
    # gets temperature
    t = response_as_json['current_weather']['temperature']
    temp_int = int(t)
    t_c = simpleio.map_range(temp_int, min_temp, max_temp, 255, 0)
    # gets time
    json_time = response_as_json['current_weather']['time']
    n_t = json_time.rsplit("T", 1)[-1]
    n_t = int(n_t[:2])
    return w, t, t_c, n_t

# initial API call
weather, temp, temp_color, new_time = get_the_weather()

# font edit code by Jeff Epler
tom_thumb = bitmap_font.load_font("tom-thumb.pcf", Bitmap)

_glyph_keys = ['bitmap', 'tile_index', 'width', 'height', 'dx', 'dy', 'shift_x', 'shift_y']
def patch_glyph(base, **kw):
    d = {}
    for k in _glyph_keys:
        d[k] = kw.get(k, getattr(base, k))
    return fontio.Glyph(**d)

class PatchedFont:
    def __init__(self, base_font, patches):
        self.base_font = base_font
        self.patches = patches

    def get_glyph(self, glyph):
        g = self.base_font.get_glyph(glyph)
        patch = self.patches.get(glyph)
        if patch is not None:
            #print("patching", repr(chr(glyph)), g)
            g = patch_glyph(g, **patch)
            #print("patched", g)
        return g

    def get_bounding_box(self):
        return self.base_font.get_bounding_box()

font = PatchedFont(tom_thumb,
    {
        32: {'shift_x': 1, 'dx': 0},
        105: {'dx': 0, 'shift_x': 2},
        33: {'dx': 0, 'shift_x': 2},
    })
# thank you Jeff for this PatchedFont() function!

# temperature for scrolling text
label = Label(text="   %s°%s   " % (temp, temp_unit), font=font)
text = label.bitmap

# create 5x5 neopixels
pixels = neopixel.NeoPixel(board.A3, 5*5, brightness=.08, auto_write=False)
# count for pixels when drawing bitmaps
count = 0
# arrays to pack assets from weather_codes helper
# weather condition code
codes = []
# bitmaps for daytime
day_images = []
# bitmaps for nighttime
night_images = []

for i in weather_codes:
    codes.append(i['code'])
    day_images.append(i['day_img'])
    night_images.append(i['night_img'])

# checks if it's day or night based on hour
def day_or_night(t):
    if t in range(daytime_min, daytime_max):
        z = day_images[weather]
    else:
        z = night_images[weather]
    return z

# initial sprite selection
img = day_or_night(new_time)

# draw bitmap sprite
def draw_sprite(c):
    for pixel in img:
        pixels[c] = pixel
        pixels.show()
        c  = 1
        time.sleep(0.001)
    c = 0

# ticks time tracker
clock = ticks_ms()

# 15 minutes in milliseconds
weather_check = 900000

# display current weather sprite & scroll temperature
while True:
    # checks the time
    if ticks_diff(ticks_ms(), clock) > weather_check:
        print("pinging Open-Meteo")
        # make the API request with function
        # return weather ID, temp, temp color & hour
        weather, temp, temp_color, new_time = get_the_weather()
        # checks if it's day or night based on hour
        # & returns day or night version of sprite
        img = day_or_night(new_time)
        label.text = "   %s°%s   " % (temp, temp_unit)
        # reset clock
        clock = ticks_add(clock, weather_check)
    # draw bitmap sprite
    draw_sprite(count)
    # blocking delay to hold the sprite on the display
    time.sleep(5)
    # draw scrolling text
    for v in range(2):
        for i in range(text.width):
            # Scoot the old text left by 1 pixel
            pixels[:20] = pixels[5:]
            # adjust color based on temperature
            color = colorwheel(temp_color)
            # Draw in the next line of text
            for y in range(5):
                # Select black or color depending on the bitmap pixel
                pixels[20 y] = color * text[i,y]
            pixels.show()
            time.sleep(.1)

‎ View on GitHub

Upload the Code and Libraries to the QT Py ‎ESP32-S2‎

After downloading the Project Bundle, plug your QT Py ESP32-S2 ‎into the computer's USB port with a known good USB data power ‎cable. You should see a new flash drive appear in the computer's File ‎Explorer or Finder (depending on your operating system) ‎called CIRCUITPY. Unzip the folder and copy the following items to ‎the QT Py ESP32-S2's CIRCUITPY drive. ‎

  • lib folder

  • code.py

  • weather_codes.py

Your QT Py ESP32-S2 CIRCUITPY drive should look like this after ‎copying the lib folder, weather_codes.py file and the code.py file.‎

qtpy_10

Add Your settings.toml File

As of CircuitPython 8.0.0, there is support for Environment Variables. ‎These Environmental Variables are stored in a settings.toml file. ‎Similar to secrets.py, the settings.toml file separates your sensitive ‎information from your main code.py file. ‎Add your settings.toml file as described in the Create Your ‎settings.toml File page earlier in this guide. You'll need to include ‎your CIRCUITPY_WIFI_SSID and CIRCUITPY_WIFI_PASSWORD.‎

Download File

Copy Code
CIRCUITPY_WIFI_SSID = "your-ssid-here"
CIRCUITPY_WIFI_PASSWORD = "your-ssid-password-here"

The weather_codes.py File

The weather_codes.py file is a helper file that contains the sprite ‎information and assigns the sprites to the weather condition codes ‎that will be returned from Open-Meteo. ‎

The file begins by defining RGB color values that will be used to ‎create the sprites.‎

Download File

Copy Code
y = (255, 125, 0)
o = (0, 0, 0)
a = (0, 75, 125)
w = (255, 255, 255)
v = (127, 0, 255)
b = (0, 0, 255)
z = (0, 0, 25)
g = (25, 25, 25)

The sprites are defined as five-by-five arrays. In total, there are eleven ‎sprite arrays.‎

Download File

Copy Code
sun_bitmap = [
    y,a,y,a,y,
    a,y,y,y,a,
    y,y,y,y,y,
    a,y,y,y,a,
    y,a,y,a,y,
]
cloud_bitmap = [
    a,a,a,w,a,
    a,w,w,w,a,
    a,w,w,w,a,
    a,a,w,w,a,
    a,a,a,w,a,
]
# etc

weather_codes is a dictionary that contains the weather codes and the ‎associated daytime and nighttime sprite. The codes are WMO Codes ‎as defined by NOAA. There are 100 possible codes, ranging ‎from 0 to 99. In code.py, these weather codes are used as indexes to ‎access the appropriate sprite.‎

Download File

Copy Code
weather_codes = [
{"code" : 0, "day_img" : sun_bitmap, "night_img" : night_bitmap},
{"code" : 1, "day_img" : sun_bitmap, "night_img" : night_bitmap},
{"code" : 2, "day_img" : sun_bitmap, "night_img" : night_bitmap},
  ...
{"code" : 99, "day_img" : thunder_bitmap, "night_img" : nightThunder_bitmap}
]

How the CircuitPython Code Works

At the top of the code are variables that can be edited to customize ‎your code.py file for your needs. min_temp and max_temp are used in ‎the map_range() function that determine the color of the temperature ‎text. ‎The min_temp number can be negative if you are in a colder ‎climate. daytime_min and daytime_max are used to determine the hours ‎in which a daytime sprite is shown versus a nighttime ‎sprite. lat and long hold your location's latitude and longitude. ‎Finally, temperature_unit and temp_unit hold either Fahrenheit or ‎Celsius. ‎

Download File

Copy Code
# minimum expected temperature
min_temp = 0
# maximum expected temperature
max_temp = 100
# first daylight hour
daytime_min = 7
# last daylight hour
daytime_max = 17
# latitude
lat = 42.36
# longitude
long = -71.06
# temp unit for API request
temperature_unit = "fahrenheit"
# temp unit for display
temp_unit = "F"

The Request URL

The API request to Open-Meteo is passed as a ‎URL. lat, long and temperature_unit are passed to the URL ‎string. Open-Meteo has documentation with more information on ‎building a URL for an API request.‎

Download File

Copy Code
# API request to open-meteo
weather_url = "https://api.open-meteo.com/v1/forecast?"
# pass latitude and longitude
weather_url  = "latitude=%d&longitude=%d&timezone=auto" % (lat, long)
# pass temperature_unit
weather_url  = "¤t_weather=true&temperature_unit=%s&windspeed_unit=mph" % temperature_unit

Get the Weather

The function get_the_weather() is used to make the API request and ‎return values for the current weather condition, temperature, the ‎color mapped to the current temperature and the current time.‎

Download File

Copy Code
def get_the_weather():
    # make the API request
    response = requests.get(weather_url)
    # packs the response into a JSON
    response_as_json = response.json()
    print()
    # prints the entire JSON
    print(response_as_json)
    print()
    # gets current weather code
    w = int(response_as_json['current_weather']['weathercode'])
    # gets temperature
    t = response_as_json['current_weather']['temperature']
    temp_int = int(t)
    t_c = simpleio.map_range(temp_int, min_temp, max_temp, 255, 0)
    # gets time
    json_time = response_as_json['current_weather']['time']
    n_t = json_time.rsplit("T", 1)[-1]
    n_t = int(n_t[:2])
    return w, t, t_c, n_t

# initial API call
weather, temp, temp_color, new_time = get_the_weather()

Import the Sprites

A for statement packs the list entries from weather_codes into three ‎different arrays: codes for the weather code numbers, day_images for ‎the daytime sprites and night_images for the nighttime sprites.‎

Download File

Copy Code
for i in weather_codes:
    codes.append(i['code'])
    day_images.append(i['day_img'])
    night_images.append(i['night_img'])

Day or Night?‎

The function day_or_night() determines which sprite is shown based ‎on the weather condition and time of day.‎

Download File

Copy Code
# checks if it's day or night based on hour
def day_or_night(t):
    if t in range(daytime_min, daytime_max):
        z = day_images[weather]
    else:
        z = night_images[weather]
    return z

# initial sprite selection
img = day_or_night(new_time)

Draw the Sprite

The draw_sprite() function draws the weather sprite to the 5x5 grid of ‎NeoPixels.‎

Download File

Copy Code
# draw bitmap sprite
def draw_sprite(c):
    for pixel in img:
        pixels[c] = pixel
        pixels.show()
        c  = 1
        time.sleep(0.001)
    c = 0

Tick, tick, tick...‎

For tracking time, the ticks library is used. ticks manages time in ‎milliseconds, rather than seconds like in time.monotonic(). The API ‎will be called every fifteen minutes, or every 900000 milliseconds.‎

Download File

Copy Code
# ticks time tracker
clock = ticks_ms()

# 15 minutes in milliseconds
weather_check = 900000

The Loop

In the loop, the API is called every 15 minutes. The sprite and scrolling ‎temperature text is updated depending on the data that is returned.‎

Download File

Copy Code
# checks the time
    if ticks_diff(ticks_ms(), clock) > weather_check:
        print("pinging Open-Meteo")
        # make the API request with function
        # return weather ID, temp, temp color & hour
        weather, temp, temp_color, new_time = get_the_weather()
        # checks if it's day or night based on hour
        # & returns day or night version of sprite
        img = day_or_night(new_time)
        label.text = "   %s°%s   " % (temp, temp_unit)
        # reset clock
        clock = ticks_add(clock, weather_check)

Scroll the Weather

The core functionality of the display loops continuously. The sprite is ‎drawn to the 5x5 grid and is shown for five seconds. Then, the ‎temperature text is scrolled across the display. Once the text finishes ‎scrolling, the process begins again by drawing the sprite.‎

Download File

Copy Code
# draw bitmap sprite
    draw_sprite(count)
    # blocking delay to hold the sprite on the display
    time.sleep(5)
    # draw scrolling text
    for v in range(2):
        for i in range(text.width):
            # Scoot the old text left by 1 pixel
            pixels[:20] = pixels[5:]
            # adjust color based on temperature
            color = colorwheel(temp_color)
            # Draw in the next line of text
            for y in range(5):
                # Select black or color depending on the bitmap pixel
                pixels[20 y] = color * text[i,y]
            pixels.show()
            time.sleep(.1)

3D Printing‎

3dprinting_11

The weather display may be assembled with 3D printed parts, ‎described below. The case has two parts: a cloud-shaped lid and a ‎case to house the boards. Both parts print without supports.‎

The STL files can be downloaded directly here, from Thingiverse or ‎from Printables.‎

‎5x5WeatherDisplaySTLfiles.zip‎

Thingiverse download

Printables download

The main case has cutouts for the QT Py USB C port and the reset ‎and boot buttons on the back. It has tiny holes to mount the QT Py ‎header pins to keep the boards properly secured in the case.‎

case_12

The cloud lid has an opening for the 5x5 NeoPixel Grid. Its snap fits ‎onto the main case.‎

lid_13

Assembly

assembly_14

Solder socket headers to the 5x5 NeoPixel Grid BFF and solder plug ‎headers to the QT Py ESP32-S2.‎

solder_15

Plug the QT Py ESP32-S2 into the NeoPixel Grid BFF. Make sure that ‎the QT Py USB port is oriented properly by referencing the USB ‎labeling and arrow on the back of the BFF.‎

plug_16

Insert the boards into the main case by lining up the QT Py header ‎pins with the header pin slots in the bottom of the case.‎

insert_17

The boards should be situated in the center of the case with the QT ‎Py USB port accessible via the side cutout.‎

boards_18

Close the case with the cloud lid. Make sure that the 5x5 NeoPixel ‎Grid is centered in the cloud's cutout. ‎

That completes the assembly!‎

close_19

Usage

display_20

To use the weather display, plug the QT Py ESP32-S2 into a USB-C ‎cable to power it. After connecting to your SSID / WiFi, the QT Py will ‎make a request to the Open-Meteo API and display the current ‎weather condition sprite and the current temperature.‎

As the incoming data changes from the API, the displayed sprite and ‎temperature reading will update. Additionally, the sprite will change ‎depending on the time of day as each sprite has a daytime and ‎nighttime version.‎

Update Your Latitude and Longitude

Open-Meteo uses latitude and longitude to pinpoint your location's ‎weather. You can update these values to match your location at the ‎top of the code.py file.‎

open_21

You can use Google Maps to find the latitude and longitude of your ‎location. Search your location and then right-click on the map. The ‎latitude and longitude will appear in a pop-up window on the screen.‎

map_22

Customize the API Request

You can customize the Open-Meteo API request by changing the ‎parameters in the URL. Open-Meteo has documentation and a URL ‎builder to track various pieces of weather data.‎

data_23

מק"ט יצרן # 5646
ADAFRUIT 5X5 NEOPIXEL GRID BFF A
Adafruit Industries LLC
מק"ט יצרן # 4154
CONN HEADER VERT 36P 2.54MM 10PK
Adafruit Industries LLC
מק"ט יצרן # 4160
20PIN FEMALE HEADER RAINBOW 5PK
Adafruit Industries LLC
מק"ט יצרן # 5153
CABLE A PLUG TO C PLUG 3.28'
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.