Maker.io main logo

No-Code, No-Solder Monitoring For Perfect Bread

172

2025-05-27 | By Adafruit Industries

License: See Original Project Humidity Temperature Adafruit Feather STEMMA

Courtesy of Adafruit

Guide by Ben Everard

Overview

sensors_1

Taking regular readings with a sensor and storing the results are a common task for ‎microcontrollers, but it usually requires some programming and soldering. However, ‎thanks to WipperSnapper Offline and STEMMA QT, we can get everything up and running ‎without programming or soldering.‎

In this project, you create a temperature and humidity monitor that can record values ‎as bread dough rises (the process known as proofing). However, you can use this for any ‎situation where you want to record the temperature and humidity over time. It's not just ‎temperature & humidity; you can connect a wide variety of sensors to record other things. ‎There's a list of supported hardware at https://learn.adafruit.com/no-code-offline-data-‎logging-with-wippersnapper/supported-hardware.‎

Parts

The SHT45 sensor is available with and without a PTFE filter. In this case, I recommend the ‎version with the filter as it will help keep contaminants out of the sensor.‎

WipperSnapper offline can work with any MicroSD card under 32 GB. If you don't already ‎have one, I recommend the following:‎

  • SD/MicroSD Memory Card (8 GB SDHC)‎

Optional components

The above components will let you record data at regular intervals but won't keep track of ‎the time that readings were taken. If you want to record the actual time of readings, then ‎you'll need the real-time clock (RTC) below and another STEMMA QT cable.‎

You might also need:‎

You'll also need a way of connecting the RP2040 Adalogger to a computer and a power ‎supply. The RP2040 Adalogger has a USB-C port, so depending on your computer, you'll ‎need one of the following if you don't already have them.‎

You'll also need a way of reading the data off the MicroSD card. Many laptops have SD cards ‎built in, though you might need a MicroSD to SD adapter, which is included with the ‎MicroSD card above. If you don't have one already, you'll need something like the following ‎‎(which needs a USB-C port)‎.

Configure the MicroSD Card

A MicroSD card is required to be inserted into your board for offline mode. This applies ‎even for cases where data is only intended to log to USB serial. ‎

Which MicroSD Card Should I Get?‎

Any MicroSD Card with a capacity of less than 32GB should be good. When purchasing ‎the card, be aware that some cheap cards are "fakes" and may cause headaches. ‎The MicroSD cards in the Adafruit shop are guaranteed to work.‎

You will also need a way to read the logged data from the MicroSD Card. To do this, you will ‎need an external SD Card reader to plug into your computer.‎

Formatting under Windows/Mac

If you bought a MicroSD card, chances are it's already pre-formatted with a FAT filesystem. ‎However, you may have problems with how the factory formats the card, or if it's an old ‎card, it needs to be reformatted. The Arduino SD library used in the Wippersnapper ‎software supports both FAT16 and FAT32 filesystems.‎

If you have a MicroSD card with a very small capacity, say 8-32 Megabytes you might find it ‎is formatted FAT12 which isn't supported by Offline Mode. You'll have to reformat these ‎cards.‎

Either way, it's always a good idea to format the card before using it, even if it's ‎new! Note that formatting will erase the card so save anything you want first.‎

Before proceeding with the guide, we strongly recommend you use the official SD card ‎formatted utility to format your MicroSD Card. This tool is written by the SD Association, ‎and it solves many problems that come with bad formatting. The link is below:‎

Download the Official SD Card Formatter for Windows/Mac

Insert the MicroSD Card

The Feather RP2040 Adalogger's MicroSD card slot is located at the end of the board, ‎directly behind the STEMMA QT port. After formatting the MicroSD card, insert the card into ‎the MicroSD card slot.‎

sensors_adafruit_products_5980-05

Connecting the Hardware

Connect the RP2040 Adalogger to the DS3231 clock (if you are using one), and then the ‎other port on the DS3231 to the SHT45 using STEMMA QT Cables. You can use either port ‎on the DS3231 and SHT45 for input or output. The circuit will work whether you have the ‎SHT45 or the DS3231 first in the chain. However, I found it a bit easier to position the ‎hardware for accurate temperature monitoring if the SHT45 is last in the chain.‎

The cables should push snugly into place. they only go in one way around, so if they're not ‎going in, try rotating them.‎

The circuit should look like this if you have a clock:‎

circuit_2

Or this if you don't:‎

circuit_3

Protecting the hardware

In this project, we're working with food and electronics, and we want to be a bit careful to ‎keep the two separate. At the same time, we need the sensor to be exposed so that it can ‎fully sense the environment. The best setup here depends on what your bread proofing ‎setup looks like. ‎

In many cases, you should be fine placing your electronics next to the bowl or basket you're ‎proofing your dough in.‎

If you're proofing dough on a metal baking sheet, be careful to place the electronics in ‎contact with anything conductive.‎

With everything together, you're now ready to install the firmware.‎

Install WipperSnapper Offline Firmware

I have a compatible board already running WipperSnapper but want to try out Offline Mode

If you wish to try Offline Mode and have a device running WipperSnapper, you must ‎download the WipperSnapper Offline Mode beta firmware and install it on your device. This ‎will replace the existing WipperSnapper (online) firmware on your board. ‎

WipperSnapper (offline) is not permanently installed on your board, you can switch back to ‎WipperSnapper (online) at any time.‎

I have a compatible board running an Arduino Sketch but want to try out Offline Mode

Installing WipperSnapper Offline will completely erase the Arduino sketch that is ‎currently running on your board. Before installing WipperSnapper Offline, ensure your ‎computer has a backup of the sketch running on the Arduino.‎

WipperSnapper is not permanently installed on your board, you can switch back to Arduino ‎at any time.‎

I have a compatible board running CircuitPython but want to try out Offline Mode

WipperSnapper is a different application from CircuitPython. Because of this, installing ‎WipperSnapper will completely erase the CircuitPython installation and all files on your ‎board. WipperSnapper is not permanently installed on your board, you can switch back to ‎CircuitPython at any time.‎

Before installing WipperSnapper, verify and back up your CircuitPython Installation by ‎following the instructions below:‎

When you plug a CircuitPython board into your computer, your computer will see the ‎board's flash memory as a USB flash drive where files can be stored. When the board is ‎running CircuitPython, you'll see the CIRCUITPY drive.‎

drive_3a

If you see the CIRCUITPY drive appear as a USB flash drive:‎

  • Copy all files to a safe location on your computer, like your desktop. code.py is the ‎most important file on this drive as it contains your CircuitPython code.‎

If you do not see the CIRCUITPY drive and instead see a drive ‎named boardnameBOOT (or similar such as one of these drive names):‎

  • Locate the reset button on your board. It's a small, black button, and on most of the ‎boards, it will be the only button available. It is typically labeled RESET or RST on the ‎board.‎

  • Tap this button once

  • If the drive changes from boardnameBOOT to CIRCUITPY, follow the instructions ‎above to back up its contents

  • If it stays as boardnameBOOT, the board does not have CircuitPython installed. You ‎may proceed to the next step.‎

Once you've backed up your CIRCUITPY drive, proceed to the next steps to download ‎and install the WipperSnapper firmware.‎

Download WipperSnapper Firmware with Offline Mode

WipperSnapper will ultimately be released as a single firmware file that supports ‎online and offline modes. But, for now, WipperSnapper is split into two different ‎files/firmware:‎

To download WipperSnapper with Offline Mode, navigate to the releases page for the ‎WipperSnapper Arduino project.‎

From the releases page, click the release for the latest version of the offline firmware. The ‎offline firmware will have "offline" in the title.‎

page_4

Under Assets, select the UF2 file for the Adafruit RP2040 FeatherWing. It should look ‎something like wippersnapper.feather_rp2040_adalogger_tinyusb.1.0.0-offline-‎beta.x.uf2.‎

Save the file to your computer's desktop.‎

save_5

Install WipperSnapper Offline Firmware ‎

install_6

To enter the bootloader, hold down the BOOT/BOOTSEL button (highlighted in red above), ‎and while continuing to hold it (don't let go!), press and release the reset ‎button (highlighted in red or blue above). Continue to hold the BOOT/BOOTSEL button ‎until the RPI-RP2 drive appears!‎

If the drive does not appear, release all the buttons, and then repeat the process above.‎

You can also start with your board unplugged from USB, press, and hold the BOOTSEL ‎button (highlighted in red above), continue to hold it while plugging it into USB, and wait for ‎the drive to appear before releasing the button.‎

A lot of people end up using charge-only USB cables and it is very frustrating! Make sure ‎you have a USB cable you know is good for data sync.‎

You will see a new disk drive appear called RPI-RP2.‎

Drag the wippersnapper.feather_rp2040_adalogger_tinyusb.1.0.0-offline-beta.x.uf2 file ‎to RPI-RP2.‎

drive_7

drive_8

The RPI-RP2 drive will disappear, and a new disk drive called WIPPER will appear.‎

That's it, you're done! :)‎

disk_9

Flash Resetting UF2‎

If your board ever gets into a really weird state and the WIPPER doesn't show up as a disk ‎drive after installing WipperSnapper, try loading this 'nuke' UF2 to RPI-RP2. which will do a ‎‎'deep clean' on your Flash Memory. You will lose all the files on the board, but at least ‎you'll be able to revive it!‎

After loading this UF2, follow the steps above to re-install WipperSnapper.‎

Download Flash "Nuke"/Reset UF2 file for RP2 based boards

If not using the Raspberry Pi Pico (or 2 / W) then find your board's learn guide for further ‎details on resetting/erasing the flash memory and restoring the UF2 bootloader.‎

Setting the Configuration

Now that you have the hardware connected and the firmware installed, you need to ‎configure WipperSnapper so that it knows what hardware is connected and how frequently ‎you want to take readings. You do this with the config.json file.‎

Connect the Adafruit Feather RP2040 Adalogger to your computer via USB, and you should ‎see a new drive appear called WIPPER. You need to save the configuration in a text file ‎called config.json in that directory.‎

Using a text editor, copy the text to the editor and save the file onto the WIPPER drive.‎

The contents of the file should be one of the following:‎

If you have the DS3231 real-time clock attached, then it should be:‎

Download File

Copy Code
{
    "exportedFromDevice": {
        "referenceVoltage": 3.3,
        "totalGPIOPins": 18,
        "totalAnalogPins": 4,
        "sd_cs_pin": 23,
        "statusLEDBrightness": 0.5,
        "rtc": "DS3231"
    },
    "components": [
        {
            "name": "SHT45 Sensor",
            "componentAPI": "i2c",
            "i2cDeviceName": "sht45",
            "period": 15,
            "i2cDeviceAddress": "0x44",
            "i2cDeviceSensorTypes": [
                {"type": "relative-humidity"},
                {"type": "ambient-temp"},
                {"type": "ambient-temp-fahrenheit"}
            ]
        }
    ]
}

If you aren't using the real-time clock, it should be:‎

Download File

Copy Code
{
    "exportedFromDevice": {
        "referenceVoltage": 3.3,
        "totalGPIOPins": 18,
        "totalAnalogPins": 4,
        "sd_cs_pin": 23,
        "statusLEDBrightness": 0.5
    },
    "components": [
        {
            "name": "sht45",
            "componentAPI": "i2c",
            "i2cDeviceName": "sht45",
            "period": 15,
            "i2cDeviceAddress": "0x44",
            "i2cDeviceSensorTypes": [
                {"type": "relative-humidity"},
                {"type": "ambient-temp"},
                {"type": "ambient-temp-fahrenheit"}
            ]
        }
    ]
}

Once that's saved to the device, you can reset the device (either by pressing the reset button ‎or by plugging it in and then unplugging it), and it will start recording data. The status light ‎on the Adafruit RP2040 Adalogger should flash every 15 seconds when it takes a reading.‎

You now have a working temperature logger. Next, to look at the data that is being stored.‎

Analysing Your Data

WipperSnapper saves data in a format called JSON and stores it on the SD card. To read the ‎data, unplug the device to power it down, then take out the MicroSD card and plug it into ‎your computer. You should see one or more files with names ending .log.‎

If you have a real-time clock module attached, the files should contain something like this:‎

Download File

Copy Code
{"i2c_address":"0x44","timestamp":1742312411,"value":66.88853,"si_unit":"%"}
{"i2c_address":"0x44","timestamp":1742312411,"value":18.89563,"si_unit":"C"}
{"i2c_address":"0x44","timestamp":1742312411,"value":66.00252,"si_unit":"F"}
{"i2c_address":"0x44","timestamp":1742312426,"value":66.76837,"si_unit":"%"}
{"i2c_address":"0x44","timestamp":1742312426,"value":18.89029,"si_unit":"C"}
{"i2c_address":"0x44","timestamp":1742312426,"value":66.01213,"si_unit":"F"}
{"i2c_address":"0x44","timestamp":1742312441,"value":66.97055,"si_unit":"%"}
{"i2c_address":"0x44","timestamp":1742312441,"value":18.86625,"si_unit":"C"}
{"i2c_address":"0x44","timestamp":1742312441,"value":66.03136,"si_unit":"F"}
{"i2c_address":"0x44","timestamp":1742312456,"value":66.97055,"si_unit":"%"}
{"i2c_address":"0x44","timestamp":1742312456,"value":18.88228,"si_unit":"C"}
{"i2c_address":"0x44","timestamp":1742312456,"value":65.95926,"si_unit":"F"}

‎While if you don't have a clock module, they should look like this:‎

Download File

Copy Code
{"i2c_address":"0x44","timestamp":0,"value":63.74326,"si_unit":"%"}
{"i2c_address":"0x44","timestamp":1,"value":19.98245,"si_unit":"C"}
{"i2c_address":"0x44","timestamp":2,"value":67.97803,"si_unit":"F"}
{"i2c_address":"0x44","timestamp":3,"value":65.10895,"si_unit":"%"}
{"i2c_address":"0x44","timestamp":4,"value":19.40032,"si_unit":"C"}
{"i2c_address":"0x44","timestamp":5,"value":66.94461,"si_unit":"F"}
{"i2c_address":"0x44","timestamp":6,"value":65.95392,"si_unit":"%"}
{"i2c_address":"0x44","timestamp":7,"value":19.13062,"si_unit":"C"}
{"i2c_address":"0x44","timestamp":8,"value":66.47356,"si_unit":"F"}
{"i2c_address":"0x44","timestamp":9,"value":66.48989,"si_unit":"%"}
{"i2c_address":"0x44","timestamp":10,"value":18.92767,"si_unit":"C"}
{"i2c_address":"0x44","timestamp":11,"value":66.10345,"si_unit":"F"}
{"i2c_address":"0x44","timestamp":12,"value":66.97437,"si_unit":"%"}
{"i2c_address":"0x44","timestamp":13,"value":18.78881,"si_unit":"C"}
{"i2c_address":"0x44","timestamp":14,"value":65.79103,"si_unit":"F"}

The difference is that with a clock, each reading is tagged with the timestamp (this is the ‎number of seconds since January 1st, 1970), while if you don't, each reading is numbered ‎sequentially.‎

Converting to CSV

You can read the JSON files, but if you want to analyse the data in a spreadsheet, you'll ‎need the data in another form. Now let's convert it into CSV (comma separated values), a ‎common file type for data like this.‎

Head to https://konbert.com/convert/jsonl/to/csv and upload the log file. Click Convert and ‎then Download to save your data. The downloaded file can then be read in by most popular ‎spreadsheets.‎

We'll now look at how to generate useful charts with this using Google Sheets, and the ‎process is very similar in LibreOffice Calc or MS Excel.‎

Loading into Google Sheets

Head to https://sheets.google.com and create a new sheet (you might need to sign up for ‎an account if you don't already have one). Then go to File > Import and load the CSV file that ‎you downloaded in the previous step.‎

If you are using a real time clock, we can convert the time into a more usual date and time ‎format. If you're not using the clock, you can skip this step.‎

Create a new column that will hold your date. In the top data cell in that column, enter the ‎formula

‎=EPOCHDATE(B2)‎

and this should convert the timestamp (in cell B2) into a human-readable date. You can ‎copy and paste this down the whole column and it will give you the correct date and time for ‎each reading.

sheets_10

You also need to break out the temperature and humidity data into their own columns so ‎that the chart will plot them correctly. Create a new column called temp and add the ‎formula:‎

‎=if(E2="C", D2, "")‎

or

‎=if(E2="F", D2, "")‎

Depending on if you want the temperature in Celsius or Fahrenheit.‎

Then create a new column called humidity and add the formula

‎=if(E3="%", D3, "")‎

Both of these new formulas should be copied and pasted down the column.‎

sheets_11

We're now ready to create the chart. Highlight the data and then go to Insert > Chart. This ‎should create a scrambled chart that we need to change some settings on. In the box on the ‎right-hand side select the following (and remove any additional entries in the X axis and ‎Series):‎

  • Chart Type: Line chart

  • X axis: date or timestamp if not using the real time clock

  • Series: temp and humidity

Your chart should now be displaying temperature and humidity against time. You can set ‎the title and other parts of its appearance in the Customize section should you wish.‎

sheets_12

We've used this to monitor the temperature and humidity of our bread proofing. There are ‎many different opinions on what the best temperature and humidity may be. Do you want a ‎slow steady rise, or do you need the bread to be ready quickly? By monitoring the values, ‎you can see how they affect the bread and decide what is the best option for what you want ‎to bake.

מק"ט יצרן # 5980
FEATHER RP2040 ADALOGGER
Adafruit Industries LLC
מק"ט יצרן # 6174
ADAFRUIT SENSIRION SHT45 PRECISI
Adafruit Industries LLC
מק"ט יצרן # 4399
STEMMA QWIIC JST SH CABLE 50MM
Adafruit Industries LLC
מק"ט יצרן # 5188
STEMMA QT DS3231 PRECISION RTC
Adafruit Industries LLC
מק"ט יצרן # 4474
CABLE A PLUG TO C PLUG 3'
Adafruit Industries LLC
מק"ט יצרן # 4199
CABLE C PLUG TO C PLUG 3.28'
Adafruit Industries LLC
מק"ט יצרן # 5212
USB TYPE C MICROSD CARD READER/W
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.