Maker.io main logo

PixelDust Digital Sand Demos for Arcada

85

2024-10-09 | By Adafruit Industries

License: See Original Project LCD / TFT Adafruit Feather Grove STEMMA

Courtesy of Adafruit

Guide by Lady Ada

Overview

PyGamer and PyBadge have built in accelerometers - which you can ‎use in your games or demos to make nifty motion-activated effects. ‎In this mini guide we'll show you some examples ‎of PaintYourDragon's PixelDust library but for Arcada boards.

Supported Hardware

You'll need a board with Adafruit Arcada support + an accelerometer ‎such as...‎

Text editor powered by tinymce.‎

Start by following your board's guide on installing Arduino IDE, and ‎support for the board you have. Then install the Adafruit Arcada ‎libraries (there's a lot of em!)‎

Also install the Adafruit PixelDust library

sensors_ezgif-1-4b7d80e51b58

Compilation Settings

As you get to a few thousand particles, you'll want to speed up your ‎board as much as possible. Compile with ultra-speed settings such ‎as 200MHz overclock, -Ofast optimizations, and Cache enabled.‎

settings_1

Runtime Settings

There's not a lot of things you can adjust but here's a few common ‎ones:‎

#define CHUNKY_SAND‎

If this is at the top of the code, it will make each particle a 2x2 pixel ‎rather than a single pixel. this makes it look a little better, but you ‎can't fit as many particles on the screen.‎

#define N_FLAKES 2000

How many particles to simulate. More look cooler but too many and ‎it slows down! 1000-2000 seems to be a good number, especially ‎with CHUNKY_SAND turned on.‎

On this line in the loop:‎

pixeldust->iterate(xx 3000.0, yy 3000.0, zz * 3000.0);‎

The multiplier affects the 'gravity' of the pixels. Larger numbers will ‎drag the pixels down faster, smaller numbers will make the pixels ‎float a little more.‎

Snow Demo

Start with the pixeldust_demos->pixeldust_snow example, it’s the ‎simplest demo - each pixel is the same white color.‎

demo_2

Upload and enjoy!‎

upload_3

Sand Demo

This demo builds on the snow version to add speckled yellow colors ‎to each particle, to create a sand-effect!‎

sand_4

You can add color to each pixel by creating a new array of 16-bit ‎colors as we do in this demo with the creation of uint16_t ‎‎*flake_colors; and then later flake_colors = (uint16_t )malloc(N_FLAKES 2).‎

Then you can assign the colors, we'll use an HSV picker to find a hue ‎we think is sandy...‎

colors_5

And randomly assign brightness/saturations so we get a range of ‎sandy colors!‎

‎Download File

Copy Code
  // randomize colors
  for (int i=0; i< N_FLAKES; i++) {
    flake_colors[i] = 
      __builtin_bswap16(arcada.ColorHSV565(40, // Hue (sandy)
                                           random(50, 100),  // saturation
                                           random(50, 100))); // brightness
  }

Note we use __builtin_bswap16 on each color word. That's because we ‎later use DMA to write out all the pixels and we need to have the ‎high/low bytes of color swapped in order for it to run as fast as ‎possible (it’s a weird effect of TFT DMA on Arduino)‎.

Later on, when we draw the pixels, we'll look up the corresponding ‎color before we draw the color to our framebuffer:‎

‎Download File

Copy Code
  for(int i=0; i<N_FLAKES; i++) {
    pixeldust->getPosition(i, &x, &y);
    //Serial.printf("(%d, %d) -> %d\n", x, y, x * width + y);
    uint16_t flakeColor = flake_colors[i];
#ifdef CHUNKY_SAND
    framebuffer[2*y * width + 2*x] = flakeColor;
    framebuffer[2*y * width + 2*x+1] = flakeColor;
    framebuffer[(2*y+1) * width + 2*x] = flakeColor;
    framebuffer[(2*y+1) * width + 2*x + 1] = flakeColor;
#else
    framebuffer[y * width + x] = flakeColor;
#endif
  }

Logo Demo

Finally, the most advanced of the demos adds a logo 'obstacle' both ‎as an image and a 'mask' that tells PixelDust where not to let pixels ‎go. This makes for lovely effects as particles slide around.‎

sensors_ezgif-1-247db949ce6f

For the logo, which is 8-bit grayscale and stored in the header, you ‎can use a tool like this that will take an image and convert it into a ‎header file.‎

Like the sand demo we will store a color for each particle. Except this ‎time instead of randomly placing them on the display, they are put ‎into boxes along the bottom of the screen:‎

Download File

Copy Code
  // Set up initial sand coordinates, in 8x8 blocks
  int n = 0;
  for(int i=0; i<N_COLORS; i++) {
    int xx = i * play_width / N_COLORS;
    int yy =  play_height - BOX_HEIGHT;
    for(int y=0; y<BOX_HEIGHT; y++) {
      for(int x=0; x<play_width / N_COLORS; x++) {
        //Serial.printf("#%d -> (%d, %d)\n", n,  xx + x, yy + y);
        pixeldust->setPosition(n++, xx + x, yy + y);
      }
    }
  }

Since the chunks of particle divide up into 8 colors, we don’t have to ‎store the color of each one, we know that the index of the particle, ‎divided by 8, gives the color index. Notes we have to bswap16 the color ‎here like we did before.‎

‎Download File

Copy Code
  colors[0] = arcada.color565(40 , 40, 40);   // Dark Gray
  colors[1] = arcada.color565(120, 79, 23);   // Brown
  colors[2] = arcada.color565(228,  3,  3);   // Red
  colors[3] = arcada.color565(255,140,  0);   // Orange
  colors[4] = arcada.color565(255,237,  0);   // Yellow
  colors[5] = arcada.color565(  0,128, 38);   // Green
  colors[6] = arcada.color565(  0, 77,255);   // Blue
  colors[7] = arcada.color565(117,  7,135); // Purple
  for (int i=0; i<N_COLORS; i++) {
    colors[i] = __builtin_bswap16(colors[i]);  // we swap the colors here to speed up DMA
  }

Then before we draw all the particles, we also have to draw the logo:‎

Download File

Copy Code
  int logo_origin_x = (width  - 2*LOGO_WIDTH ) / 2;
  int logo_origin_y = (height - 2*LOGO_HEIGHT ) / 2;
  // Draw the logo atop the background...
  for(int yl=0; yl<LOGO_HEIGHT; yl++) {
    for(int xl=0; xl<LOGO_WIDTH; xl++) {
      uint16_t c = 
         __builtin_bswap16(arcada.color565(logo_gray[yl][xl], logo_gray[yl][xl], logo_gray[yl][xl]));
      x = logo_origin_x + 2*xl;
      y = logo_origin_y + 2*yl; 
      
      framebuffer[y * width + x] = c;
      framebuffer[y * width + x+1] = c;
      framebuffer[(y+1) * width + x] = c;
      framebuffer[(y+1) * width + x+1] = c;
    }
  }

Text editor powered by tinymce.‎

מק"ט יצרן # 4277
PYGAMER STARTER KIT
Adafruit Industries LLC
מק"ט יצרן # 4242
PYGAMER FOR MAKECODE ARCADE, CIR
Adafruit Industries LLC
מק"ט יצרן # 4200
ADAFRUIT PYBADGE FEATHER
Adafruit Industries LLC
מק"ט יצרן # 592
CABLE A PLUG TO MCR B PLUG 3'
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.