Maker.io main logo

Plant Monitoring with Enviro Grow

238

2023-04-20 | By Pimoroni

License: See Original Project Raspberry Pi SBC

Courtesy of Pimoroni

Guide by Pimoroni

Enviro Grow is a clever little Raspberry Pi Pico W- powered data-logging board ‎which will let you keep an eye on all the metrics that your plants care about - ‎water and light, plus environmental conditions like temperature and humidity. ‎Team it with tiny pumps to water your plants automatically!‎

In this tutorial, we’ll show you how everything fits together and how to get ‎started monitoring and auto watering your plants.‎

What you’ll Need

  • An Enviro Grow kit. For monitoring the moisture levels of your plants ‎you just need the Grow Sensors kit, but if you want to do auto-‎watering as well you'll want the full Grow Accessory kit
  • Some plants or seeds that rely on you for sustenance, and soil and pots ‎for them to live in
  • If you're planning on auto-watering, you'll need a reservoir to hold water. ‎We're using a mug for ours, but other types of container are available ‎‎(you probably shouldn't go for this kind)

Prerequisites

We're going to assume that you've provisioned your Enviro Grow and you've ‎got it posting data somewhere. If you haven't done that yet, consult Getting ‎Started with Enviro - this will show you how to set up your Enviro and ‎connect it to adafruit.io - an easy to use cloud data service. We've got our ‎Enviro Grow hooked up to an InfluxDB database hosted on a Raspberry Pi - if ‎you'd like to do the same you can find instructions on how to do that at the ‎link below.‎

Enviro (Pico W Aboard) and InfluxDB

data_1

If you don't want to post your data anywhere right now, you could just save it ‎locally on your Enviro. It's easy to change this later if you want.‎

UPDATING YOUR ENVIRO FIRMWARE

To see the Grow specific settings, you'll need to update your Enviro firmware ‎to the most recent version. Note that updating will delete any files on the ‎device, so you might want to back up any important details/readings first. ‎Here's how to update it:‎

  • Download the latest Enviro .uf2 from the releases page
  • Plug Enviro into your computer
  • Hold down the BOOTSEL button on Enviro and hit RESET to put the ‎board into DFU mode
  • Copy the .uf2 file across to the new RPI-RP2 drive
  • After a few seconds, Enviro should start up in provisioning mode (with ‎the white activity LED flashing quickly). You'll need to reprovision it ‎once you've updated.‎

Plant Monitoring

CONNECTING THE MOISTURE SENSORS

The moisture sensors come in sets of three, still attached to their sprues. ‎Side cutters are the best way to separate them if you have them but ‎snapping them by hand along the perforation line will work too. You can tidy ‎up the rough edge with sandpaper or an emery board if you want (but your ‎plants probably won't mind if you don't).‎

There's an area near the top of each sensor for you to label your plant. Giving ‎your plants names is great for morale, you should definitely do this (ultra-fine ‎Sharpies work well for labelling).‎

label_2

The moisture sensor cables have three wires and are used to connect the ‎sensors to the three ports labelled SOIL on the front of Enviro Grow. The ‎connectors will only go in one way round, so if you’re having trouble plugging ‎them in try rotating the connector and trying it the other way.

sensor_3

For the capacitive moisture sensors to work best as much of them will need ‎to be surrounded by soil as possible, so it’s best to position the sensors a ‎little way in from the edge of the pot and push them in as far as they can go. ‎The Under/Ground line should be above the level of the soil, to avoid the ‎components at the top of the sensors coming into contact with water.‎

cable_4

If the moisture sensor cables that come in the kit are too short, we also stock ‎a longer version.‎

HOW THE MOISTURE SENSORS WORK

Grow's capacitive moisture sensors work using Pulse-Frequency ‎Modulation - they report the moisture level by sending out a regular pattern ‎of on-off electrical pulses, with varying frequency.

‎The Raspberry Pi Pico W on the back of Grow reads the frequency of the ‎pulses, and the Enviro software converts this reading into a percentage ‎relating to the moisture saturation of the soil.‎

We like capacitive sensors because they don't have exposed electrodes, ‎which makes them more resistant to corrosion and means they last longer ‎than old-school conductive moisture sensors.‎

BUZZER ALERTS

These instructions assume that you've updated to v0.0.9 (or later) of the ‎Enviro firmware.‎

Grow will make a cute little noise to attract your attention when the moisture ‎level drops beneath a certain percentage (50% by default). It will make a ‎slightly different noise for each channel so you can tell which pot needs ‎water - one drip for channel 1, two drips for channel 2 etc.‎

You can customise the threshold at which it starts bleeping by re-entering the ‎provisioning process and connecting to Grow with your phone or other device ‎‎(to re-provision: hold down Poke, tap reset and keep holding Poke until the ‎Activity LED starts flashing rapidly). When provisioning an Enviro Grow, there ‎will be an extra page allowing you to adjust the moisture_target percentages.‎

Alternatively, you can edit config.py with Thonny and change ‎the moisture_target percentages under the relevant channel. If you need more ‎help with using Thonny to edit files, check out the link below.‎

If you're not using all the sensors (or if you don't want Grow to make noise) ‎set the relevant channels to 0.‎

A good way of figuring out the right levels is by letting your pots dry out to ‎the point at which you think they need watering, checking the readings, and ‎then setting the moisture_targets to that number.‎

target_5

Note that in v0.0.9 and later the moisture_target channels are named a, b and c ‎‎(to match the printed labels on the board).

‎If you're happy watering your plants manually when Enviro Grow bleeps at ‎you, then you're ready to go. If, however, you have a brain that struggles to ‎remember to do stuff even if things are beeping at you (hi!), you might want ‎to consider getting it to water your plants too!‎

Auto-watering

TIPS FOR SUCCESS

  • Water and electricity are not besties, so make sure to position your ‎auto-watering system as far away from plugs and mains power as you ‎can. It's a good idea to put the whole thing on a tray or something ‎similar, so if you get any water escaping it won't get anywhere ‎dangerous
  • Avoid starting a siphon with your pumps - this could result in your entire ‎water reservoir emptying into your pots quite quickly, which your plants ‎won't appreciate. Make sure that the plant ends of your tubes are ‎always higher than the water level in your reservoir to beat physics and ‎stay dry!‎

SELECTING A WATER RESERVOIR

We're using a mug as our water reservoir for this tutorial, but you could totally ‎build something more elaborate. Something with a lid is good as it will stop ‎your water stash from evaporating - but any kind of plastic box that you can ‎make holes in to poke tubes out of will work - check out our original Grow ‎HAT tutorial for an example of how to do that (this setup is still keeping our ‎office plants alive two years on, hooray!).‎

reservoir_6

Once you've decided what you're using for a reservoir, work out what lengths ‎of tube you will need to connect your reservoir to your pots and chop the tube ‎into an appropriate number of bits. Push the ends of the tube into the outlets ‎on the pumps.‎

pump_7

We sell tube separately if you need more!‎

ATTACHING THE TUBES TO THE POTS

When figuring out how to attach the other end of the tubes to your pots, keep ‎two things in mind.‎

  • Make sure the tube end is securely fastened in place over the pot - if it ‎comes adrift, water is likely to go places it shouldn't
  • Aim to have the tube end positioned well away from the surface of the ‎soil to avoid soil being sucked back down the tube at the end of a ‎watering 'pulse' - if soil gets inside the pump, it could jam or damage it.‎

We're using some little 3D printed widgets to keep the end of our tubes in ‎place here, but you could make a loop of wire round your pot to keep the tube ‎end in place or tie the end to something like a wooden stake.‎

pot_8

For best results, position the tubes so that they're not running directly onto ‎the moisture sensors. We put our tubes and sensors on opposite sides of the ‎pot to make sure that the pot gets thoroughly watered.‎

CONNECTING THE PUMPS TO ENVIRO

The ends of the pump wires plug into the two pin PUMP connectors on the ‎back of Enviro Grow, these connectors are slightly squarer than the ones for ‎the moisture sensors. If you want to plug in other (low current, 5V) devices to ‎these connectors (or extend the length of the pump cables) we ‎sell compatible cables on the shop.‎

connect_9

The connectors will only go in one way round, so if they don't fit, try rotating ‎them. If you need to remove them, make sure to pull on the plug rather than ‎the wires so you don't detach the wires from the connector.‎

FINAL CHECKS

Once you've plugged everything in, double check that each pump matches ‎with the correct moisture sensor for the pot they'll be watering (so the pot ‎containing the sensor attached to SOIL A should be watered by the pump ‎connected to PUMP A). You could draw coloured dots on the connectors, ‎sensors and tube ends so you can keep track of which one is which and ‎match them up correctly.‎

You'll probably find that you'll need to rearrange the pots and adjust the angle ‎of the tube to find a position that they sit nicely in - the tube is rather springy. ‎The cables on the pumps are quite long, so after we added the pumps to our ‎water reservoir we did a bit of cable management to tuck the surplus wire ‎out of the way.‎

watering_10

ENABLING AUTO-WATERING

When you're ready to turn on auto-watering, open up config.py in Thonny and ‎change auto_water to True. Be sure to save the file when you're done. If you're ‎running v0.0.9 or later of the firmware, you can also enable auto-watering ‎through the provisioning process.‎

auto_11

Double check your tube ends are positioned over your plant pots, just in case, ‎and press the poke button. If your Enviro has power, and if the soil moisture ‎level is sufficiently below the moisture_target, watering should happen!‎

CONFIGURING AUTO-WATERING

You'll probably want to adjust the moisture_target settings depending on what ‎kind of plants you're watering. Our second moisture sensor is monitoring Very ‎Spiky Cactus who likes drier soil, so we only want it watering up to 20% ‎saturation. Sensor 1 is monitoring Spider Jerusalem who enjoys more water, ‎so we've left that one at 50% saturation. If you're not sure what saturation ‎level targets to use for your plants, water them manually to the saturation ‎level you want, then check the readings to see what saturation %s is being ‎reported.‎

Our auto-watering code will calculate how long to run the pumps for based on ‎the difference between the moisture level reported by the sensors and ‎the moisture_target level and deliver a bigger pulse of water if more watering is ‎needed.‎

If you want to change this behaviour (to allow for longer tubes, perhaps), ‎open up enviro/boards/grow.py in Thonny and look for this line:‎

duration = round((targets[i] - moisture_levels[i]) / 25, 1)‎

You could change the 25 to a smaller number (like 10) to make all the pulses ‎longer or even change the line to something like the one below if you wanted ‎it to dispense the same amount of water every time. This number is how ‎many seconds the pump will run for.‎

duration = 0.2‎

There will likely be some adjustment required to find the right levels for your ‎setup! If you're tweaking the code, we'd suggest not leaving your setup ‎unattended or overnight until you've monitored it for a while and are happy ‎it's working as intended.‎

Next Steps

Hopefully that will help you get started with the basics of setting up plant ‎monitoring / auto-watering system - as always, tweet us @pimoroni and let ‎us know how you're getting on. Here's Auntie Dawn, fully hydrated!‎

complete_12

That's all folks!

מק"ט יצרן # COM3800
SILICONE TUBE (1M)
Pimoroni Ltd
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.