Maker.io main logo

Power Delivery Board - USB-C (Qwiic) Hookup Guide

168

2024-06-25 | By SparkFun Electronics

License: See Original Project Arduino Qwiic

Courtesy of SparkFun

Guide by ALEX THE GIANT, ELL C

Introduction

USB Type-C brought two significant changes to the USB standard. The reversible connector ‎eliminated the problem of trying to plug the connector in the right way every time. The second ‎major change was allowing the flexibility to have USB power with an adjustable USB voltage from ‎anywhere between 5V and 20V and up to 100W of power. The SparkFun Power Delivery ‎Board takes advantage of the power delivery standard with the use of a standalone controller from ‎STMicroelectronics, the STUSB4500. The controller does all the heavy lifting of power negotiation ‎and provides an easy way to configure over I2C.‎

SparkFun Power Delivery Board - USB-C (Qwiic)‎

 

Required Materials

To follow along with this guide, you will need the following materials. You may not need everything, ‎depending on what you have. Add it to your cart, read through the guide, and adjust the cart as ‎necessary.‎

Power Delivery Board USB-C Wish List SparkFun Wish List

Additional Tools

You will also need a USB Type-C power adapter that supports power delivery and a power delivery ‎Type-C cable which has thicker power wires in the cable. This will minimize voltage drops across ‎the cable and heat up less under high current loads. The Power Delivery Board's voltages and ‎available current output are limited by the power delivery adapter used. The cable and power ‎adapter used in this guide is a 87W USB-C Power Adapter made by Apple, and supports 5.2V, 9V, ‎‎14.5V, and 20.3V.‎

Note: During testing we noticed a significant delay changing voltages with some power adapters ‎that have both a USB Type-A fast charging plug as well as USB Type-C power delivery plug. We ‎recommend getting a power adapter that supports power delivery that only has a USB Type-C ‎connector.‎

voltages_1

Power Adapter Output Voltages‎

Suggested Reading

Before continuing on with this guide, you may want to familiarize yourself with some of these topics ‎if they're unfamiliar to you. If you aren't familiar with the Qwiic system, we recommend reading here ‎for an overview.‎

qwiic_2

Qwiic Connect System

If you aren't familiar with the following concepts, we recommend checking out these tutorials before ‎continuing. Make sure to install the appropriate drivers before uploading code. In this case, we'll ‎need to make sure the CH340 driver are installed for the RedBoard Qwiic.‎

  • I2C: An introduction to I2C, one of the main embedded communications protocols in use today.‎
  • How to Use a Multimeter: Learn the basics of using a multimeter to measure continuity, ‎voltage, resistance and current.‎
  • RedBoard Qwiic Hookup Guide: This tutorial covers the basic functionality of the RedBoard ‎Qwiic. This tutorial also covers how to get started blinking an LED and using the Qwiic system.‎
  • How to Install CH340 Drivers: How to install CH340 drivers (if you need them) on Windows, ‎Mac OS X, and Linux.‎

Hardware Overview

STUSB4500‎

When it comes to power delivery you have two types of power roles. The first is the provider, also ‎known as the source, which is capable of providing power over the USB power bus. The other role ‎is the consumer, also known as the sink, which draws power from the source.‎

The STUSB4500 is a USB Type-C and power delivery controller IC for sink applications. The ‎controller is able to negotiate a power delivery contract with a source (ie a power delivery wall wart ‎or power adapter) without the need for an external microcontroller, although you will need a ‎microcontroller to configure the board. With this controller, we are taking advantage of ‎STMicroelectronics’s proprietary algorithms and configurable power data objects (PDOs) using ‎integrated non-volatile memory (NVM). Its laundry list of features include:‎

  • ‎"Attach detection" between two USB Type-C ports
  • Establish a valid source-to-sink connection
  • Negotiate a USB power delivery (PD) contract with a PD capable source
  • Monitor the VBUS power path and manage the VBUS voltage transitions
  • Manage high voltage protections
  • Dual high power charging path support

Understanding how the power negotiation will be covered in the USB-C Power Negotiation section, ‎but for right now, let's go over the board itself.‎

Power

The Power Delivery board can be powered in one of two ways, either through the USB Type-C ‎connector, or with 3.3V from the Qwiic Connector if you just need to configure a new power ‎delivery profile.‎

board_3

I2C Pins

To configure the board, you will need an I2C bus. The Qwiic system makes it easy to connect the ‎Power Delivery board to a microcontroller to set the NVM parameters to power your project via the ‎Qwiic connector. Depending on your application, you can also connect to the I2C bus via the plated ‎through holes for SDA and SCL.‎

connector_4

Qwiic Connector‎

top_5

Top View

bottom_6

Bottom View

I2C PTH Pins

Pins

The board breaks out the following pins:‎

pintable_7

pins_8

IO Pins

Jumpers

The board has a few jumper pads to configure the I2C bus.‎

‎If you have not worked with jumper pads, make sure to check out the tutorial on how to work with ‎jumper pads and PCB traces for more information.

pads_9

How to Work with Jumper Pads and PCB Traces

Handling PCB jumper pads and traces is an essential skill. Learn how to cut a PCB trace, add a ‎solder jumper between pads to reroute connections, and repair a trace with the green wire method ‎if a trace is damaged.‎

Address Select

The default address of the board is 0x28. If you need to adjust the address of the board, you can ‎cut one or both of the address pads labels ADDR0 and ADDR1.‎

labels_10

The table below lists the four jumper configurations along with the corresponding hexadecimal ‎device address.‎

config_11

Pull-Up Resistors

The board also includes jumpers to disable the pull-up resistors on the I2C bus. If you are using a ‎few I2C devices on the same bus that already have pull-up resistors on their board, you may want to ‎cut the jumpers to disconnect these pull-up resistors. The Power Delivery board utilizes non-volatile ‎memory, the settings saved to device stay configured even if it loses power, so the only time this ‎board needs to be connected over I2C is to modify the NVM parameters.‎

pullup_12

Dimensions

dimensions_13

USB-C Power Negotiation

Power Data Objects (PDOs)‎

The STUSB4500 has a set of user defined parameters that can be customized using the NVM re-‎programming through the I2C interface. This allows for changing the preset configuration of the ‎power delivery interface and define new configurations based on specific application requirements.‎

On power-up, or after a hard reset, the NVM parameters are copied into the I2C registers and used ‎by the controller during the system operation. After a soft reset, the controller will use the values ‎saved in I2C registers to re-negotiate with the source. The controller can store up to three PDOs, ‎with PDO3 having the highest priority and PDO1 having the lowest. After the NVM parameters have ‎been copied to the I2C registers, the STUSB4500 will ask the source for its capabilities to find a ‎PDO match.‎

Each PDO has four parameters as shown in the table below:‎

parameter_14

Each source might have a slightly different voltages listed on the case. One charger might advertise ‎‎12V, while another might advertise 12.3V perhaps to compensate for voltage drop across the cable, ‎while another might say 11.5V to indicate the voltage at the end of the cable under the full load. ‎Most sources though will advertise some combination of 5V, 9V, 12V, 15V, or 20V when negotiating ‎with the consumer.‎

The current should be the maximum amount of current that the Power Delivery board ‎expects to draw from the source. The STUSB4500 is not able to measure the actual current ‎draw and will allow as much current as the source is able to deliver. If the current parameter is less ‎than or equal to the max current the source advertised, the controller will send a request to source ‎for that power profile. If the voltage or current parameters do not match with one of the capabilities ‎of the source, the controller will try the next PDO to find a match with the source.‎

If the source accepts the contract, the source will switch from the defaulted VBUS voltage of 5V, to ‎the voltage that was requested, and the VBUS_EN_SINK pin will be pulled low and enable current ‎to flow through the MOSFET which controls power to the VSNK power output pin.‎

Power Delivery Contract between Source and Sink

With the "U" in USB standing for Universal, when two devices are connected there are a bunch of ‎messages sent between them to figure out what each device is connected to, and what each device ‎supports. For the sake of simplicity, we're only going to look at the power delivery contract from a ‎high level to understand what's going on.‎

delivery_15

Image courtesy of Chindi.ap, CC BY-SA 4.0

Of the 24 pins of the USB Type-C connector (shown above), the STUSB4500 only connects ‎directly to 10 of these: 4 pins are used for VBUS, another 4 pins to ground, and the 2-channel ‎configuration, or CC, pins. Depending on the cable orientation, one of these CC pins is used to ‎send and receive messages between the sink and source. When a sink device connects to a ‎source, the voltage on the VBUS starts off at 5V, just like the old USB standard.‎

Shortly after the source and sink are connected, the source will advertise its capabilities as a power ‎source, such as 5V@3A, 9V@2A, and any other power delivery options it's capable of. After that ‎message is received, the controller will look at the PDO options available to find a match. Upon a ‎match, the controller will ask for one of the voltage and current options. After the source accepts, ‎the voltage is then switched to the voltage requested.‎

To find a match, the STUSB4500 controller first looks at the SNK_PDO_NUMB parameter, which is ‎an integer value between 1 and 3, which corresponds to the highest priority PDO number. If the ‎SNK_PDO_NUMB has a value of 3, it will first check to see if the source is able to provide PDO3, if ‎not it will check PDO2, followed by PDO1. If SNK_PDO_NUMB has a value of 2, it will start by ‎checking PDO2, followed by PDO1, and ignore PDO3. Finally, if SNK_PDO_NUMB has a value of 1, ‎it will only check PDO1. The two values the controller looks at to find a match are the voltage and ‎current. As previously mentioned, most of the power delivery adapters will have a combination of ‎‎5V, 9V, 12V, 15V, and 20V. The packaging might say 5.2V or 20.3V, but in the capabilities message ‎they'll actually specify 5V or 20V.‎

The other portion of the contract is the current being requested. If the voltage is accepted but is ‎only capable of delivering 1.5A of current at that voltage, but 2.0A of current was requested, that ‎contract will be rejected by the source even though the source was capable of supplying that ‎voltage. Alternatively, requesting 0.5A of current with a source capable of delivering 1.5A will be ‎accepted. The amount of current requested should be about is expected for the project, but the ‎source will allow the sink to draw more current than requested, up to the limit of that power delivery ‎option.‎

Hardware Hookup

This is an I2C based board, which allows us to include a Qwiic connector on the breakout board. ‎Hooking up the device is easy, just plug one end of the Qwiic cable into the Power Delivery board ‎and the other to your development board. In this case it's the RedBoard Qwiic.‎

redboard_16

Note: If you've never connected an CH340 device to your computer before, you may need to ‎install drivers for the USB-to-serial converter. Check out our section on How to Install CH340 ‎Drivers for help with the installation.

install_17

How to Install CH340 Drivers

How to install CH340 drivers (if you need them) on Windows, Mac OS X, and Linux.‎

Suppling power to your project can be accomplished in couple of ways. The board provides ‎breadboard friendly 0.1 inch spacing, along with 3.5mm screw terminal spacing. If you're new to ‎soldering, refer to our How To Solder Tutorial.‎

solder_18

After the board has been configured, the Qwiic connector can be removed, and the board will ‎remember the settings even after power is disconnected. With those connections out of the way, ‎it's time to configure the board!

‎Arduino Library

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. ‎If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE. If you ‎have not previously installed an Arduino library, please check out our installation guide.‎

SparkFun has written a library to control the Power Delivery board for the STUSB4500. You can ‎obtain this library through the Arduino Library Manager. By searching for STUSB4500, you should ‎see one written by SparkFun Electronics and you should be able to install the latest version. If ‎you prefer downloading libraries manually, you can grab them from the GitHub Repository.‎

DOWNLOAD THE SPARKFUN POWER DELIVERY BOARD - USB-C ARDUINO LIBRARY ‎‎(ZIP)

Functions

The library has a ton of functions available for reading each of the NVM parameters for the Power ‎Delivery board. Below is a list of the functions available along with a description of what each ‎function does and how to use it.‎

  • uint8_t begin( uint8_t deviceAddress, TwoWire &wirePort ) - Call at the beginning of the ‎sketch to initialize the device. This function takes two optional parameters: deviceAddress and ‎wirePort. This function will return true when the device is initialized, and false if it is unable ‎to communicate with the device.‎
    • wirePort - By default, the library uses the standard Wire bus, but if your board has ‎multiple I2C buses, you can define Wire1 here.‎
    • deviceAddress - If both of the address jumpers on the back of the board are closed, ‎this parameter does not need to be provided. Otherwise, you can use the table below ‎to get the I2C address of the Power Delivery Board.‎

functions_19

  • void read( void ) - This function reads the NVM parameters and loads them into memory. ‎This function is called in the begin() function and shouldn't need to be called in your program.‎
  • void write( uint8_t defaultVals ) - This function writes the NVM parameters to the ‎STUSB4500. After all of the parameters have been changed, calling this function will save the ‎parameters to the device. This function takes an optional argument of DEFAULT. When ‎DEFAULT is passed to the write function, the default NVM parameters are written to the ‎device.‎
  • void softReset( void ) - This function performs a soft reset of the STUSB4500. After a soft ‎reset power is re-negotiated with the source using the values loaded in the PDO registers. To ‎see this function in use, refer to Example4-ChangingVoltages in the Arduino library, or the ‎‎“Changing Voltages on the Fly” example below.‎
  • float getVoltage( uint8_t pdo_numb ) - Returns the voltage requested for the PDO number ‎‎(1-3).‎
  • float getCurrent( uint8_t pdo_numb ) - Returns the current requested for the PDO number ‎‎(1-3).‎
  • uint8_t getLowerVoltageLimit( uint8_t pdo_numb ) - Returns the under-voltage lockout ‎parameter for the PDO number (1-3). PDO1 has a fixed value that cannot be changed and will ‎always return 0. The under-voltage limit is fixed at 3.3V. PDO2 and PDO3 will return a value ‎between 5% and 20%.
  • uint8_t getUpperVoltageLimit( uint8_t pdo_numb ) - Returns the over voltage lockout ‎parameter for the PDO number (1-3). The value returned will be between 5% and 20%.‎
  • float getFlexCurrent( void ) - Return the value for the flex current parameter, which is a ‎global variable common to all PDOs. Refer to setFlexCurrent function for more information on ‎how to use flex current.
  • uint8_t getPdoNumber( void ) - Returns value saved in memory for the highest priority PDO ‎number (1-3).‎
  • uint8_t getExternalPower( void ) - Returns the value for the SNK_UNCONS_POWER ‎parameter (0 or 1). SNK_UNCONS_POWER is the unconstrained power bit setting in ‎capabilities message sent by the sink. A 0 means there is no external source of power ‎‎(default), and a 1 means an external source of power is available and is sufficient to ‎adequately power the system while charging external devices.
  • uint8_t getUsbCommCapable( void ) - Returns the value for the USB_COMM_CAPABLE ‎parameter (0 or 1). USB_COMM_CAPABLE refers to USB2.0 or 3.x data communication ‎capability by the sink system. A 0 means the sink device does not support data communication ‎‎(default). A 1 means that the sink does support data communication.‎
  • uint8_t getConfigOkGpio( void ) - Returns the POWER_OK_CFG parameter value (0-3), ‎which controls the behavior of the VBUS_EN_SNK, POWER_OK2, and POWER_OK3 pins. ‎Refer to the setConfigOKGPIO function for more information.‎
    • ‎0 - Configuration 1
    • ‎1 - Not applicable
    • ‎2 - Configuration 2 (default)
    • ‎3 - Configuration 3
  • uint8_t getGpioCtrl( void ) - Returns the behavior setting for the GPIO pin (0-3). Refer to ‎the setGpioCtrl function for more information.‎
    • ‎0 - Software controlled GPIO
    • ‎1 - Error recovery
    • ‎2 - Debug
    • ‎3 - Sink power
  • uint8_t getPowerAbove5vOnly( void ) - Returns the POWER_ONLY_ABOVE_5V parameter ‎‎(0 or 1). If 0 is returned, the output will be enabled when the source is attached, regardless of ‎the voltage. If 1 is returned, the output will be enabled only when the source is attached and ‎VBUS voltage is negotiated to PDO2 or PDO3.‎
  • void setPdoNumber( uint8_t pdo_numb ) - Takes the parameter pdo_numb (1-3). There ‎are three Power Data Objects (PDO) that the Power Delivery board can store. PDO3 has the ‎highest priority, followed by PDO2, and finally PDO1. This function declares which of the ‎three PDOs should be negotiated first. For example, if setPdoNumber is set to 3, PDO3 will ‎be negotiated first, followed by PDO2 if a contract is not made, and finally PDO1 if PDO2 fails ‎as well. If setPdoNumber is set to 2, PDO3 will be ignored and PDO2 will be negotiated, ‎followed by PDO1. Lastly if setPdoNumber is set to 1, only PDO1 will be negotiated.‎
  • void setVoltage( uint8_t pdo_numb, float voltage ) - Takes two parameters: pdo_numb ‎‎(1-3), and voltage (10-bit resolution). PDO1 is fixed at 5V and cannot be changed. PDO2 and ‎PDO3 can be any voltage up to 20V.‎
    • The PDO3 has the highest priority and PDO1 has the lowest priority, starting at the ‎number defined in the setPdoNumber()parameter. The source controls the voltage ‎present on VBUS, or in the case of the Power Delivery board, VIN. Common voltages ‎available from sources are: 5V, 9V, 12V, 15V, and 20V.‎
  • void setCurrent( uint8_t pdo_numb, float current ) - Takes two parameters: pdo_numb (1-‎‎3), and current (16 values). The current values are: 0 (Flex Current), 0.5A, 0.75A, 1.0A, 1.25A, ‎‎1.50A, 1.75A, 2.0A, 2.25A. 2.50A, 2.75A, 3.0A, 3.5A, 4.0A, 4.5A, and 5.0A.‎
    • The current value should be the amount that the source should be expected to output. ‎If the current is higher than the source is able to provide, the contract will be rejected ‎and the next PDO contract will be negotiated. The Power Delivery board will sink more ‎current than negotiated if the source is able deliver it, but it's recommended to provide ‎the maximum amount of current the project is expected to draw.‎
  • setFlexCurrent( float value ) - Takes a float value to set the current common to all PDOs. ‎This value is only used in the power negotiation if the setCurrent value for that PDO is set to 0. ‎The flex current has a resolution of 10mA. Just like the setCurrent function, the current value ‎should be the amount that the source should be expected to deliver. If the current is higher ‎than the source is able to provide, the contract will be rejected and the next PDO contract will ‎be negotiated.‎
  • setLowerVoltageLimit (uint8_t pdo_numb, uint8_t value ) - Takes two parameters: ‎pdo_numb (2-3), and a integer value (5-20%). Only PDO2 and PDO3 can be changed as ‎PDO1 has a fixed value of 3.3V. In combination with the setUpperVoltageLimit function, this ‎is used to define an acceptable window for the voltage output.
    • ‎For example, if the Power Delivery board requests 15V and has a under voltage ‎tolerance of 5%, the controller will disable the output of the Power Delivery board if ‎the voltage drops below 14.25V, which is 5% of 15V.‎
  • setUpperVoltageLimit( uint8_t pdo_numb, uint8_t value ) - Takes two parameters: ‎pdo_numb (1-3), and a integer value (5-20%). In combination with ‎the setLowerVoltageLimit function, this is used to define an acceptable window for the ‎voltage output.‎
    • For example, if the Power Delivery board requests 15V and has an over voltage ‎tolerance of 5%, the controller will disable the output of the Power Delivery board if ‎the voltage exceeds 15.75V, which is 5% of 15V.‎
  • setExternalPower( uint8_t value ) - Takes an integer value (0 or 1). Setting to 0, there is no ‎external source of power. Setting to 1, means there is an external power source available, and ‎is sufficient to adequately power the system while charging external devices.‎
  • setUsbCommCapable( uint8_t value ) - Takes an integer value (0 or 1). Setting to 0, there ‎sink does not support data communication. Setting to 1, means the sink does support data ‎communication.
  • setConfigOkGpio( uint8_t value ) - Takes an integer value (0-3):‎
    • ‎0 - Configuration 1
    • ‎1 - Not applicable
    • ‎2 - Configuration 2 (default)
    • ‎3 - Configuration 3

set_20

Note: For configuration 3: "Source supplies 1.5A/3.0A USB Type-C current at 5V when source is ‎attached" is based on what the source advertises when the cable is connected and ‎does not indicate that the output voltage is actually 5V.‎

  • setGpioCtrl( uint8_t value ) - Takes an integer value (0-3) to control the GPIO pin (active ‎LOW).

sink_21

Note: For value 3 - Sink Power: "Source supplies 1.5A/3.0A USB Type-C current at 5V when ‎source is attached" is based on what the source advertises when the cable is connected and ‎does not indicate that the output voltage is actually 5V.‎

  • setPowerAbove5vOnly( uint8_t value ) - Takes an integer value (0 or 1). Setting to 0, the ‎output is enabled regardless of the of the negotiated voltage. When set to 1, the output is ‎enabled only when the source is attached, and the voltage is negotiated for PDO2 or PDO3.‎
  • setReqSrcCurrent( uint8_t value ) - Takes an integer value (0 or 1). Setting to 0 requests ‎the sink current as operating current in the RDO message. Setting to 1 requests the source ‎current as operating current in the RDO message.‎

Arduino Library Examples

In these examples, we'll connect our Power Delivery board to a RedBoard Qwiic using a Qwiic cable. ‎The Type-C power adapter used in these examples is an Apple 87W USB-C Power Adapter which ‎has an output of 20.3V/4.3A, or 14.5V/2A, or 9V/3A, or 5.2V/2.4A.‎

Example 1: Reading the NVM Values

In this first example we'll see what settings are currently saved in the board. For this example, you ‎don't need to connect to your USB cable, the only connection needed is VDD, GND, SCL, and SDA ‎‎(which the Qwiic cable will provide).‎

After the library has been installed, access the first example from your Arduino menu by clicking ‎on: File > Examples > SparkFun STUSB4500 > Example1-ReadParameters. Select your board ‎‎(in this case Arduino Uno) and COM port that the board enumerated to. Hit the upload button. ‎Open the serial monitor at 115200 baud to see what the current settings are.‎

com9_22

The STUSB4500 is able to store up to three power data objects, or PDOs. Each PDO contains the ‎voltage and current to be requested, along with the voltage tolerance. We can see that the PDO ‎number parameter is set to 3, which means that when we plug in the power adapter, the board will ‎first try to find a power option that matches PDO3, which has a voltage of 20.00V, and maximum ‎current draw of 1.0A. If the power adapter is able to provide at least 1.0A of current at 20.00V, the ‎contract will be accepted by the source and switch to the higher voltage. If the output voltage falls ‎outside of the tolerance window of +10% or -20% (16-22V), the sink controller will disconnect from ‎the source and reset. However, if PDO3 does not match with the source, it will try PDO2's ‎parameters, and if a match is still not made the voltage would stay at 5V.‎

Flex current is set to 2.00A, but since none of the PDOs have a current set to 0, that value will not ‎be used. We also see that the board is not expecting an external source of power, nor does it ‎expect the source to support USB communication. The Configuration OK GPIOs are set to 2, which ‎will mean that when a source is connected, if the contract for PDO2 or PDO3 is accepted, the LED ‎corresponding to that PDO will turn on. GPIO control is set to 1, which means the GPIO LED is ‎currently configured for error recovery indication. The enable power only above 5V bit is not set, so ‎the output voltage will briefly be at 5V, but will increase after a contract is accepted. Lastly, we see ‎that the request source current bit is not set.‎

Now that we know what the board is configured for, in our next example we'll configure the board ‎based on the capabilities of our power adapter.‎

Example 2: Setting NVM Values

In this example we'll modify the NVM values. The code listed below is NOT the same as ‎the SetParameters example in Arduino - below we set actual values, whereas ‎the SetParameters example is a template for your future use.‎

For this example, we'll need to use a power delivery source, which is a 87W USB-C Power Adapter ‎made by Apple, but there are plenty of other adapters available that provide a range of voltages. ‎The power adapter should have a label that describes the input and output power capabilities as ‎shown below.‎

setting_23

The input power is 100-240 VAC and up to 1.5A of primary current. The output can provide one of ‎the following: 20V/4.3A, or 15V/2A, or 9V/3A, or 5V/2.4A. Based on these options, let's change the ‎voltage to 15V. That voltage option is able to draw up to 2A of current. The current requested can ‎only go up to that value for the power delivery contract to be accepted. The increased voltage of ‎‎15.3V instead of 15.0V is labeled based on the actual output voltage, but the source should ‎advertise 15.0V. The increase is to compensate for voltage drop across the cable under heavy ‎current draw. The settings we're going to change though are:‎

  • PDO Number: 3
  • PDO3 Voltage: 15.0V
  • PDO3 Current: 0.5A
  • PDO3 Upper Voltage Tolerance: 20%‎
  • PDO3 Lower Voltage Tolerance: 20%‎

Copy the code below into your Arduino IDE and upload it to your board. After the code has been ‎uploaded, open your serial port, and verify the changes were applied.‎

Copy Code
/*
Writing New Settings to the STUSB4500 Power Delivery Board
By: Alex Wende
SparkFun Electronics
Date: February 6th, 2020
License: This code is public domain but you buy me a beer if you use this and we meet someday (Beerware license).
Feel like supporting our work? Buy a board from SparkFun!
https://www.sparkfun.com/products/15801

This example demonstrates how to write new NVM settings to the STUSB4500

Quick-start:
- Use a SparkFun RedBoard Qwiic -or- attach the Qwiic Shield to your Arduino/Photon/ESP32 or other
- Upload example sketch
- Plug the Power Delivery Board onto the RedBoard/shield
- Open the serial monitor and set the baud rate to 115200
- The RedBoard will connect to the Power Delivery Board over I2C write the settings:
* PDO Number: 3
* PDO3 Voltage: 15.00V
* PDO3 Current: 0.5A
* PDO3 Under Voltage Lock Out: 20%
* PDO3 Over Voltage Lock Out: 20%
- After the settings are written, the old settings are printed out and then the new settings are printed
*/
// Include the SparkFun STUSB4500 library.
// Click here to get the library: http://librarymanager/All#SparkFun_STUSB4500

#include <Wire.h>
#include <SparkFun_STUSB4500.h>

STUSB4500 usb;

void setup()
{
Serial.begin(115200);
Wire.begin(); //Join I2C Bus
delay(500);

/* The Power Delivery board uses the default settings with address 0x28 using Wire.

Opionally, if the address jumpers are modified, or using a different I2C bus,
these parameters can be changed here. E.g. usb.begin(0x29,Wire1)

It will return true on success or false on failure to communicate. */
if(!usb.begin())
{
Serial.println("Cannot connect to STUSB4500.");
Serial.println("Is the board connected? Is the device ID correct?");
while(1);
}

Serial.println("Connected to STUSB4500!");
delay(100);

float voltage, current;
byte lowerTolerance, upperTolerance, pdoNumber;

pdoNumber = usb.getPdoNumber();
voltage = usb.getVoltage(3);
current = usb.getCurrent(3);
lowerTolerance = usb.getLowerVoltageLimit(3);
upperTolerance = usb.getUpperVoltageLimit(3);

/* Since we're going to change PDO3, we'll make sure that the
STUSB4500 tries PDO3 by setting PDO3 to the highest priority. */
usb.setPdoNumber(3);

/* PDO3
- Voltage 5-20V
- Current value for PDO3 0-5A, if 0 used, FLEX_I value is used
- Under Voltage Lock Out (setUnderVoltageLimit) 5-20%
- Over Voltage Lock Out (setUpperVoltageLimit) 5-20%
*/
usb.setVoltage(3,15.0);
usb.setCurrent(3,0.5);
usb.setLowerVoltageLimit(3,20);
usb.setUpperVoltageLimit(3,20);

/*Write and save settings to STUSB4500*/
usb.write();

/*Read settings saved to STUSB4500*/
usb.read();

Serial.println();

/*Print old setting*/
Serial.println("Original Values:");
Serial.print("PDO Number: ");
Serial.println(pdoNumber);
Serial.print("Voltage3 (V): ");
Serial.println(voltage);
Serial.print("Current3 (A): ");
Serial.println(current);
Serial.print("Lower Voltage Tolerance3 (%): ");
Serial.println(lowerTolerance);
Serial.print("Upper Voltage Tolerance3 (%): ");
Serial.println(upperTolerance);

Serial.println();

/*Print new settings*/
Serial.println("New Values:");
Serial.print("PDO Number: ");
Serial.println(usb.getPdoNumber());
Serial.print("Voltage3 (V): ");
Serial.println(usb.getVoltage(3));
Serial.print("Current3 (A): ");
Serial.println(usb.getCurrent(3));
Serial.print("Lower Voltage Tolerance3 (%): ");
Serial.println(usb.getLowerVoltageLimit(3));
Serial.print("Upper Voltage Tolerance3 (%): ");
Serial.println(usb.getUpperVoltageLimit(3));
}

void loop()
{
}

After the code has uploaded, open the serial monitor at 115200 baud and make sure the settings ‎were applied, as shown below.‎

com_24

Reset the Power Delivery board and connect the USB-C cable. If the contract was accepted, the ‎yellow LED for PDO3 should be on. With a multimeter, verify the voltage is around 15V as shown ‎below. If the LED turns off, press the reset button and board should switch to the correct voltage.‎

reset_25

Example 3: Changing Voltages on the Fly

In this example we will use the soft reset function to force the STUSB4500 to re-negotiate with the ‎power delivery source. Using the same power supply as the previous example, we have 5, 9, 12, 15, ‎and 20V available. If you’re following along from the previous example, the Power Delivery board ‎will initially negotiate for 15V, then the voltage will change to 9V, followed by 12V, and then 5V ‎before looping back to 9V about every three seconds.‎

Copy the code below into your Arduino IDE and upload to your board, or you can load Example 4-‎ChangingVoltages from the examples menu for the SparkFun STUSB4500 library.‎

Copy Code
/*
Changing Output Voltage on the Fly
By: Alex Wende
SparkFun Electronics
Date: February 16th, 2021
License: This code is public domain but you buy me a beer if you use this and we meet someday (Beerware license).
Feel like supporting our work? Buy a board from SparkFun!
https://www.sparkfun.com/products/15801

This example demonstrates how to change the STUSB4500 output voltage without cycling power or pressing the
reset button for the STUSB4500. Note that the STUSB4500 is not a voltage regulator, the voltages the board is
capable of outputting are only those supported by the USB-C power adapter connected.

Quick-start:
- Use a SparkFun RedBoard Qwiic -or- attach the Qwiic Shield to your Arduino/Photon/ESP32 or other
- Modify the voltages to match those supported by the power adapter (most common are 5,9,12,15,20V)
- Upload the sketch
- Plug the Power Delivery Board onto the RedBoard/shield
- Open the serial monitor and set the baud rate to 115200
- The RedBoard will connect to the Power Delivery Board over I2C and print out all of the settings saved.
*/

// Include the SparkFun STUSB4500 library.
// Click here to get the library: http://librarymanager/All#SparkFun_STUSB4500

#include <Wire.h>
#include <SparkFun_STUSB4500.h>

STUSB4500 usb;

void setup()
{
Serial.begin(115200);
Wire.begin(); //Join I2C bus

delay(500);

/* The Power Delivery board uses the default settings with address 0x28 using Wire.

Opionally, if the address jumpers are modified, or using a different I2C bus,
these parameters can be changed here. E.g. usb.begin(0x29,Wire1)

It will return true on success or false on failure to communicate. */
if(!usb.begin())
{
Serial.println("Cannot connect to STUSB4500.");
Serial.println("Is the board connected? Is the device ID correct?");
while(1);
}

Serial.println("Connected to STUSB4500!");
delay(100);

/* Read the settings saved to the NVM map*/
usb.read();

/* Read the Power Data Objects (PDO) highest priority */
Serial.print("PDO Number: ");
Serial.println(usb.getPdoNumber());

/* Read settings for PDO1 */
Serial.println();
Serial.print("Voltage1 (V): ");
Serial.println(usb.getVoltage(1));
Serial.print("Current1 (A): ");
Serial.println(usb.getCurrent(1));
Serial.print("Lower Voltage Tolerance1 (%): ");
Serial.println(usb.getLowerVoltageLimit(1));
Serial.print("Upper Voltage Tolerance1 (%): ");
Serial.println(usb.getUpperVoltageLimit(1));
Serial.println();

/* Read settings for PDO2 */
Serial.print("Voltage2 (V): ");
Serial.println(usb.getVoltage(2));
Serial.print("Current2 (A): ");
Serial.println(usb.getCurrent(2));
Serial.print("Lower Voltage Tolerance2 (%): ");
Serial.println(usb.getLowerVoltageLimit(2));
Serial.print("Upper Voltage Tolerance2 (%): ");
Serial.println(usb.getUpperVoltageLimit(2));
Serial.println();

/* Read settings for PDO3 */
Serial.print("Voltage3 (V): ");
Serial.println(usb.getVoltage(3));
Serial.print("Current3 (A): ");
Serial.println(usb.getCurrent(3));
Serial.print("Lower Voltage Tolerance3 (%): ");
Serial.println(usb.getLowerVoltageLimit(3));
Serial.print("Upper Voltage Tolerance3 (%): ");
Serial.println(usb.getUpperVoltageLimit(3));
Serial.println();

/* Read the flex current value */
Serial.print("Flex Current: ");
Serial.println(usb.getFlexCurrent());

/* Read the External Power capable bit */
Serial.print("External Power: ");
Serial.println(usb.getExternalPower());

/* Read the USB Communication capable bit */
Serial.print("USB Communication Capable: ");
Serial.println(usb.getUsbCommCapable());

/* Read the POWER_OK pins configuration */
Serial.print("Configuration OK GPIO: ");
Serial.println(usb.getConfigOkGpio());

/* Read the GPIO pin configuration */
Serial.print("GPIO Control: ");
Serial.println(usb.getGpioCtrl());

/* Read the bit that enables VBUS_EN_SNK pin only when power is greater than 5V */
Serial.print("Enable Power Only Above 5V: ");
Serial.println(usb.getPowerAbove5vOnly());

/* Read bit that controls if the Source or Sink device's
operating current is used in the RDO message */
Serial.print("Request Source Current: ");
Serial.println(usb.getReqSrcCurrent());
}

void loop()
{
/*
* The output voltage shouldn't change yet. This is because
* the soft reset function needs to called to take affect.
*/
Serial.println("\nSet PDO3 to 9V (nothing should happen)");
usb.setPdoNumber(3); //Make sure PDO3 is set to the highest priority for this example
usb.setVoltage(3,9.0);
delay(3000);

// Now the voltage should change to 9V after calling the softReset function
Serial.println("Performing a soft reset should now let the voltage change");
usb.softReset();
delay(3000);

// Let's try changing to 12V now
Serial.println("Setting PDO3 to 12V");
usb.setVoltage(3,12.0);
usb.softReset();
delay(3000);

/*
* Instead of writing a voltage, you can also just change the PDO number,
* and then call softReset.
*
* USB PD must be able to support at least 5V. As a result, PDO1 is fixed
* at 5V and cannot be changed. Switching to PDO1 is a fast and easy way
* swap to 5V without having to set the voltage to 5V.
*/
Serial.println("Switching to PDO1");
usb.setPdoNumber(1);
usb.softReset();
delay(3000);
}

After the code has been uploaded, open the serial monitor at 115200 baud, and you should see ‎something like this:‎

code_26

The softReset function forces the STUSB4500 to re-negotiate with the source using the values ‎saved in the I2C registers, not the NVM registers. When the voltage is changed in the highest ‎priority PDO register and a soft reset is performed the Power Delivery board re-negotiates with new ‎voltage and current values. If you want to flip between the three different PDO values, you can ‎change the value of the setPdoNumber function instead changing the voltage or current values.

‎It’s important to mention that these values are not saved to the NVM registers unless ‎the write function is called. So, after a hard reset using the reset button or pin, or after a power ‎cycle, the values saved in the NVM registers get copied into the PDO registers.‎

Troubleshooting

‎Need help? ‎

If your product is not working as you expected or you need technical assistance or information, ‎head on over to the SparkFun Technical Assistance page for some initial troubleshooting. ‎

If you don't find what you need there, the SparkFun Forums are a great place to find and ask for ‎help. If this is your first visit, you'll need to create a Forum Account to search product forums and ‎post questions.‎

Resources and Going Further

Can't get enough details of our Power Delivery Board? Check out these resources:‎

מק"ט יצרן # 15801
POWER DELIVERY USB-C QWIIC
SparkFun Electronics
מק"ט יצרן # 17259
FLEXIBLE QWIIC CABLE - 100MM
SparkFun Electronics
מק"ט יצרן # 15123
REDBOARD QWIIC ATMEGA328 EVAL BD
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.