Maker.io main logo

Pulse Room

72

2017-07-19 | By Adafruit Industries

License: See Original Project Arduino Adafruit Feather

Courtesy of Adafruit

Guide by Collin Cunningham

 

 

Overview

Technology connects us to the outer world, but have we lost touch with our inner selves? Let's attempt to remedy this modern condition by controlling room lighting & sound with the beating of your own heart. Hey - it's worth a shot.

This project uses a Pulse Sensor Amped, Feather M0, MusicMaker FeatherWing, RGB LED strips, and power MOSFETs to turn any room into a thumping, flashing pulse room. For a more refined version of this idea in a gallery setting, see Sean Montgomery's excellent Emergence installation.

What you'll need

Basics:

Feather Parts:

LED Driver Parts:

Software

Software image

The code for this project is based off the Pulse Sensor Amped's Arduino sketch. Modifications have been made to include audio file playback, timer interrupts on the Feather M0, and serial output has been removed to keep things simple.

First, install the latest version of the Arduino IDE, if you haven't already:

Download Arduino IDE.zip

Install Adafruit SAMD Boards

SAMD Warning

Open the Arduino IDE and go to Tools->Board->Boards Manager... and use the search box to find "SAMD". First, ensure that Arduino SAMD Boards is not installed (if it is installed, remove it). Then select Adafruit SAMD Boards, click the Select Version pulldown menu, select version 1.0.13. Click the Install button and wait for the process to complete.

Board Manager

Install Libraries

Next, you'll need a couple of Arduino libraries. The first one can be installed via the Arduino IDE's library manager. Go to the Sketch->Include Library->Manage Libraries... Search for "VS1053" and install the Adafruit VS1053 Library.

Library Manager

Next, download the Adafruit ZeroTimer library from GitHub:

Download Adafruit Zerotimer Library.zip

Unzip the downloaded archive, and rename the resulting folder to "Adafruit_ZeroTimer" (just remove the "-master" string). Once the folder is renamed, move it to your Arduino library folder (Documents/Arduino/libraries) and restart the Arduino IDE.

rename the resulting folder to "Adafruit_ZeroTimer"

You'll also need the Adafruit_ASFCore library, which is available here:

Adafruit_ASFcore library.zip

Unzip the downloaded archive, and rename the resulting folder to "Adafruit_ASFcore" (just remove the "-master" string). Once the folder is renamed, move it to your Arduino library folder (Documents/Arduino/libraries) and restart the Arduino IDE.

Download project code & upload to Feather

Grab the Pulse_Room project code from GitHub:

Download Pulse Room Code.zip

Unzip the downloaded archive and rename the resulting folder to Pulse_Room. Inside the folder, you'll find the Pulse_Room.ino file - open it in the Arduino IDE.

rename the resulting folder to Pulse_Room

Pulse Room

Connect your Feather M0 board via USB. Go to Tools->Board and select Adafruit Feather M0 (Native USB Port) from the list. Then go to Tools->Port and select the port for your Feather M0. Click the Upload button and wait for the process to complete.

Sound File

Now that the Feather is programmed, we can put our sound file on an SD Card for playback. You could use your own sound file, or the one I used named beat1.mp3, which is included in the Pulse_Room zip file downloaded in the previous step. More info on compatible file formats can be found in the MusicMaker FeatherWing guide.

I used named beat1.mp3

put our sound file on an SD Card

Copy the file to the root level of your Micro SD card. Note that your SD card should be formatted for FAT16 or FAT32 and have a capacity greater than 64MB.

Feather Connections

Feather Connections

About those headers…

In order to have access to the Feather M0's prototyping area, I decided to mount the MusicMaker Wing underneath the Feather. I also wanted to easily connect & disconnect the Pulse Sensor - so this means we'll need female headers on both the M0 & MusicMaker Wing.

Solder the stacking female headers

Solder the stacking female headers (headers with longer pins) to the Feather M0.

Solder the regular female headers

Solder the regular female headers to the MusicMaker FeatherWing.

Once complete, your boards should look something like this …

your boards should look something like this

Mount components on Feather M0

We'll be adding two components to the Feather M0's prototyping area:

  • SPDT slide switch for muting sound & light output until we have a steady pulse
  • 5-pin terminal block for easy connections to the LED driver boards

Here's a schematic showing all the connections we'll make to the Feather (including the Pulse Sensor Amped).

schematic showing the connections to the Feather

Position the terminal block and slide switch

Position the terminal block and slide switch on the Feather's prototyping area and solder them in place.

Solder bottom 3 pins to GND/solder top 2 pins together

Solder the bottom 3 pins of the terminal block to GND and solder the top 2 pins together (we'll connect these to pin 11).

Connect M0

Use solid core hookup wire to connect the M0's Pin 12 to the center pin of the switch and solder the switch's bottom pin to GND.

Use another hookup wire to connect the M0's Pin 11 to the top 2 pins of the terminal block. Solder the terminal blocks

For reference - below is a shot of the feather after soldering is complete. Note the use of the GND bus conveniently located in the Feather's prototyping area:

The feather after soldering is complete

To avoid mistakes later, use a marker or paint to label the terminal block's ground connections.

label the terminal block

Connect it all

Connect Feather M0 on top of MusicMaker FeatherWing

Connect the Feather M0 on top of the MusicMaker FeatherWing and make sure they're securely mounted.

Connect the Pulse Sensor Amped to the Feather M0

Connect the Pulse Sensor Amped to the Feather M0:

  • Purple wire = A0
  • Black wire = GND
  • Red wire = 3V

Pop the SD card into the MusicMaker Wing

Pop the SD card into the MusicMaker Wing, and you're good to go.

LED Driver

The LED driver board will take the 3.3 V PWM signal from the Feather M0 and use it to control 12 V power needed for the LED strips. One board connected to a 12V 1A power supply is capable of pulsing the red channel of two 5-meter LED strips without the need for a heatsink.

The board itself is quite simple. Check out the schematic below:

Check out the schematic

We put down a 1 Megaohm resistor for the pulldown resistor but later found 10 Kohm works better!

Component layout

Component layout

Place the components on the Perma-Proto board, solder, and trim any protruding leads.

Place the components on the Perma-Proto board

Solder and trim any protruding leads

Solder wire jumpers

Solder the necessary connections between components using solid core hookup/jumper wire. Check the image below to reference what connections need to be made:

Solder the necessary connections between components

The finished board should look something like this:

finished board should look something like this

Label the terminal block

Label the terminal block to avoid incorrect connections. You can use a marker, paint, or the best of both worlds - a paint marker.

Label terminal block to avoid incorrect connections

Since we're only using the red channel of the LED strips, each 12V LED Driver board will be able to power 2 x 5-meter strips. Build additional boards as needed …

Build additional boards as needed

Wiring

A whole lotta wire…

Determine where you'd like to place the Feather + Pulse Sensor in your room and then decide where you to place the LED driver boards + LED strips. I placed the Feather near the middle of the room on a coffee table and the driver boards on opposite walls – so I needed a lot of wire to connect the Feather to each driver (~20ft to allow for routing around furniture/etc).

A whole lotta wire

Each board needs 2 connections - one for PWM signal, and one for ground. 2-conductor cable, such as a thin coaxial type, would be ideal for this situation. I had 26AWG stranded wire on hand, so that's what's used in this guide.

Figure out the length you'll need, then cut two matching lengths of different colored wire (I used black for ground & yellow for PWM)

Strip 1/4 inch of insulation off the ends of each wire

Strip about 1/4 inch of insulation off the ends of each wire, then tin the tips with solder.

Optionally, to keep the wires from getting too unruly, you can twist the pairs together and bind them at regular intervals with tape or heat shrink tubing …

Twist wires together and bind at regular intervals

Extend the LED Strip Wires

The wires coming off the LED strips aren't very long, so you'll likely need to solder extensions to them. Since we're only using the red channel, we only need to extend the red & black wires.

color coding on the strip

The color coding on the strip's wires is a bit confusing. The red wire is a ground/negative connection for the red channel and the black wire is the positive/12V connection for the whole strip. Because these colors were the opposite of conventional designation, I swapped them when extending. Hopefully, this does not make things even more confusing for those following along.

Strip and solder the tips

Cut two pieces of stranded wire for the extensions - ~4ft worked for me. Strip and solder the tips.

Solder the extensions to the LED strip

Solder the extensions to the LED strip's wires and seal the connections with heat shrink tubing or electrical tape.

The tail end of the LED strip also has wire leads for chaining strips (an option I did not explore). To avoid shorts, wrap the red and black wires on that end with a couple layers of electrical tape…

To avoid shorts, wrap the red and black wires

Installation & Usage

Mount LED strips & drivers

The LED strips have adhesive backing

The LED strips have an adhesive backing which is handy for mounting but could potentially damage some delicate surfaces. If you wish to minimize adhesive contact, leave the paper backing on the strips and use pieces of double sided or gaffers tape at ~1ft intervals.

You could also simply hang them around like Christmas lights - experiment to see what you like the best.

To minimize harshness mount out of direct sight

These LEDs are quite bright and looking at them directly can be rough on the eyes.

To minimize harshness, mount the LEDs around molding, behind furniture, or facing upward above eye level - this will create a pleasantly diffused and ambient effect.

Mount LED driver boards/connect to LED strip

Mount the LED driver boards on the wall or somewhere close enough to connect to the LED strip's wires. Insert the wires into the driver board's terminal block and screw them into place.

Don't connect power to the boards just yet!

Final Connections

Connect power to Feather M0 via USB jack/JST battery

Connect power to the Feather M0 via the USB jack or JST battery connector and connect audio to your amplifier via the MusicMaker wing's 3.5mm jack.

Insert and screw down ground & PWM wires on the Feather and connect them to the LED driver boards.

Use Pulse Sensor

Finally, Connect 12V power to the LED driver boards.

Use it.

Pulse Sensor

See the Pulse Sensor Amped guide for specifics on wearing the sensor. I found attaching it to my thumb with the included velcro strips produced the most reliable, steady connection.

Red LED on Feather M0 will flash at every beat

The red LED on the Feather M0 will flash at every beat detected. Once you see a relatively slow, steady flashing, you'll know you have a good connection to the pulse sensor.

Once you have a steady pulse shown on the Feather's LED, go ahead and flick the switch on the Feather and witness your pulse displayed at room scale …

switch on the Feather and witness your pulse

Now sit and ask yourself, "Why did I do this?" and suddenly remember – art serves no practical purpose. It's just cool.

ON-OFF-ON-OFF ALTERNATING POWER
מק"ט יצרן # 1684
ON-OFF-ON-OFF ALTERNATING POWER
Adafruit Industries LLC
מק"ט יצרן # 24-6040-0010
SOLDER RA 60/40 24AWG 1LB
Kester Solder
מק"ט יצרן # 1311
HOOK-UP 22AWG SOLID - 6 X 25FT
Adafruit Industries LLC
מק"ט יצרן # 2976
HOOK-UP 22AWG BLACK 25'
Adafruit Industries LLC
מק"ט יצרן # JIC-2030
WIRE STRIPPER 20-30 AWG
Jonard Tools
מק"ט יצרן # 95190
SCREWDRIVER SET PHIL/SLOT 6PC
Wiha
מק"ט יצרן # 11574
PULSE SENSOR FOR ARDUINO
SparkFun Electronics
MCX JACK TO BNC RF CABLE ADAPTER
מק"ט יצרן # 1531
MCX JACK TO BNC RF CABLE ADAPTER
Adafruit Industries LLC
מק"ט יצרן # 3357
MUSIC MAKER FEATHERWING
Adafruit Industries LLC
מק"ט יצרן # 2886
FEATHER HEADER KIT FML
Adafruit Industries LLC
מק"ט יצרן # 2830
FEATHER STACKING HEADERS FML
Adafruit Industries LLC
מק"ט יצרן # IRLB8721PBF
MOSFET N-CH 30V 62A TO220AB
Infineon Technologies
מק"ט יצרן # OSTVN05A150
TERM BLK 5P SIDE ENT 2.54MM PCB
On Shore Technology Inc.
מק"ט יצרן # OSTVN06A150
TERM BLK 6P SIDE ENT 2.54MM PCB
On Shore Technology Inc.
מק"ט יצרן # PJ-102AH
CONN PWR JACK 2X5.5MM SOLDER
Same Sky (Formerly CUI Devices)
מק"ט יצרן # 1608
BREADBOARD GENERAL PURPOSE PTH
Adafruit Industries LLC
מק"ט יצרן # 104990000
ADDRESS LED STRIP SERIAL RGB 1M
Seeed Technology Co., Ltd
מק"ט יצרן # AP8GMCSH4-B
MEMORY CARD MICROSD 8GB CLASS 4
Apacer Memory America
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.