Maker.io main logo

Qwiic Micro Magnetometer

50

2022-11-08 | By SparkFun Electronics

License: See Original Project

Courtesy of SparkFun

Guide by ELL C

Introduction

The SparkFun Qwiic Micro MMC5983MA Magnetometer is a micro-sized, 0.75in. by 0.30in. sensor ‎that utilizes the highly sensitive triple-axis magnetometer by MEMSIC. We've attached the ‎magnetometer IC onto an incredibly small Qwiic board form factor that we like to call Qwiic Micro! ‎The MMC5983MA is capable of sensing down to 0.4mG, enabling a heading accuracy of ±0.5°. ‎The Qwiic MMC5983MA IMU communicates over I2C by default utilizing our handy Qwiic Connect ‎System, so no soldering is required to connect it to the rest of your boards.

‎Saturation is a problem for all mag sensors. The MMC5983MA has built-in degaussing circuitry to ‎clear any residual magnetization. Output rates of 1000Hz, ±8G FSR, and 18-bit resolution make the ‎MMC5983MA a phenomenal magnetic sensor for electronic compass applications.‎

SparkFun Micro Magnetometer - MMC5983MA (Qwiic)‎

Required Materials

To follow along with this tutorial, you will need the following materials. You may not need everything ‎though depending on what you have. Add it to your cart, read through the guide, and adjust the cart ‎as necessary.‎

Qwiic Micro Magnetometer - MMC5983MA Hookup Guide Wish List SparkFun Wish List

VIEW QWIIC MICRO MAGNETOMETER - MMC5983MA HOOKUP GUIDE WISH LIST ON ‎SPARKFUN.COM

Suggested Reading

If you aren’t familiar with the following concepts, we recommend checking out these tutorials before ‎continuing.‎

  • Logic Levels: Learn the difference between 3.3V and 5V devices and logic levels.‎

  • Accelerometer Basics: A quick introduction to accelerometers, how they work, and why they're ‎used.‎

  • I2C: An introduction to I2C, one of the main embedded communications protocols in use today.‎

  • Serial Terminal Basics: This tutorial will show you how to communicate with your serial devices ‎using a variety of terminal emulator applications.‎

Hardware Overview

The beautiful thing about this Qwiic board is that it is extremely simple. Let's dive in and have a look ‎at its features!‎

MMC5983MA

The MMC5983MA is an AEC-Q100 qualified, fully integrated 3-axis magnetic sensor with on-chip ‎signal processing and integrated I2C/SPI bus. It has superior dynamic range and accuracy with ±8G ‎FSR, 18bit operation, 0.4mG total RMS noise, and can enable heading accuracy of 0.5º. More ‎information can be found in the datasheet.‎

sensor_1

Qwiic Connector

Our Qwiic Ecosystem makes sensors pretty much plug and play. There's a Qwiic connector on the ‎side of the Qwiic Micro Magnetometer to provide power and I2C connectivity simultaneously. The ‎default I2C address is 0x30.‎

qwiic_2

Pins

We've broken out the interrupt and ground pins to PTH on either side of the board. The interrupt ‎pin is active high - writing “1” will enable the interrupt for completed measurements. Once a ‎measurement is finished, either magnetic field or temperature, an interrupt will be sent to the host.‎

pins_3

Jumpers

I2C

Like our other Qwiic boards, the Qwiic Micro Magnetometer comes equipped with pull-up resistors ‎on the clock and data pins. If you are daisy chaining multiple Qwiic devices, you will want to cut this ‎jumper; if multiple sensors are connected to the bus with the pull-up resistors enabled, the parallel ‎equivalent resistance will create too strong of a pull-up for the bus to operate correctly. As a ‎general rule of thumb, disable all but one pair of pull-up resistors if multiple devices are connected ‎to the bus. To disable the pull up resistors, use an X-acto knife to cut the joint between the two ‎jumper pads highlighted here.‎

jumpers_4

LED

If power consumption is an issue, cutting this jumper will disable the Power LED on the front of the ‎board.‎

led_5

Board Outline

This ultra-tiny Qwiic breakout board measures 0.75" x 0.30".‎

board_6

Hardware Hookup

Grab your Qwiic cable and plug one end into the RedBoard Qwiic and the other end into the Qwiic ‎Micro Magnetometer. Voila!‎

hookup_7

Software Setup and Programming

Note: Make sure you are using the latest stable version of the Arduino IDE on your desktop. ‎

If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE. If you ‎have not previously installed an Arduino library, please check out our installation guide.‎

We've written a simple Arduino library to quickly get started reading data from the Qwiic Micro ‎Magnetometer. Install the library through the Arduino Library Manager tool by searching ‎for "SparkFun MMC5983MA". Users who prefer to manually install it can get the library from ‎the GitHub Repository or download the ZIP by clicking the button below:‎

SPARKFUN QWIIC MICRO MAGNETOMETER - MMC5983MA ARDUINO LIBRARY

Example 1: I2C Simple Measurement

Now that we've got our library installed and our hardware all hooked up, let's look at some examples.‎

This first example just does some basic measurements. To find Example 1, go to File -‎‎> Examples -> SparkFun MMC5983MA Magnetometer Arduino Library -> Example1-‎I2C_Simple_measurement.‎

example_8

Make sure you have the correct board and port selected. For this tutorial, your selections should ‎look something like this:‎

port_9

Once you're ready to go, go ahead and hit the upload button (the right facing arrow button under ‎the "Edit" menu item). Once your code is uploaded, open the Serial Monitor and you'll see X, Y, and ‎Z values start printing out.‎

upload_10

Example 2: I2C Digital Compass

Example 2 shows how to compute the heading based on the basic X/Y/Z readings from the sensor ‎over Qwiic. To find this example, go to File -> Examples -> SparkFun MMC5983MA ‎Magnetometer Arduino Library -> Example2-I2C_Digital_compass.‎

example2_11

Make sure you have the correct board and port selected. For this tutorial, your selections should ‎look something like this:‎

correct_12

Once you're ready to go, go ahead and hit the upload button (the right facing arrow button under ‎the "Edit" menu item). Once your code is uploaded, open the Serial Monitor and you'll see compass ‎readings start printing out.‎

code_13

If you look at the above image, you'll see where I abruptly changed the direction the sensor was ‎pointing.‎

Example 3: I2C Continuous Measurement

Example 3 demonstrates how to use interrupts to quickly read the sensor instead of polling. To find ‎this example, go to File -> Examples -> SparkFun MMC5983MA Magnetometer Arduino ‎Library -> Example3-I2C_Continuous_measurement.‎

example3_14

Make sure you have the correct board and port selected. For this tutorial, your selections should ‎look something like this:‎

selections_15

Once you're ready to go, go ahead and hit the upload button (the right facing arrow button under ‎the "Edit" menu item). Once your code is uploaded, open the Serial Monitor and you'll see compass ‎readings start printing out.‎

edit_16

Examples 4 and 5‎

A Note on Examples 4 and 5: This library is shared with the SparkX Breakout Board using the ‎same MMC5983MA chip. However, due to the tiny size of this Micro Breakout Board, SPI ‎functionality is not available for the Qwiic Micro Magnetometer. The two SPI examples included with ‎the Arduino Library are for use with the SparkX board only.‎

Troubleshooting

Need help? ‎

If your product is not working as you expected or you need technical assistance or information, ‎head on over to the SparkFun Technical Assistance page for some initial troubleshooting. ‎

If you don't find what you need there, the SparkFun Forums are a great place to find and ask for ‎help. If this is your first visit, you'll need to create a Forum Account to search product forums and ‎post questions.‎

Resources and Going Further

Now that you've successfully got your Qwiic Micro Magnetometer up and running, it's time to ‎incorporate it into your own project!‎

For more information, check out the resources below:‎

מק"ט יצרן # 15123
REDBOARD QWIIC ATMEGA328 EVAL BD
SparkFun Electronics
מק"ט יצרן # 17260
FLEXIBLE QWIIC CABLE - 50MM
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.