Maker.io main logo

Qwiic MultiPort Hookup Guide

86

2022-02-03 | By SparkFun Electronics

License: See Original Project

Courtesy of SparkFun

Guide by BBOYHO

Introduction

The SparkFun Qwiic Multiport adds additional ports to boards that have only one Qwiic port on their I2C bus. Once added, you can use it as a hub to add as many I2C devices to the bus as you need [1] ! You can also use the board as an alternative to a daisy chained configuration.

SparkFun Qwiic MultiPort

 

Note: Technically, there are limitations to how many boards that you can add to the bus. You may need to adjust pull-up resistors depending on what is connected. This is usually about 7x boards. You may also need to disconnect 3.3V to certain devices and inject power depending on the total power required. Keep in mind the Qwiic cable wires are small and have a max current of about 226mA.

Required Materials

To follow along with this tutorial, you will need a microcontroller or single board computer with a Qwiic connector. You will also need a Qwiic cable and a way to power the board. You may not need everything though depending on what you have. Add it to your cart, read through the guide, and adjust the cart as necessary.

Besides having the Qwiic MultiPort in your cart, here are the parts if you decide to go with a microcontroller. You can easily swap out the microcontroller depending on your project's needs with MicroMod. Make sure to include the Qwiic-enabled device in your cart as well!

Here are the parts if you decide to go with a single board computer. The Qwiic SHIM kit is a great starting point if you do not have a Qwiic-enabled device in mind.

Suggested Reading

If you aren't familiar with the MicroMod ecosystem, we recommend reading here for an overview. We recommend reading here for an overview if you decide to take advantage of the Qwiic connector.

MicromodQwiic_1

MicroMod Ecosystem                       Qwiic Connect System

We also recommend taking a look through the following tutorials if you are not familiar with the concepts covered in them:

  • Logic Levels: Learn the difference between 3.3V and 5V devices and logic levels.

  • I2C: An introduction to I2C, one of the main embedded communications protocols in use today.

  • Raspberry Pi 4 Kit Hookup Guide: Guide for hooking up your Raspberry Pi 4 Model B basic, desktop, or hardware starter kit together.

  • Getting Started with MicroMod: Dive into the world of MicroMod - a compact interface to connect a microcontroller to various peripherals via the M.2 Connector!

Hardware Overview

The board is a simple design that allows you to connect devices to the I2C bus easily with the Qwiic Connect System. Power and logic levels are set to 3.3V. Make sure to use a logic level converter if your board uses a voltage higher than 3.3V.

Wirecolor_2

Qwiic Connectors

There are 4x Qwiic connectors populated on the board.

Board_3

LED and Jumper

In addition to the connectors, there is an LED to indicate when power is available on the I2C bus. On the back, there is a jumper in case you would like to disable the LED.

Front_3

Front of Board

Back_4

Back of Board

Mounting Holes

There are 2x mounting holes included on the board.

Holes_5

Board Dimensions

Below are the board dimensions. The overall size of the board is 1.00" x 1.00". Each connector extending from the center has a width of about 0.30". As stated earlier, this board has 2x mounting holes located around the center.

Dimensions_6

Hardware Assembly

Expanding on Boards with One Qwiic Connector

Depending on the design, there may only be enough room for one Qwiic connector. Below are a few of these boards from the SparkFun catalog.

If you are looking to connect more than one device with one Qwiic connector to your development board, you will just need a Qwiic MultiPort board and an additional Qwiic cable for each device.

Connect_7

Alternative to a Daisy Chained Configuration

The Qwiic MultiPort can also be used as a hub so that you do not have to place the board with one Qwiic connector at the end of the daisy chain. Below is an example with the Qwiic SHIM Kit for Raspberry Pi. Instead of having the Qwiic 9DoF between the Pi and Qwiic SerLCD.

Daisy_8

Mounting with Standoffs

The two boards can be mounted with standoffs for a secure connection. Below is the Qwiic Micro (SAMD21), Qwiic MultiPort, Qwiic GPS (ZOE-M8Q), and a GPS antenna (W3062A) connected stacked on top of each other. They are all connected to the Qwiic SerLCD connect using Qwiic cables (with the exception of the antenna).

Standoffs_9

 

Resources and Going Further

Now that you've connected your Qwiic MultiPort, it's time to incorporate it into your own project! For more information, check out the resources below:

מק"ט יצרן # 15081
QWIIC CABLE KIT
SparkFun Electronics
מק"ט יצרן # 16791
MICROMOD SAMD51 PROCESSOR
SparkFun Electronics
מק"ט יצרן # 16885
MICROMOD ATP CARRIER BOARD
SparkFun Electronics
מק"ט יצרן # 14743
CABLE A PLUG TO C PLUG 3.28'
SparkFun Electronics
מק"ט יצרן # 16987
SPARKFUN QWIIC SHIM KIT FOR RASP
SparkFun Electronics
מק"ט יצרן # 15801
POWER DELIVERY USB-C QWIIC
SparkFun Electronics
מק"ט יצרן # 15193
SPARKFUN GPS BREAKOUT - ZOE-M8Q
SparkFun Electronics
מק"ט יצרן # 16396
SPARKFUN 16X2 SERLCD - RGB BACKL
SparkFun Electronics
מק"ט יצרן # 16397
SPARKFUN 16X2 SERLCD - RGB TEXT
SparkFun Electronics
מק"ט יצרן # 17731
QWIIC SOIL MOISTURE SENSOR
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.