Maker.io main logo

Qwiic Pressure Sensor (BMP581) Hookup Guide

205

2022-09-22 | By SparkFun Electronics

License: See Original Project

Courtesy of SparkFun

Guide by EL DUDERINO

Introduction

The SparkFun Pressure Sensor - BMP581 (Qwiic) and Micro Pressure Sensor - BMP581 ‎‎(Qwiic) feature the BMP581 absolute pressure sensor from Bosch Sensortec. The BMP581 boasts ‎exceptional resolution and accuracy and uses on-chip linearization and temperature compensation ‎to provide true absolute data for pressure and temperature.‎

SparkFun Pressure Sensor - BMP581 (Qwiic)‎

SparkFun Micro Pressure Sensor - BMP581 (Qwiic)‎

 

This guide will take you through the hardware present on these Qwiic breakouts, connecting them ‎to a Qwiic circuit and using the BMP581 with the SparkFun BMP581 Arduino Library.‎

Required Materials

To follow along with this guide, you will need a microcontroller to communicate with the BMP581. ‎Below are a few options that come Qwiic-enabled out of the box:‎

If your chosen microcontroller is not already Qwiic-enabled, you can add that functionality with one ‎or more of the following items:‎

You will also need at least one Qwiic cable to connect your sensor to your microcontroller.‎

Recommended Reading

If you aren't familiar with the Qwiic system, we recommend reading here for an overview.‎

qwiic_1

We would also recommend taking a look at the following tutorials if you aren't familiar with them. If ‎you are using one of the Qwiic Shields listed above, you may want to read through their respective ‎Hookup Guides as well before going through this guide for this BMP581 Qwiic breakout.‎

Hardware Overview

In this section we'll take a closer look at the hardware present on these Qwiic Pressure Sensor - ‎BMP581 breakouts.‎

BMP581 Pressure Sensor

The BMP581 is an extremely precise and versatile absolute pressure sensor from Bosch Sensortec ‎that uses on-chip linearization and temperature compensation to provide true absolute pressure and ‎temperature data.‎

sensor_2

sensor_3

The BMP581 features a wide pressure sensing range (30 to 125 kPa), pressure data resolution of ‎‎1/64 Pa with excellent accuracy across the sensing range (± 0.5 hPa (max)) as well as output data ‎rates up to 622 Hz. All of this in a package size of just 2.0 mm2!‎

The sensor accepts a supply voltage of 1.71V to 3.6V though the board runs the sensor at 3.3V. ‎The BMP581 includes a FIFO buffer that can store up to 32 samples, user-programmable low-pass ‎filtering as well as configurable IIR settings to help offset noise created by ambient changes in ‎pressure such as doors/windows opening or closing or wind passing by the sensor. Lastly, the ‎BMP581 even has 6 bytes of user-programmable non-volatile memory.‎

The table below outlines some of the BMP581's sensing parameters. For a full overview of the ‎BMP581, refer to the datasheet.‎

table_4

Pressure Noise1

Output Data Rate1

The sensor has seven operating modes outlined in the table below. For complete information on ‎the power modes and configuration settings available or required for them, refer to section 4.3 of ‎the datasheet:‎

table_5

‎1. Refer to section 4.4.2 of the BMP581 datasheet for more information on how oversampling ‎settings/ratios affect pressure RMS noise and output data rate.‎

Communication Interfaces - I2C & SPI

The standard size Qwiic Pressure Sensor (BMP581) communicates over I2C by default but also ‎supports using the BMP581 over SPI. The Qwiic Micro version only supports I2C over the Qwiic ‎connector on the board.‎

sensor_6

sensor_7

The breakout routes the I2C interface to a pair of Qwiic connectors as well as a 0.1"-spaced PTH ‎header for users who prefer a traditional, soldered connection. This PTH header shares the SPI ‎connections and also includes the Interrupt pin.‎

The board sets the BMP581's I2C address to 0x77 by default. Adjust the ADR jumper to change to ‎the alternate address (0x76) or leave it completely open to use the SPI interface (Standard size ‎only). More information on this jumper in the Solder Jumpers section below.‎

Solder Jumpers

If you have never worked with solder jumpers and PCB traces before or would like a quick ‎refresher, check out our How to Work with Solder Jumpers and PCB Traces tutorial for detailed ‎instructions and tips.‎

The standard size breakout has four solder jumpers labeled: I2C, ADR, CSB and LED. The micro ‎size breakout has all but the CSB jumper since the micro version does not support SPI.‎

breakout_8

breakout_9

The I2C jumper connects a pair of 2.2kΩ resistors to the SDA/SCL lines. Leave these enabled ‎unless you have a large number of I2C devices on the same bus.‎

The ADR jumper sets the I2C address of the BMP581 to 0x47 by default (0x46 alternate). It also ‎controls whether it operates via I2C or SPI. Open the jumper completely to set the BMP581 to ‎communicate via SPI.‎

The CSB jumper pulls the Chip Select pin to VDD (3.3V) through a 10kΩ resistor. Open the jumper ‎to disable the pullup.‎

The LED jumper completes the Power LED circuit. Open the jumper to disable the Power LED if ‎desired.‎

Board Dimensions

The standard size Qwiic breakout matches the 1.0" x 1.0" (25.4mm x 25.4mm) form factor for Qwiic ‎breakouts with two mounting holes that fit a size 4-40 screw. The Micro version of this breakout ‎matches the Qwiic Micro form factor and measures 0.75" x 0.30" (24.65mm x 7.62mm) and has one ‎mounting hole that fits a size 4-40 screw.‎

board_10

board_11

Hardware Assembly

Now that we're familiar with the Qwiic Pressure Sensor (BMP581), we can start assembling our ‎circuit.‎

Qwiic/I2C Assembly

The fastest and easiest way to get started using the breakout is to connect the Qwiic connector on ‎the breakout to a Qwiic-enabled development board like the SparkFun RedBoard Artemis with a ‎Qwiic cable and as shown in the image below.‎

assembly_12

If you would prefer a more secure and permanent connection with the Standard size version, you ‎can solder headers or wire to the PTH header on the board.‎

SPI Assembly (Standard Size Only)‎

Setting the breakout up to communicate with the sensor over SPI requires completely opening the ‎ADR jumper and we recommend soldering to the PTH header to make the connections. If you are ‎not familiar with through-hole soldering, take a read through this tutorial:‎

tutorial_13

How to Solder: Through-Hole Soldering

This tutorial covers everything you need to know about through-hole soldering.‎

Along with tools for soldering, you'll need either some hookup wire or headers and jumper wires. ‎Sever the trace between the "Center" and "Right" pads of the ADR jumper to tell the BMP581 to ‎communicate using SPI. After opening this jumper, connect the BMP581 to your controller's SPI ‎pins.‎

connect_14

Remember, the BMP581 operates at 3.3V logic so make sure to connect to a board running at the ‎same logic level like the RedBoard Artemis or use a level shifter to adjust it to a safe voltage.‎

SparkFun BMP581 Arduino Library

Note: This library assumes you are using the latest version of the Arduino IDE on your desktop. If ‎this is your first time using Arduino, please review our tutorial on installing the Arduino IDE. If you ‎have not previously installed an Arduino library, please check out our installation guide.‎

The SparkFun BMP581 Arduino Library is based off the API for the sensor from Bosch. Install the ‎library through the Arduino Library Manager tool by searching for "SparkFun BMP581". Users ‎who prefer to manually install the library can download a copy of it from the GitHub repository by ‎clicking the button below:‎

SPARKFUN BMP581 ARDUINO LIBRARY (ZIP)‎

Heads Up! We recommend choosing a development board with plenty of available RAM like the ‎RedBoard Artemis shown in the Hardware Assembly section if you want to use the FIFO buffer as it ‎is read all at once which causes some microcontrollers like the ATMega328 on the RedBoard/Uno ‎to run out of RAM after just a few samples. All other use cases of the Arduino Library will work with ‎most microcontrollers.‎

Library Functions

The list below outlines and describes the functions available in the SparkFun BMP581 Library:‎

  • int8_t beginI2C(uint8_t address = BMP581_I2C_ADDRESS_DEFAULT, TwoWire& wirePort = ‎Wire); - Initialize the BMP581 at the default I2C address on the specified Wire port.

  • int8_t beginSPI(uint8_t csPin, uint32_t clockFrequency = 100000); - Initialize the ‎BMP581 over SPI using the defined Chip Select pin and set clock frequency (default 100kHz).

  • int8_t init(); - Initialize the BMP581 sensor. The begin function handles this automatically.‎

  • int8_t setMode(bmp5_powermode mode); - Set the operating mode. Valid options are: . The ‎begin function handles this automatically.‎

  • int8_t getMode(bmp5_powermode* mode); - Returns the value set for the operating mode.‎

  • int8_t enablePress(uint8_t pressEnable); - Enable pressure and temperature sensing. The ‎begin function handles this automatically.‎

Sensor Data and Settings

  • int8_t getSensorData(bmp5_sensor_data* data); - Pulls pressure and temperature data from ‎the sensor.

  • int8_t setODRFrequency(uint8_t odr); - Set the output data rate frequency.

  • int8_t getODRFrequency(uint8_t* odr); - Returns the value set for the output data rate ‎frequency.

  • int8_t setOSRMultipliers(bmp5_osr_odr_press_config* config); - Set the oversampling ‎multiplier.

  • int8_t getOSRMultipliers(bmp5_osr_odr_press_config* config); - Returns the value stored ‎for the oversampling multiplier.‎

  • int8_t getOSREffective(bmp5_osr_odr_eff* osrOdrEffective);

  • int8_t setFilterConfig(bmp5_iir_config* iirConfig); - Set the IIR filter configuration.‎

  • int8_t setOORConfig(bmp5_oor_press_configuration* oorConfig); - Set the OOR (Out-of-‎Range) configuration.‎

  • int8_t setInterruptConfig(BMP581_InterruptConfig* config); - Set the Interrupt Settings ‎‎(output mode, level, latch and data ready). Refer to Example 3 - Interrupts in the Arduino ‎Library for a detailed demonstration of setting and using the Interrupt pin.‎

  • int8_t getInterruptStatus(uint8_t* status); - Returns the settings for the Interrupt.‎

FIFO Buffer Control

Refer to Example 6 - FIFO Buffer in the Arduino library for a detailed example of setting and using ‎the FIFO buffer.‎

  • int8_t setFIFOConfig(bmp5_fifo* fifoConfig); - Set the FIFO buffer settings.

  • int8_t getFIFOLength(uint8_t* numData); - Set the number of samples stored in the FIFO ‎buffer at a time.‎

  • int8_t getFIFOData(bmp5_sensor_data* data, uint8_t numData); - Pull the FIFO data ‎stored on the BMP581.

  • int8_t flushFIFO(); - Flush the FIFO buffer.‎

NVM Control

  • int8_t readNVM(uint8_t addr, uint16_t* data); - Read data stored in the non-volatile ‎memory.‎

  • int8_t writeNVM(uint8_t addr, uint16_t data); - Write data to the non-volatile memory.‎

Error Codes

Most of the functions in this list return specific error codes (instead of a true/false boolean) if called ‎properly. The examples demonstrate how to set up and call error codes. For information on the ‎error codes, refer to the BMP581 defs.h file in the BMP581 API.‎

Arduino Examples

With the Arduino library installed, it's time to upload some code to use the BMP581. In this section ‎we take a closer look at several of the examples included with the library.‎

Example 1 - Basic Readings (I2C)‎

The first example initializes the BMP581 to communicate over I2C with default settings. Open the ‎example by navigating to File Examples > SparkFun BMP581 Arduino Library > ‎Example_1_Basic_ReadingsI2C. Select your Board and Port and click upload. Open the serial ‎monitor after the upload completes with the baud set to 115200 to watch pressure data (in Pascals) ‎print out.‎

If you have switched to the alternate address, comment/uncomment the line with the correct value:‎

Copy Code
uint8_t i2cAddress = BMP581_I2C_ADDRESS_DEFAULT; // 0x47
//uint8_t i2cAddress = BMP581_I2C_ADDRESS_SECONDARY; // 0x46

The code attempts to initialize the sensor with default settings in I2C at the specified address and ‎prints out an error message if it cannot initialize properly:‎

Copy Code
while(pressureSensor.beginI2C(i2cAddress) != BMP5_OK)
{
    // Not connected, inform user
    Serial.println("Error: BMP581 not connected, check wiring and I2C address!");

    // Wait a bit to see if connection is established
    delay(1000);
}

After initializing, the main loop polls the BMP581 for pressure and temperature data every second. ‎If polling for data fails, the code will print out an error code for debugging. Try moving the sensor ‎up and down and you should see noticeable differences in pressure readings with just a few inches ‎of movement.‎

Copy Code
void loop()
{
    // Get measurements from the sensor
    bmp5_sensor_data data = {0};
    int8_t err = pressureSensor.getSensorData(&data);

    // Check whether data was acquired successfully
    if(err == BMP5_OK)
    {
        // Acquisistion succeeded, print temperature and pressure
        Serial.print("Temperature (C): ");
        Serial.print(data.temperature);
        Serial.print("\t\t");
        Serial.print("Pressure (Pa): ");
        Serial.println(data.pressure);
    }
    else
    {
        // Acquisition failed, most likely a communication error (code -2)
        Serial.print("Error getting data from sensor! Error code: ");
        Serial.println(err);
    }

    // Only print every second
    delay(1000);
}

Example 3 - Interrupts

Example 3 shows how to set up and use the out-of-range (OOR) interrupt condition on the ‎BME581 to trigger interrupt routines on an attached microcontroller. If you're not familiar with ‎processor interrupts, this tutorial gives a good primer on using them with Arduino.‎

When assembling the interrupt circuit, make sure to connect the INT pin on the breakout to a pin ‎capable of accepting external interrupts. The code sets up D2 as the interrupt pin so adjust this line ‎if your microcontroller does not support external interrupts on that pin:‎

Copy Code
// Pin used for interrupt detection
int interruptPin = 2;

The code creates a flag to know when an interrupt condition occurs and sets the out-of-range ‎condition specifications to ±50 Pa with a center value of 84000 Pa:‎

Copy Code
language:c    
// Flag to know when interrupts occur
volatile bool interruptOccurred = false;

// OOR range specification
uint32_t oorCenter = 84000;
uint8_t oorWindow = 50;

Example 7 - Non-Volatile Memory

As we covered in the Hardware Overview section, the BMP581 includes 6 bytes of non-volatile ‎memory (NVM) you can write to and read from. Example 7 demonstrates how to interact with the ‎NVM.‎

Along with the other standard definitions and calls, we need to set the data to write to the NVM. You ‎can store any 6 bytes of data but in this example, we'll store some characters:‎

Copy Code
char dataToWrite[] = "Hello!";

After initializing the sensor in the BMP581 and verifying it is connected, the code attempts to write ‎the data declared above to the NVM. If this is successful, the code then prints out the stored data:‎

Copy Code
Serial.println("Writing data to NVM: ");
Serial.println(dataToWrite);

// The BMP581 contains non-volatile memory (NVM) that is primarily used for
// calibration data internally by the sensor. However 6 bytes are user programmable,
// stored in 3 2-byte locations (0x20 - 0x22).
uint16_t dataIndex = 0;
for(uint8_t addr = BMP5_NVM_START_ADDR; addr <= BMP5_NVM_END_ADDR; addr++)
{
    uint16_t data = dataToWrite[dataIndex] | (dataToWrite[dataIndex+1] << 8);
    dataIndex += 2;

    pressureSensor.writeNVM(addr, data);
}

Serial.println("Data read back from NVM: ");

// Now we can read back the data and display it
for(uint8_t addr = BMP5_NVM_START_ADDR; addr <= BMP5_NVM_END_ADDR; addr++)
{
    uint16_t data = 0;
    pressureSensor.readNVM(addr, &data);
    char first = data & 0xFF;
    char second = (data >> 8) & 0xFF;
    Serial.print(first);
    Serial.print(second);
}

Example 8 - Low Power

Example 8 is a demo of how to reduce power in a circuit with the BMP581 using the Deep Standby ‎and Forced modes along with the BMP581's interrupt pin. The interrupt pin can be used to wake a ‎microcontroller whenever the BMP581 takes a reading and fires the interrupt. The code uses D5 as ‎the interrupt pin so adjust this line of code if your microcontroller does not support external ‎interrupts on that pin:‎

Copy Code
int interruptPin = 5;

The code initializes the sensor on the I2C bus, sets it into Deep Standby mode and enables the ‎interrupt pin to fire whenever data is ready (when the sensor is put into Forced Mode):‎

Copy Code
err = pressureSensor.setMode(BMP5_POWERMODE_DEEP_STANDBY);
if(err != BMP5_OK)
{
    // Interrupt settings failed, most likely a communication error (code -2)
    Serial.print("Set mode failed! Error code: ");
    Serial.println(err);
}

The main loop includes a one second delay before transitioning the sensor from Deep Standby to ‎Forced Mode. The delay can be replaced with a power sequence setting the microcontroller into a ‎low power mode.‎

After transitioning to Forced Mode, the code performs a series of checks in case the measurement ‎ready condition timed out and if the interrupt is ready or the get status call failed. Once the checks ‎have passed, the code checks if the interrupt status matches the Data Ready state, pulls ‎temperature and pressure data from the BMP581 and prints it over serial:‎

Copy Code
if(interruptStatus & BMP5_INT_ASSERTED_DRDY)
{
    // Get measurements from the sensor
    bmp5_sensor_data data = {0};
    int8_t err = pressureSensor.getSensorData(&data);

    // Check whether data was acquired successfully
    if(err == BMP5_OK)
    {
        // Acquisistion succeeded, print temperature and pressure
        Serial.print("Temperature (C): ");
        Serial.print(data.temperature);
        Serial.print("\t\t");
        Serial.print("Pressure (Pa): ");
        Serial.println(data.pressure);
    }
    else
    {
        // Acquisition failed, most likely a communication error (code -2)
        Serial.print("Error getting data from sensor! Error code: ");
        Serial.println(err);
    }
}
else
{
    Serial.println("Wrong interrupt condition!");
}

Example 9 - Fast Measurements

The final example demonstrates how to use continuous mode for max speed measurements. This ‎example uses Continuous Mode where the sensor performs measurements as soon as the ‎previous measurement finishes. This example is a bit different from the other examples as it only ‎reports the number of measurements taken during a one second interval and does not print the ‎actual data measured by the sensor.‎

The code sets the oversampling ratio to 1x so the sensor can perform measurements at up to ‎‎500Hz in Continuous Mode and configures the Interrupt pin to trigger an interrupt every time a ‎measurement is performed:‎

Copy Code
err = pressureSensor.setMode(BMP5_POWERMODE_CONTINOUS);
if(err != BMP5_OK)
{
    // Interrupt settings failed, most likely a communication error (code -2)
    Serial.print("Set mode failed! Error code: ");
    Serial.println(err);
}

// Configure the BMP581 to trigger interrupts whenever a measurement is performed
BMP581_InterruptConfig interruptConfig =
{
    .enable   = BMP5_INTR_ENABLE,    // Enable interrupts
    .drive    = BMP5_INTR_PUSH_PULL, // Push-pull or open-drain
    .polarity = BMP5_ACTIVE_HIGH,    // Active low or high
    .mode     = BMP5_PULSED,         // Latch or pulse signal
    .sources  =
    {
        .drdy_en = BMP5_ENABLE,        // Trigger interrupts when data is ready
        .fifo_full_en = BMP5_DISABLE,  // Trigger interrupts when FIFO is full
        .fifo_thres_en = BMP5_DISABLE, // Trigger interrupts when FIFO threshold is reached
        .oor_press_en = BMP5_DISABLE   // Trigger interrupts when pressure goes out of range
    }
};

The main loop checks if it is time to print (one second) and then prints the number of ‎measurements taken during the print period:‎

Copy Code
if(millis() > lastPrintTime + printPeriod)
    {
        // Print out number of measurements this period
        Serial.print("Number of measurements in ");
        Serial.print(printPeriod);
        Serial.print("ms: ");
        Serial.println(measurementsThisPeriod);

        // Reset number of measurements for next period
        measurementsThisPeriod = 0;

        // Increment last print time
        lastPrintTime += printPeriod;
    }

Troubleshooting

Pressure Data as Altitude

If you want to use the pressure data from the BMP581 to determine the altitude of the sensor, refer ‎to this section of our MPL3115A2 Breakout Hookup Guide for more information on how to ‎manipulate and correctly interpret pressure data.‎

Error Codes

Most of the functions in this list return specific error codes (instead of a true/false boolean) if called ‎properly. The examples demonstrate how to set up and call error codes. For information on the ‎error codes, refer to the BMP581 defs.h file in the BMP581 API.‎

General Troubleshooting

Not working as expected and need help?

If you need technical assistance and more information on a product that is not working as you ‎expected, we recommend heading on over to the SparkFun Technical Assistance page for some ‎initial troubleshooting.

SPARKFUN TECHNICAL ASSISTANCE PAGE‎

If you don't find what you need there, the SparkFun Forums are a great place to find and ask for ‎help. If this is your first visit, you'll need to create a Forum Account to search product forums and ‎post questions.

CREATE NEW FORUM ACCOUNT     LOG INTO SPARKFUN FORUMS

Resources and Going Further

For more information about the SparkFun Pressure Sensor - BMP581 (Qwiic and Qwiic Micro) ‎check out the following resources:‎

 

מק"ט יצרן # 20170
SPARKFUN PRESSURE SENSOR - BMP58
SparkFun Electronics
מק"ט יצרן # 20171
SPARKFUN MICRO PRESSURE SENSOR -
SparkFun Electronics
מק"ט יצרן # 14713
THING PLUS - SAMD51
SparkFun Electronics
מק"ט יצרן # 15081
QWIIC CABLE KIT
SparkFun Electronics
מק"ט יצרן # 14495
QWIIC ADAPTER
SparkFun Electronics
מק"ט יצרן # 14352
QWIIC SHIELD FOR ARDUINO
SparkFun Electronics
מק"ט יצרן # 16790
QWIIC SHIELD FOR THING PLUS
SparkFun Electronics
מק"ט יצרן # 14427
QWIIC CABLE - 100MM
SparkFun Electronics
מק"ט יצרן # 14426
QWIIC CABLE - 50MM
SparkFun Electronics
מק"ט יצרן # 14429
QWIIC CABLE - 500MM
SparkFun Electronics
מק"ט יצרן # 14428
QWIIC CABLE - 200MM
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.