Maker.io main logo

Qwiic SHIM for Raspberry Pi Hookup Guide

166

2020-02-20 | By SparkFun Electronics

License: See Original Project Raspberry Pi SBC

Courtesy of SparkFun

Introduction

The SparkFun Qwiic SHIM for Raspberry Pi is a small, easily removable breakout to add a Qwiic connector to your Raspberry Pi. The SHIM (short for Shove Hardware in the Middle) design allows you to plug directly to the Pi's I2C bus with no soldering required and the thin PCB design allows for it to be sandwiched on your Pi GPIO with other HATS. The Qwiic SHIM works great when you do not need the full capabilities of the Qwiic pHAT for Raspberry Pi or if you want to add a Qwiic connector to your Pi but do not have room for yet another HAT.

 

SparkFun Qwiic SHIM for Raspberry Pi

Required Materials

To follow along with this tutorial, you will need the following materials. You may not need everything though depending on what you have. Add it to your cart, read through the guide, and adjust the cart as necessary.

Single Board Computer

You will need Raspberry Pi with 2x20 male headers installed.

A Pi Zero W will also work but you will need to make sure to solder some male headers to it.

Or you could connect it to any single board computer (like the NVIDIA Jetson Nano) that utilizes the 40-pin Raspberry Pi GPIO header footprint.

Qwiic Board

Now you probably wouldn't buy the Qwiic SHIM if you didn't have any Qwiic products to use with it, right? If you don't have any Qwiic products, the following might not be a bad place to start.

Finally, you'll need our handy Qwiic cables to easily connect sensors to your Qwiic SHIM. Below are a few options.

Required Setup Tools

If you are using your Pi (or other single-board computer) as a desktop, these peripherals are required:

  • USB Mouse

  • USB Keyboard

  • HDMI monitor/TV

  • 5V Power Supply

Suggested Reading

If you aren't familiar with the Qwiic system, we recommend reading here for an overview of everything Qwiic:

system_2

We would also recommend taking a look at the following tutorials if you aren't familiar with the content covered in them.

Hardware Overview

The Qwiic SHIM uses a unique friction-based connector that wedges itself onto the GPIO header for a secure, solderless connection. As you would expect, it has a single Qwiic connector that connects to your Pi's I2C bus (SDA, SCL, 5V and Ground). The SHIM also has a 3.3V regulator so it will work with all Qwiic devices.

top_view_3

Top View Photo of Qwiic SHIM

Press Fit Header

The Press Fit Header on the Qwiic SHIM allows you to easily place the Qwiic SHIM on to your Pi (or other Single-Board Computer with the Pi GPIO) aligning the square pin on the Qwiic SHIM with Pin 1 of your GPIO. Pin one on the GPIO can be identified by the square pin or the beveled corner on the silkscreen. We will cover that in more detail in the Hardware Hookup section.

header_4

Press Fit Header

Voltage Regulator

For you savvy readers out there, you may wonder why not just connect directly to the 3.3V rail on the Pi GPIO? A simple answer is the Pi's 5V rail is able to source more current than the 3.3V rail so the regulator allows you to connect more devices to the I2C bus without needing to worry about overtaxing your Pi. The on board AP2112K 3.3V regulator provides a clean 3.3V out for all attached Qwiic devices and can source up to 600mA@3.3V so you should have plenty of available current for your Qwiic project.

voltage_5

Voltage Regulator

Board Dimensions

eagle_6

Eagle File Photo with dimensions

Hardware Hookup

Getting started with the Qwiic SHIM is a snap (well, actually it's more like a push but you get the idea). Making sure to align the Qwiic SHIM's Pin 1 with Pin 1 on your Pi's GPIO header, press the Qwiic SHIM down onto the header. Pin 1 on both the Qwiic SHIM and the Pi GPIO will be marked with a square pin. There is also a beveled corner on the Pi GPIO header indicating Pin 1 from the top of your Pi. That's it! With the SHIM in place you can now attach all your Qwiic devices to your Pi with space to spare for other Pi HATs.

Warning! When connecting the Qwiic SHIM to your GPIO header, make sure to align it properly with Pin 1. If the Qwiic SHIM is not aligned properly (either if it is upside down or not aligned on the correct pins) you can short your 5V rail to Ground!

config_7

GPIO Configuration for old and new model Raspberry Pi from the Raspberry Pi GPIO Tutorial.

With your Qwiic SHIM mounted on your Pi it should look like this:

Qwiic SHIM mounted on a Pi 4

Qwiic SHIM mounted on a Pi 4

Qwiic SHIM mounted on a Pi Zero W

Qwiic SHIM mounted on a Pi Zero W

With the Qwiic SHIM in place, you can now stack all the HATs you would like on top. With a HAT on top of the SHIM, the press fit header will make an even better connection and the thin PCB allows any HAT to still connect fully to the GPIO header.

breakout_9

The Qwiic SHIM is seen here nicely wedged by the SparkFun Pulsed Radar Breakout

hat_10

And here you can see it shoved in the middle with the SparkFun Pi Servo HAT.

Note: The Qwiic SHIM can also be connected in the same way with single board computers (like the NVIDIA Jetson Nano or the Google Coral) that utilize the 40-pin Raspberry Pi header footprint. Just remember to make sure you are aligning it properly!

Setting up I2C on Raspberry Pi

OS and Library Install

If you're starting from scratch, with a blank microSD card, you'll want to install Raspbian. If you've already got a working Raspbian system, skip ahead to step 3.

  1. Download the latest version of the NOOBS image. As of this writing, that is version 3.2.1.

  2. Follow the official installation instructions.

  3. Follow the Wiring Pi Instructions to get git, update and upgrade your Raspbian packages, then install WiringPi.

Be patient -- each of these steps takes a while.

Once you've got wiringPi installed, run the gpio commands shown below.

Copy Code
>gpio -v
>gpio readall

It should respond with some information about the wiringPi version and the Pi that its running on, then draw a table illustrating the configuration for the pins in the 40-pin connector.

Configuration

Like the SPI peripheral, I2C is not turned on by default. Again, we can use raspi-config to enable it.

  1. Run sudo raspi-config

  2. Use the down arrow to select 5 Interfacing Options

  3. Arrow down to P5 I2C

  4. Select yes when it asks you to enable I2C

  5. Select OK and then Finish

Once you return to terminal, enter this command:

Copy Code
>ls /dev/*i2c*

The Pi should respond with:

Copy Code
/dev/i2c-1

Which represents the user-mode I2C interface.

Utilities

There is a set of command-line utility programs that can help get an I2C interface working. You can get them with the apt package manager.

Copy Code
sudo apt-get install -y i2c-tools

In particular, the i2cdetect program will probe all the addresses on a bus, and report whether any devices are present. Call i2cdetect -y 1 to probe the first I2C bus, which is what the Qwiic SHIM is connected to.

Copy Code
pi@raspberrypi:~/$ i2cdetect -y 1
     0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f
00:          -- -- -- -- -- -- -- -- -- -- -- -- --
10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
60: 60 -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
70: -- -- -- -- -- -- -- --

This map indicates that there is a peripheral at address 0x60. We can read and write its registers using the i2cget, i2cset, and i2cdump commands.

Qwiic Py Drivers

Now that you have I2C set up on your Pi, you can start programming your Qwiic devices on your Pi or if you'd like to start with some examples, we have a host of Python drivers for Qwiic breakouts available in the GitHub repository linked below. You can read more about Python for the SparkFun Qwiic system in this blog post.

SPARKFUN QWIIC PY GITHUB REPO

Resources and Going Further

For more information, check out the resources below:

But I Already Have Sensors!

If you already have a handful of SparkFun sensors and parts? SparkFun has been putting our standard GND/VCC/SDA/SCL pinout on all our I2C boards for many years. This makes it possible to attach a Qwiic Adapter that will get your SparkFun I2C sensor or actuator onto the Qwiic system.

Here is the list of the boards that have the standard I2C pinout and will work with the Qwiic adapter board:

  • 9DoF Stick IMU - LSM9DS1

  • 9DoF IMU - MPU-9250

  • 6DoF IMU - LSM303C

  • 6DoF IMU - LSM6DS3

  • Triple Axis Accelerometer - LIS3DH

  • Triple Axis Magnetometer - MAG3110

  • Triple Axis Magnetometer - MLX90393

  • Compass Module - HMC6343

  • Atmospheric Sensor - BME280

  • Barometric Pressure Sensor - MS5803-14BA

  • Barometric Pressure Sensor - T5403

  • Humidity and Temperature Sensor - Si7021

  • Digital Temperature Sensor - TMP102

  • Particle Sensor - MAX30105

  • Air Quality Sensor - CCS811

  • ToF Range Finder - VL6180

  • Haptic Motor Driver - DRV2605L

  • Micro OLED Display

  • RGB and Gesture Sensor - APDS-9960

  • RGB Light Sensor - ISL29125

  • LED Driver - LP55231

  • DAC Breakout - MCP4725

  • 16 Output I/O Expander - SX1509

  • Battery Babysitter - BQ24075

Check out this related tutorial:

Raspberry Pi SPI and I2C Tutorial

Raspberry Pi SPI and I2C Tutorial

מק"ט יצרן # 15794
QWIIC SHIM FOR RASPBERRY PI
SparkFun Electronics
מק"ט יצרן # 14275
RASPBERRYPI GPIO MALE HEADER
SparkFun Electronics
מק"ט יצרן # 102110268
NVIDIA JETSON NANO DEV KIT
Seeed Technology Co., Ltd
מק"ט יצרן # 14532
QWIIC MICRO OLED BREAKOUT
SparkFun Electronics
מק"ט יצרן # 15440
QWIIC BME280 ATMOSPHERIC SENSOR
SparkFun Electronics
מק"ט יצרן # 15177
QWIIC VCNL4040 PROXIMITY SENSOR
SparkFun Electronics
מק"ט יצרן # 15290
QWIIC KEYPAD - 12 BUTTON
SparkFun Electronics
מק"ט יצרן # 14427
QWIIC CABLE - 100MM
SparkFun Electronics
מק"ט יצרן # 14428
QWIIC CABLE - 200MM
SparkFun Electronics
מק"ט יצרן # 14426
QWIIC CABLE - 50MM
SparkFun Electronics
מק"ט יצרן # 14429
QWIIC CABLE - 500MM
SparkFun Electronics
מק"ט יצרן # 15316
SERVO PHAT FOR RASPBERRY PI
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.