Maker.io main logo

Raspberry Pi Wearable Time Lapse Camera

240

2025-02-18 | By Adafruit Industries

License: See Original Project Camera Wearables Raspberry Pi SBC

Courtesy of Adafruit

Guide by Phillip Burgess and 1 other contributor

Overview

wearable_1

Worn on a lanyard or clipped to a pocket or pack, this adorable ‎camera snaps a photo every few seconds. Slide the SD card into your ‎computer to review the day’s activities or merge all the images into ‎a timelapse animation.‎

Powered by the diminutive and affordable Raspberry Pi Zero, this ‎DIY project is eminently configurable and customizable!‎

parts_2

Parts and Tools Required

The “canonical” build in this guide is illustrated with the following ‎parts:‎

The first three listed items are available in packs with either ‎a regular or infrared camera.‎

The example software will run on any Raspberry Pi computer. Since ‎Pi Zero supplies are constrained…or if you just want to use a different ‎board or battery, or create your own enclosure in another ‎medium…you might instead consider:‎

  • Raspberry Pi Model A+ (any Pi can work, but most are bulkier ‎and draw more power)‎

  • All but the Pi Zero can use the standard flex cable already ‎included with the camera. Custom cables for novel form-factors ‎are optional.‎

  • You can skip the PowerBoost and power the Pi directly from ‎a USB phone charger battery.‎

  • For the LED sequin, you can substitute a regular through-hole ‎LED (any color) and resistor (75 to 500 Ohm).‎

  • Likewise, most any pushbutton or switch can be substituted if ‎you’re not using the 3D-printed case.‎

The 500 mAh battery is good for about 2 hours run time. If you want ‎to keep it going all day, you could design an enclosure around a ‎larger battery…or simply plug the PowerBoost into a USB phone ‎charger to greatly extend its life!‎

You may need some additional parts depending on the installation ‎procedure used (perhaps a USB flash card reader, or a second ‎Raspberry Pi during setup, etc.). Read through the whole guide and ‎check your parts stash before making any purchasing decisions.‎

camera_3

camera_4

camera_5

‎3D Printing

printing_6

This case does not fit the Raspberry Pi Zero 2 W due to the size of the ‎WiFi module. It was designed for the Pi Zero.‎

Let’s start with the printing first. You can work on the software and ‎electronics while the printer runs the job.‎

If doing your own custom build — for example, if using a Raspberry ‎Pi Model A+ or a different battery — skip ahead to the next page. The ‎‎3D-printed parts are specifically designed around the Pi Zero and ‎components listed previously.‎

Download 3D Files from Thingiverse

Download 3D Files from Youmagine

Download Fusion 360 Source

The 3D parts will fit on even the smallest of printers, no problem ‎there. 20% infill works well, and no support material is required.‎

PLA filament is easiest to work with. If printing in ABS instead, you ‎might need to scale the model up slightly (about 2%) to allow for ‎shrinkage…the parts tolerances are very tight.‎

No fasteners are used. Instead, parts can be held with small dabs of ‎E6000 craft glue, or cyanoacrylate “Krazy” glue.‎

The clip glues to a slot in the bottom case.‎

The tripod mount and tripod base glue together the “tall” way…then ‎the camera (with clip) can slide onto this or be removed and worn.‎

Software

This guide was originally written with instructions providing a ready-‎made image but became quite outdated. Rather than continually ‎building new images from scratch, it's much easier to describe how ‎you can put together all the software parts manually. ‎

The “Using It” page of this guide provides configuration and ‎operation details…but if nothing else: it’s super especially important ‎that you press and hold the halt button and then wait about 20 ‎seconds before switching the camera off. Don’t just turn off the ‎power when you’re done…otherwise you may lose images and/or ‎corrupt the SD card and have to start over.‎

By default, the camera will capture a 1280x720 pixel JPEG image ‎every 15 seconds, recording it to the SD card in the “timelapse” folder. ‎You can change these options by inserting the card in your regular ‎computer and editing a configuration file, explained on the “Using It” ‎page.‎

Start with the lite version of the latest existing Raspberry Pi OS. It's ‎easiest to use the Raspberry Pi Imager, which can configure Wi-Fi for ‎you ahead of time.‎

liteversion_7

Then install all the software and scripts needed for the camera ‎project. The project has been updated to work on top of Blinka, so ‎the easiest way to do this is to follow the installation page in the ‎Blinka guide. This will get a virtual environment installed as well as ‎Blinka.‎

This requires a Raspberry Pi with a network connection, which can ‎be a nuisance if you’re working directly on the Pi Zero (rather than ‎the Zero W). It’s usually easiest to set up the SD card on a more ‎capable system (like a Raspberry Pi 3) and then move the finished ‎card over to the Pi Zero; it’ll boot all the same.‎

The latest versions of the Raspberry Pi OS automatically expand the ‎file system on the first boot. If you followed the Blinka guide and ran ‎the install script, the camera should already be enabled. If not, you ‎can enable it through the raspi-config utility.‎

Next download the timelapse script with the following commands:‎

Copy Code
sudo apt install -y wget
cd ~
wget https://github.com/adafruit/Adafruit_Learning_System_Guides/raw/main/Wearable_Time_Lapse_Camera/timelapse.py

Alternatively, if you’re logged in remotely via ssh, you can copy-and-‎paste the script below into that file. Since this will be located in the ‎Pi’s /boot directory (which also shows up on regular Windows or Mac ‎computers), you can save the script on your desktop computer and ‎move it to the card later.‎

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2024 Melissa leBlanc-Williams for Adafruit Industries
#
# SPDX-License-Identifier: MIT

#!/usr/bin/env python3

import os
import re
import time
import board
import digitalio

# Timelapse script, because timelapse options in raspistill don't power
# down the camera between captures. Script also provides a camera busy LED
# (v2 cameras don't include one) and a system halt button.
# Limitations: if DEST is FAT32 filesystem, max of 65535 files in directory;
# if DEST is ext4 filesystem, may have performance issues above 10K files.
# For intervals <2 sec, better just to use raspistill's timelapse feature.

# Configurable stuff...
INTERVAL = 15  # Time between captures, in seconds
WIDTH = 1280  # Image width in pixels
HEIGHT = 720  # Image height in pixels
QUALITY = 51  # JPEG image quality (0-100)
DEST = "/boot/timelapse"  # Destination directory (MUST NOT CONTAIN NUMBERS)
PREFIX = "img"  # Image prefix (MUST NOT CONTAIN NUMBERS)
HALT_PIN = board.D21  # Halt button GPIO pin (other end to GND)
LED_PIN = board.D5  # Status LED pin (v2 Pi cam lacks built-in LED)
COMMAND = "libcamera-still -n --width {width} --height {height} -q {quality} --thumb none -t 250 -o {outfile}" # pylint: disable=line-too-long
# COMMAND = "raspistill -n -w {width -h {height} -q {quality} -th none -t 250 -o {outfile}"

def main():
    prevtime = 0  # Time of last capture (0 = do 1st image immediately)
    halt = digitalio.DigitalInOut(HALT_PIN)
    halt.switch_to_input(pull=digitalio.Pull.UP)
    led = digitalio.DigitalInOut(LED_PIN)
    led.switch_to_output()

    # Create destination directory (if not present)
    os.makedirs(DEST, exist_ok=True)

    # Find index of last image (if any) in directory, start at this + 1
    files = os.listdir(DEST)
    numbers = [
        int(re.search(r"\d+", f).group())
        for f in files
        if f.startswith(PREFIX) and re.search(r"\d+", f)
    ]
    numbers.sort()
    frame = numbers[-1] + 1 if numbers else 1
    currenttime = time.monotonic()

    while True:
        while time.monotonic() < prevtime + INTERVAL:  # Until next image capture time
            currenttime = time.monotonic()
            # Check for halt button -- hold >= 2 sec
            while not halt.value:
                if time.monotonic() >= currenttime + 2:
                    led.value = True
                    os.system("shutdown -h now")
        outfile = f"{DEST}/{PREFIX}{frame:05}.jpg"
        # echo $OUTFILE
        led.value = True
        os.system(
            COMMAND.format(width=WIDTH, height=HEIGHT, quality=QUALITY, outfile=outfile)
        )
        led.value = False
        frame += 1  # Increment image counter
        prevtime = currenttime  # Save image cap time


if __name__ == "__main__":
    main()

View on GitHub

The file timelapse.py will contain our camera script. To run it, use the ‎following command:‎

Copy Code
sudo -E env PATH=$PATH python3 ~/timelapse.py

There may be some info and warnings displayed when you run it. ‎This is normal. It should still function correctly.‎

To launch the script automatically on startup, edit the ‎file /etc/rc.local and insert the following line near the end, just ‎before the final exit 0. If you are using a different username than pi, ‎you will want to change ~pi to ~yourusername.‎

Download File

Copy Code
sudo ~pi/env/bin/python3 ~pi/timelapse.py &

‎Finally, follow the Resizing the Raspberry Pi Boot Partition guide to ‎expand the boot partition.‎

Alternatively, you can use your home folder and update ‎the DEST path in the script variables. However, it may be slightly ‎harder to access the photos on some systems.‎

Camera settings and such are explained on the “Using It” page.‎

Wiring

Wiring Components

Once the parts are 3D printed and software is burnt and ready for ‎use, we can start wiring the components.‎

Slide Switch

Let's start with the slide switch. We'll need two wires here, each ‎about 8cm in length. Remove about 5mm of insulation from the tips ‎of each wire and “tin” them (apply a layer of solder) — this prevents ‎the stranded wires from fraying.‎

Next, remove one of the three legs from the switch (can be furthest ‎one from left or right, not the middle.) Then, trim the two remaining ‎legs short (about half length).‎

Now connect a wire to each leg on the slide switch by soldering ‎them together.‎

slide_8

slide_9

LED Sequin

For the LED Sequin, we'll need two wires about 7cm in length. Strip ‎and tin the tips of these wires. Then, solder them to the back of the ‎LED Sequin PCB. I suggest tinning the pads on the LED Sequin first.‎

sequin_10

sequin_11

6mm Slim Button‎

We'll need two wires about 7cm in length for the slim button. Trim ‎the two legs to about half their size. Then, tin the legs from the inside. ‎Solder wires to the legs, pointing inwards - reference the photo for ‎ideal location.‎

button_12

button_13

button_14

button_15

Raspberry Pi Power Wires

We'll need two wires to connect the PowerBoost 500C to the ‎Raspberry Pi. These can be about 8cm in length.‎

wires_16

Connect Switch to PowerBoost

Solder one of the wires from the slide switch to the EN (enable) pin ‎on the PowerBoost 500C, and the other to GND (ground). Polarity ‎doesn't matter here.‎

connect_17

Connect Pi Power Wires to PowerBoost

Now solder the two wires for the Raspberry Pi to the postive+ and ‎negative- pins on the PowerBoost 500C.‎

solder_18

With wires now added to the LED, button and PowerBoost, just a ‎few easy connections are required to the Raspberry Pi:‎

  • PowerBoost 500C output connects to 5V and GND.‎

  • LED sequin + connects to GPIO5, – to GND.‎

  • Halt button connects to GPIO21 and GND.‎

If required, the LED and button pins can be changed; this is ‎explained on the “Using It” page. Maybe you find it easier to route ‎the wires to a different spot or are building a camera with custom ‎features.‎

Here’s a full map of the Pi’s GPIO header, with our connections ‎highlighted in blue. Although this project does not use a PiTFT ‎display, those pins are marked “maybe” off-limits in the diagram ‎below, since adding a screen (with a different enclosure) might be a ‎popular upgrade project for ambitious makers.‎

map_19

Connect PowerBoost to Raspberry Pi

Solder the positive+ wire from the PowerBoost 500C to 5V on ‎Raspberry Pi. Solder the negative- wire from the PowerBoost 500C to ‎GND on Raspberry Pi. Best location is to wire them from the bottom ‎of the Pi's PCB.‎

Be extra careful to get + and – to the correct pins or you’ll fry your ‎rare and elusive Pi Zero board. Double-check all the connections ‎before finishing up and switching on!

board_20

Connect Button to Raspberry Pi

Solder the two wires from the 6mm slim button to the GPIO on the ‎bottom of the Raspberry Pi. One wire to GPIO21 and the other ‎to ground.

twowires_21

Connect LED Sequin to Raspberry Pi

Solder the postive+ wire from the LED Sequin to GPIO5 on the top of ‎the Raspberry Pi, and the negative- wire to ground.‎

top_22

Install Ribbon Cable

Now the flex cable can be installed between the camera and ‎Raspberry Pi board. The photo shows the correct orientation for each ‎end.‎

Make sure the cable is seated correctly, and the connectors are ‎latched at both ends. (If you end up with occasional green photos, it’s ‎usually a misaligned cable.)‎

Peel the protective plastic tape off the camera lens.‎

install_23

Test Circuit

OK, now most of our components are wired up. We can run a test to ‎see if everything works.‎

  • Insert the SD card to the Pi.‎

  • Connect the Pi camera module to the Pi.‎

  • Plug in the JST connector from the 500mAh LiPo battery to the ‎PowerBoost 500C.‎

circuit_24

If the blue LED turns on, the slide switch is on, and Pi will power up. ‎If not, slide the switch to turn it on. The Pi will take about ~1min to ‎boot up (on initial startup). You should see the LED sequin turn on ‎each time the Pi takes a photo.‎

Allow it to run for a few minutes collecting photos, so you can ‎confirm the camera connection is solid before sealing everything up.‎

If it’s all working as expected, hold down the 6mm slim button for ‎about ~3 seconds and wait about 30 seconds for the Pi to safely shut ‎down. Then, turn off the PowerBoost 500C with the slide switch.‎

Remove the SD card from the Pi and insert it into your computer. ‎Your photos will show up in the “timelapse” folder.‎

Once you’re satisfied everything’s operational, we can move on to ‎mounting the circuit into the 3D-printed case…‎

Assembly

Install Button

The 6mm slim button is a bit tricky to install in the case. You'll have ‎to remove it from the Pi GPIO by desoldering the wires. Once it's free, ‎thread the two wires from the button into the case - refer to the ‎photos for the location. Then, push the button through the hole. ‎Press it down until the button is positioned properly. Once nestiled in ‎place, the button will stay put when pressed. ‎

Now you can solder the wires back onto the GPIO of the Raspberry ‎Pi.‎

assembly_25

assembly_26

assembly_27

assembly_28

Install PowerBoost 500C

With the battery plugged into the PowerBoost 500C, insert the ‎PowerBoost 500C into the case and line up the mounting holes with ‎the standoffs. Press it down so the nubs from the standoffs snap into ‎the mounting holes.‎

If the nubs aren’t “snappy” enough, you can add some small dabs of ‎E6000® or Krazy Glue® to keep the board in place.‎

nubs_29

Install Battery

Fit the 500mAh lip battery into case. Carefully nestile the JST cable ‎from the battery into the case. ‎

battery_30

Install LED Sequin

Lay the LED Sequin PCB over the cavity on the case cover. Orient the ‎Sequin so the SMD LED is poking through the opening. You'll need a ‎piece of mounting tack or glue to keep it in place - It may snap into ‎place depending on your printers tolerances.‎

lay_31

Install Pi Camera

Orient the Pi camera so the lens pokes through the hole. Line up the ‎nubs from the standoffs with the mounting holes on the Pi camera ‎PCB. Press the Pi camera so it's flush with the standoffs.

install_32

Install Raspberry Pi

The Raspberry Pi will lay over the Pi camera module. Line up the ‎nubs from the standoffs with the mounting holes on the Pi. Press the ‎Pi PCB down until it snap fits into the nubs.‎

pi_33

Secure Pi Camera Cable

Bend the excess cable from the Pi camera module so its over the ‎bottom of the Pi PCB. I recommend using small pieces of mounting ‎tack to keep the ribbon cable from unfolding.‎

secure_34

Install Slide Switch

The slide switch will rest on the platform over the 6mm slim button. ‎You may need some mounting tack to keep in place while closing ‎the case.‎

slide_35

Close Case!‎

Now it's time to join the cover and case together. Make sure any ‎excess wires are tucked into the case or cover. Start by inserting the ‎cover into the case at an angle, with the ports from the Raspberry Pi ‎first. Then, press the cover into the case so it snaps fit.‎

If find the case won't close, you may need to install the switch onto ‎the cover instead - if it still doesn't close, thoroughly inspect the ‎wires and components to see if something is blocking the lip of the ‎cover.‎

case_36

case_37

case_38

Install Wearable Clip

If you plan on wearing the Pi camera, we provided a little clip. ‎There's a small little "slit" on the back of the case - press ‎the connector from clip into the slit. You’ll probably want some glue ‎to keep it in place.‎

clip_38

clip_39

Optional: Extra Lens

You can optionally add lenses to increase the viewing angle. I got ‎this 0.68X wide angle lense from Amazon.com - it's normally used for ‎mobile phones. It uses a magnet and metal ring with a stick ‎adhesive backing so you can easily add / remove the lens.‎

lens_40

lens_41

lens_42

Using It

The camera software works on its own…there’s no buttons or ‎anything to fiddle with to get it started. Just turn the power switch ‎on…once the system is booted (maybe 30 seconds or so) it will begin ‎capturing images (first-time boot may take about a minute longer as ‎it resizes the filesystem and such). The status LED will turn ON while ‎the camera is taking a picture.‎

To turn the camera off, press and hold the halt button for at least 2 ‎seconds. The status LED will turn ON while the system performs a ‎clean shutdown (about 20 seconds), then OFF to indicate it’s safe to ‎turn the power switch off.‎

Always use the halt button before powering off the camera. Don’t ‎just switch it off or you risk losing images or having to re-do the ‎whole SD card.‎

When the system is powered off, you can remove the micro-SD card ‎and install it in a USB reader on your regular computer. The images ‎will be inside a folder called “timelapse” and are numbered ‎sequentially…img00001.jpg, img00002.jpg, img00003.jpg and so ‎forth.‎

After transferring images off the card, you can delete these files (or ‎the whole timelapse folder) and the next recording will begin back ‎at #00001. Or if you leave the images there, it will begin recording at ‎the next number in the sequence.‎

Do not move, alter, or delete any files other than the images in the ‎timelapse folder. The Raspberry Pi requires these to run.‎

Settings

By default, the software will capture a 1280 by 720-pixel JPEG image ‎every 15 seconds. You can change these settings by editing the ‎file timelapse.py on the SD card using any text editor. These ‎configurable values are near the top of the file:‎

Download File

Copy Code
# Configurable stuff...
INTERVAL = 15 				# Time between captures, in seconds
WIDTH = 1280  				# Image width in pixels
HEIGHT = 720  				# Image height in pixels
QUALITY = 51  				# JPEG image quality (0-100)
DEST = "/boot/timelapse"   	# Destination directory (MUST NOT CONTAIN NUMBERS)
PREFIX = "img"  			# Image prefix (MUST NOT CONTAIN NUMBERS)
HALT_PIN = board.D21  		# Halt button GPIO pin (other end to GND)
LED_PIN = board.D5  		# Status LED pin (v2 Pi cam lacks built-in LED)

COMMAND = "libcamera-still -n --width {width} --height {height} -q {quality} --thumb none -t 250 -o {outfile}"
# COMMAND = "raspistill -n -w {width -h {height} -q {quality} -th none -t 250 -o {outfile}"

‎With this script there is a practical minimum interval of about 2 ‎seconds between captures (maybe longer for larger images); if you ‎need anything faster than that, it’s best to use the time lapse ‎features built into the libcamera-still or raspistill utility itself. This is ‎documented on the Raspberry Pi web site.‎

The GPIO pins used by the halt button and status LED can be ‎changed in the script if you’ve wired yours up differently.‎

Since libcamera-still has replaced for raspistill, this is now the ‎default. If you are on an older system, you can use the equivalent ‎raspistill line.‎

Direct Sunlight

If you find a lot of images are coming back oddly exposed, the ‎camera might need a little more “wakeup time” before capturing an ‎image. Look for the following line (up just a few lines from end of the ‎script) and change “250” to a larger value, perhaps 1000 (this is the ‎wakeup time in milliseconds; 1000 = 1 second):‎

Download File

Copy Code
libcamera-still -n --width {width} --height {height} -q {quality} --thumb none -t 1500 -o {outfile}

‎or if you are using raspistill:‎

Download File

Copy Code
raspistill -n -w {width -h {height} -q {quality} -th none -t 1500 -o {outfile}

‎There are more settings for controlling exposure, ISO, etc…see link ‎below…‎

Gotchas and Things to Know

With this or any other battery-powered Raspberry Project, there’s a ‎small possibility of losing data (or even corrupting the SD card and ‎having to start over) should the battery become depleted during ‎use…similar to switching the device off without using the halt button.‎

One way to reduce (but not eliminate) this risk is to add a “sync” ‎command immediately after the “libcamera-still” command, which ‎forces the completion of all pending file writes:‎

Download File

Copy Code
os.system(
    COMMAND.format(width=WIDTH, height=HEIGHT, quality=QUALITY, outfile=outfile)
)
os.system("sync")

‎The extra time needed for this sync operation means the practical ‎minimum INTERVAL value will be longer…perhaps 10 seconds. This is ‎why it’s not done by default.‎

Adjusting Camera Settings

The libcamera-still command (as it was with the older raspistill ‎command) has a huge number of options…you can tweak exposure ‎and white balance settings, image size, add interesting “painterly” ‎effects to the image…it’s way beyond the scope of this guide, so if ‎you’d like to dig deeper, please refer to the Pi Foundation’s reference:‎

Official Raspberry Pi Camera Documentation

Extending Run Time

If you have a very long-time lapse project in mind that exceeds the ‎longevity of the built-in battery (about 2 hours), you can use a higher ‎capacity USB phone charger battery connected one of two ways:‎

  • To the PowerBoost’s USB charge port. This will top off the ‎PowerBoost’s battery while also running the Pi.‎

  • Directly to the Pi’s USB power port. Leave the PowerBoost ‎switched OFF in this case, or there will be…trouble.‎

‎ In either case, you do still need to use the halt button before ‎switching off or disconnecting power.‎

SD Card Limitations

The /boot filesystem uses a Windows “FAT32” directory structure. This ‎limits the timelapse directory to a maximum of 65,535 images. The ‎script doesn’t enforce any specific checks on this, since other limiting ‎factors (battery longevity, card capacity, etc.) are more likely to come ‎into play much sooner.‎

The startup file system consistency check (fsck) on the /boot ‎partition has been disabled in the ready-made SD image. If a large ‎number of images (several thousand) are present on the card, boot ‎time is inordinately long with this check in place. If you really want ‎that boot-time check, you’ll need to familiarize yourself with and edit ‎‎/etc/fstab.‎

Between this and the battery concerns, copying images off the card ‎at every convenient opportunity is recommended. Also, if you’ve ‎rolled your own SD card, making a backup image is recommended.‎

Merging Stills into Video or GIF

Combining the captured images into a video or GIF you can share ‎will depend on what software you have access to and are familiar ‎with. For example, Adobe Premiere or AfterEffects have fancy GUIs ‎‎(but cost may be prohibitive if you don’t already use these tools), or ‎there are free command-line tools like ffmpeg or ‎ImageMagick’s convert.‎

Covering every tool for every likely operating system is beyond the ‎scope of this guide. If it’s an unfamiliar process, try Google searching ‎for “jpg to video windows” or “jpg to video mac” or similar. So many ‎options!‎

Just one example…in Adobe Photoshop CC, it’s possible through a ‎roundabout sequence of operations…‎

  • File→Scripts→Load Files into Stack…‎

  • In pop-up window, click “Browse” and select image files, then ‎‎“OK.”‎

  • In Timeline window, “Create Frame Animation.”‎

  • In Timeline menu, “Make Frames from Layers.”‎

  • Then the usual frame animation tools (timing, etc.) can be used ‎to create a video (File→Export→Render Video…) or animated GIF ‎‎(File→Export→Save for Web (Legacy)…).

example_43

example_44

example_45

example_46

מק"ט יצרן # SC0023
RPI CAM V2 IMX219 8MP
Raspberry Pi
מק"ט יצרן # SC0024
RPI CAM V2 NOIR IMX219 8MP
Raspberry Pi
מק"ט יצרן # SC1628
MEM CARD MICROSD 32GB CLASS 10
Raspberry Pi
מק"ט יצרן # 1758
ADAFRUIT LED SEQUINS
Adafruit Industries LLC
מק"ט יצרן # 1446
WIRE WRAP THIN PROTOTYPING & REP
Adafruit Industries LLC
מק"ט יצרן # SC0873
RASPBERRY PI CAMERA 3 NOIR
Raspberry Pi
מק"ט יצרן # 2144
RASPBERRY PI CAMERA CABLE 2M
Adafruit Industries LLC
מק"ט יצרן # 5211
RPI ZERO CAMERA CABLE 300MM
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.