Maker.io main logo

Simplifying Qualia CircuitPython Projects

194

2025-02-28 | By Adafruit Industries

License: See Original Project Board Specific Displays LCD / TFT Touch ESP32

Courtesy of Adafruit

Guide by M. LeBlanc-Williams

Overview

dotclock_1

The Qualia ESP32-S3 board is capable of driving RGB 666 dot clock displays, but the code ‎to initialize them can be a bit long and most people don't want the first 50 to 100 lines of ‎their code dedicated to just initializing the display. You can find more information about ‎their usage in the Adafruit Qualia ESP32-S3 for RGB-666 Displays guide.‎

The Qualia helper library removes a lot of the overhead work of getting the display up and ‎running allowing you to concentrate on your project code instead of trying out a myriad of ‎drivers, initialization codes, and timings just to get the display to show something.‎

It works by initializing the display as well as the appropriate touch driver if there is one for ‎the display. The Qualia helper library is also built on top of the PortalBase library, which ‎gives it many of the functions available to boards such as the PyPortal and MatrixPortal.‎

This guide will go overusing the library as well as covering the examples included with the ‎library.‎

Parts

Also, compatible displays, under Featured Products or as listed under Qualia.‎

Create Your settings.toml File

CircuitPython works with WiFi-capable boards to enable you to make projects that have ‎network connectivity. This means working with various passwords and API keys. As ‎of CircuitPython 8, there is support for a settings.toml file. This is a file that is stored on ‎your CIRCUITPY drive, which contains all of your secret network information, such as your ‎SSID, SSID password and any API keys for IoT services. It is designed to separate your ‎sensitive information from your code.py file so you are able to share your code without ‎sharing your credentials.‎

CircuitPython previously used a secrets.py file for this purpose. The settings.toml file is ‎quite similar.‎

Your settings.toml file should be stored in the main directory of your CIRCUITPY drive. It ‎should not be in a folder.‎

CircuitPython settings.toml File

This section will provide a couple of examples of what your settings.toml file should look ‎like, specifically for CircuitPython WiFi projects in general.‎

The most minimal settings.toml file must contain your WiFi SSID and password, as that is ‎the minimum required to connect to WiFi. Copy this example, paste it into ‎your settings.toml, and update:‎

  • your_wifi_ssid

  • your_wifi_password

Download File

Copy Code
CIRCUITPY_WIFI_SSID = "your_wifi_ssid"
CIRCUITPY_WIFI_PASSWORD = "your_wifi_password"

Many CircuitPython network-connected projects on the Adafruit Learn System involve using ‎Adafruit IO. For these projects, you must also include your Adafruit IO username and key. ‎Copy the following example, paste it into your settings.toml file, and update:‎

  • your_wifi_ssid

  • your_wifi_password

  • your_aio_username

  • your_aio_key

Download File

Copy Code
CIRCUITPY_WIFI_SSID = "your_wifi_ssid"
CIRCUITPY_WIFI_PASSWORD = "your_wifi_password"
ADAFRUIT_AIO_USERNAME = "your_aio_username"
ADAFRUIT_AIO_KEY = "your_aio_key"

Some projects use different variable names for the entries in the settings.toml file. For ‎example, a project might use ADAFRUIT_AIO_ID in the place ‎of ADAFRUIT_AIO_USERNAME. If you run into connectivity issues, one of the first things ‎to check is that the names in the settings.toml file match the names in the code.‎

Not every project uses the same variable name for each entry in the settings.toml file! ‎Always verify it matches the code.‎

settings.toml File Tips

Here is an example settings.toml file.‎

Download File

Copy Code
# Comments are supported
CIRCUITPY_WIFI_SSID = "guest wifi"
CIRCUITPY_WIFI_PASSWORD = "guessable"
CIRCUITPY_WEB_API_PORT = 80
CIRCUITPY_WEB_API_PASSWORD = "passw0rd"
test_variable = "this is a test"
thumbs_up = "\U0001f44d"

In a settings.toml file, it's important to keep these factors in mind:‎

  • Strings are wrapped in double quotes; ex: "your-string-here"‎

  • Integers are not quoted and may be written in decimal with optional sign (+1, -‎‎1, 1000) or hexadecimal (0xabcd).‎

o Floats, octal (0o567) and binary (0b11011) are not supported.‎
  • Use \u escapes for weird characters, \x and \ooo escapes are not available ‎in .toml files

o Example: \U0001f44d for 👍 (thumbs up emoji) and \u20ac for € (EUR sign)‎
  • Unicode emoji, and non-ASCII characters, stand for themselves as long as you're ‎careful to save in "UTF-8 without BOM" format‎

When your settings.toml file is ready, you can save it in your text editor with ‎the .toml extension.‎

settings_2

Accessing Your settings.toml Information in code.py

In your code.py file, you'll need to import the os library to access the settings.toml file. ‎Your settings are accessed with the os.getenv() function. You'll pass your settings entry to ‎the function to import it into the code.py file.‎

Download File

Copy Code
import os

print(os.getenv("test_variable"))

code_3

In the upcoming CircuitPython WiFi examples, you'll see how the settings.toml file is used ‎for connecting to your SSID and accessing your API keys.‎

Usage

Choosing your layers is an important part of creating a project with regards to the Portal-‎style libraries since it's easy to accidentally choose layers that end up duplicating some of ‎the functions. This guide is intended to help clarify your understanding of the layout so you ‎can make the best choices for your needs.‎

The PyPortal library, which is what inspired this library was written as a single layer which ‎had the advantage of making it really simple to use for a certain type of project and it ‎worked well for the PyPortal because the hardware setup varies very little between the ‎different models. As more boards were written in this style of library, a base library called ‎PortalBase was created to make it easier to maintain multiple libraries. The libraries were ‎originally broken up into layers to allow for loading only the parts that were needed for a ‎project with the advantage of saving memory when there wasn't much to spare.‎

For the Qualia ESP32-S3, there is plenty of PSRAM available, so you could just load the ‎topmost layer. However, with continuing the tradition of layers and the fact that some of the ‎huge displays can take up a good chunk of the RAM, not loading more than needed is still a ‎good approach.‎

Mixing and Matching Layers

mixing_4

Which of the layers you choose to use for your project depends on the amount of ‎customization and memory management you would like in your project. The higher level up ‎you go in the library layer hierarchy, the more automatic functions you will have available to ‎you, but it also takes away your ability to customize things and uses more memory.‎

In general, you will likely want at least one of the Graphics layers and optionally one of the ‎Network layers. If you plan on using the peripherals specific to the board such as the ‎buttons, you will want the peripherals layer as well.‎

Graphics Layers

graphics_5

For the Qualia library having multiple possible displays, a slightly different approach was ‎taken with writing Graphics layers. There is a folder of displays that contain both the ‎DotClockDisplay base class and the display-specific classes.‎

There is also a Displays class, which can be found alongside the Graphics class that was ‎written for the purpose of finding all of the display-specific classes and loading the ‎filename as an attribute in all uppercase. This class has only static functions because it is ‎meant to be used without instantiating it first.‎

This makes it easy to add new displays to the library since everything is just kept in one ‎place.‎

Network Layers

network_6

On the network functionality side of things, you will want to include the Network layer, ‎which includes some convenient functions such as fetch for data and wget for ‎downloading files. With plenty of RAM, the Qualia should be able to handle most ‎downloads.‎

Peripherals Layer

peripherals_7

To use the peripheral functionality, if you just wanted to initialize the buttons or control the ‎display's backlight, then you would want to use the Peripherals layer. Compared to some of ‎the other Portal-style boards, the Qualia ESP32-S3 has very few peripherals.‎

Top Layer

top_8

If you wanted everything along with some great functionality that ties all the legs of the ‎hierarchy together then you would want the very top layer, which is the Qualia layer. This ‎layer is the all-inclusive layer. To access the lower layers, you can use the following ‎attributes:‎

  • peripherals - The Peripherals Layer

  • graphics - The Graphics Layer

  • network - The Network Layer

  • display - The FrameBufferDisplay layer

  • graphics.dotclockdisplay - The DotClockDisplay layer

Remember that if you go with this layer, you should not import any of the lower layers with ‎the exception of the Displays layer.‎

Importing your layers

Displays Layer

This layer is special since it will automatically enumerate the displays upon import, and you ‎will need it in order to instantiate the Top or Graphics layers

Download File

Copy Code
from adafruit_qualia.graphics import Displays

To refer to a specific display, you would refer to it starting with Displays. followed by the ‎filename in all capital letters without the .py at the end. For example:‎

  • Displays.ROUND21 - Round 2.1" Display

  • Displays.SQUARE34 - Square 3.4" Display

  • Displays.BAR320X820 - 320x820 Bar Display‎

These are only a few of the supported displays. Check the displays folder for a complete list ‎of available displays. It doesn't matter whether your display has touch or not as it will ‎attempt to initialize the appropriate touch driver, but if the chip isn't found, it will still load.‎

Alternatively, you could just use a string with the filename in all lowercase without ‎the .py extension. For example, "round21".‎

Top Layer

To import the top-level layer only, you would simply just import it like this:‎

Download File

Copy Code
from adafruit_qualia import Qualia

If you would like access to the lower layers, you can directly access them as attributes. For ‎instance, if you instantiated the top layer as qualia, then you could access the layers.‎

Download File

Copy Code
qualia = Qualia(DISPLAY)
network = qualia.network
graphics = qualia.graphics
peripherals = qualia.peripherals

Replace with DISPLAY with the display you have connected such as Displays.ROUND21. ‎See the Displays Layer for more information.‎

If you would prefer, you don't even need to assign them to variable and can just directly ‎access the attributes when needed.‎

Sub-Layers

To only import sub-layers such as the Graphics and Network layers, you would import it like ‎this:‎

Download File

Copy Code
from adafruit_qualia.graphics import Graphics
from adafruit_qualia.network import Network

After they're imported, you would just instantiate each of the classes separately.‎

Download File

Copy Code
graphics = Graphics(DISPLAY)
network = Network()

Replace with DISPLAY with the display you have connected such as Displays.ROUND21. ‎See the Displays Layer for more information.‎

Code Examples

Here is the code from one of the examples that are included with the library. To run the ‎examples, simply rename them as code.py and place them in the root of ‎your CIRCUITPY drive.‎

Simple Test

This example was written to use the square 3.4" display, but should be able to work with any ‎of the displays. It uses the top-level Qualia layer and makes use of the graphics and ‎network. It connects to your WiFi, downloads some test data, and displays the data in the ‎REPL.‎

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2023 Melissa LeBlanc-Williams for Adafruit Industries
#
# SPDX-License-Identifier: Unlicense
#
# NOTE: Make sure you've set up your settings.toml file before running this example
# https://learn.adafruit.com/getting-started-with-web-workflow-using-the-code-editor/

from adafruit_qualia import Qualia
from adafruit_qualia.graphics import Displays

# Set a data source URL
TEXT_URL = "http://wifitest.adafruit.com/testwifi/index.html"

# Create the Qualia object
qualia = Qualia(Displays.SQUARE34, url=TEXT_URL)

# Go get that data
print("Fetching text from", TEXT_URL)
data = qualia.fetch()

# Print out what we got
print("-" * 40)
print(data)
print("-" * 40)

View on GitHub

fetch_9

Quotes Example

The quotes example is more like how the PyPortal works in that a data source is defined, ‎two text fields are created, and the quote and author data are displayed. This example was ‎also written for the square 3.4" display but could be modified to run on other displays by ‎adjusting the text field settings such as text_wrap.‎

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2019 Limor Fried for Adafruit Industries
# SPDX-FileCopyrightText: 2023 Melissa LeBlanc-Williams for Adafruit Industries
#
# SPDX-License-Identifier: MIT

import time
from adafruit_qualia import Qualia
from adafruit_qualia.graphics import Displays

# Set up where we'll be fetching data from
DATA_SOURCE = "https://www.adafruit.com/api/quotes.php"
QUOTE_LOCATION = [0, "text"]
AUTHOR_LOCATION = [0, "author"]

qualia = Qualia(
    Displays.SQUARE34,
    url=DATA_SOURCE,
    json_path=(QUOTE_LOCATION, AUTHOR_LOCATION),
    default_bg=0x333333,
)

qualia.add_text(
    text_position=(20, 120),  # quote location
    text_color=0xFFFFFF,  # quote text color
    text_wrap=25,  # characters to wrap for quote
    text_maxlen=180,  # max text size for quote
    text_scale=3,  # quote text size
)

qualia.add_text(
    text_position=(5, 240),  # author location
    text_color=0x8080FF,  # author text color
    text_wrap=0,  # no wrap for author
    text_maxlen=180,  # max text size for quote & author
    text_scale=3,  # author text size
)

while True:
    try:
        value = qualia.fetch()
        print("Response is", value)
    except (ValueError, RuntimeError, ConnectionError, OSError) as e:
        print("Some error occured, retrying! -", e)
    time.sleep(60)

View on GitHub

mistakes_10

QR Code Example

The QR Code Generation example generates a QR code and displays it in the center of the ‎display. This example was written for the round 2.1" display but could easily be adapted for ‎the other displays.‎

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2021 Jose David M.
# SPDX-FileCopyrightText: 2023 Melissa LeBlanc-Williams for Adafruit Industries
#
# SPDX-License-Identifier: MIT

# NOTE: Make sure you've set up your settings.toml file before running this example
# https://learn.adafruit.com/getting-started-with-web-workflow-using-the-code-editor/
"""
This example shows a web address QR on the display
"""

import time
from adafruit_qualia.graphics import Graphics, Displays
from adafruit_qualia.peripherals import Peripherals

# Background Information
base = Graphics(Displays.ROUND21, default_bg=0x990099)

# Set up Peripherals
peripherals = Peripherals(i2c_bus=base.i2c_bus)

# Set display to show
display = base.display

# WebPage to show in the QR
webpage = "http://www.adafruit.com"

# QR size Information
qr_size = 9  # Pixels
scale = 10

# Create a barcode
base.qrcode(
    webpage,
    qr_size=scale,
    x=(display.width // 2) - ((qr_size + 5) * scale),
    y=(display.height // 2) - ((qr_size + 4) * scale),
)

while True:
    if peripherals.button_up:
        peripherals.backlight = True
    if peripherals.button_down:
        peripherals.backlight = False
    time.sleep(0.1)

View on GitHub

paint_11

Paint Example

This last example is the most complex one and will run on any of the displays with a ‎touchscreen. This was adapted from an example included in the FocalTouch library and ‎ends up being around 30 lines less, but supporting many more displays. This example only ‎uses the Graphics layer and shows how to make use of the touch screen.‎

‎Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2023 Melissa LeBlanc-Williams for Adafruit Industries
# SPDX-License-Identifier: MIT
"""
Simple painting demo that works with on any touch display
"""
import displayio
from adafruit_qualia.graphics import Graphics, Displays

# For other displays:
# 2.1" Round = Displays.ROUND21
# 3.4" Square = Displays.SQUARE34
# 320 x 820 Bar - Displays.BAR320X820
# 320 x 960 Bar - Displays.BAR320X960
graphics = Graphics(Displays.SQUARE40, default_bg=None, auto_refresh=False)

if graphics.touch is None:
    raise RuntimeError("This example requires a touch screen.")

# Main Program
pixel_size = 6
palette_width = 160
palette_height = graphics.display.height // 8

bitmap = displayio.Bitmap(graphics.display.width, graphics.display.height, 65535)

# Create a TileGrid to hold the bitmap
tile_grid = displayio.TileGrid(
    bitmap,
    pixel_shader=displayio.ColorConverter(input_colorspace=displayio.Colorspace.RGB565),
)

# Add the TileGrid to the Group
graphics.splash.append(tile_grid)

# Add the Group to the Display
graphics.display.root_group = graphics.splash

current_color = displayio.ColorConverter().convert(0xFFFFFF)

for i in range(palette_width):
    color_index = i * 255 // palette_width
    rgb565 = displayio.ColorConverter().convert(
        color_index | color_index << 8 | color_index << 16
    )
    r_mask = 0xF800
    g_mask = 0x07E0
    b_mask = 0x001F
    for j in range(palette_height):
        bitmap[i, j + palette_height] = rgb565 & b_mask
        bitmap[i, j + palette_height * 2] = rgb565 & (b_mask | g_mask)
        bitmap[i, j + palette_height * 3] = rgb565 & g_mask
        bitmap[i, j + palette_height * 4] = rgb565 & (r_mask | g_mask)
        bitmap[i, j + palette_height * 5] = rgb565 & r_mask
        bitmap[i, j + palette_height * 6] = rgb565 & (r_mask | b_mask)
        bitmap[i, j + palette_height * 7] = rgb565

graphics.display.auto_refresh = True

while True:
    if graphics.touch.touched:
        try:
            for touch in graphics.touch.touches:
                x = touch["x"]
                y = touch["y"]
                if (
                    not 0 <= x < graphics.display.width
                    or not 0 <= y < graphics.display.height
                ):
                    continue  # Skip out of bounds touches
                if x < palette_width:
                    current_color = bitmap[x, y]
                else:
                    for i in range(pixel_size):
                        for j in range(pixel_size):
                            x_pixel = x - (pixel_size // 2) + i
                            y_pixel = y - (pixel_size // 2) + j

                            if (
                                0 <= x_pixel < graphics.display.width
                                and 0 <= y_pixel < graphics.display.height
                            ):
                                bitmap[x_pixel, y_pixel] = current_color
        except RuntimeError:
            pass

View on GitHub

display_12

מק"ט יצרן # 4474
CABLE A PLUG TO C PLUG 3'
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.