Maker.io main logo

Solar Boost Bag

48

2021-03-02 | By Adafruit Industries

License: See Original Project Wearables

Courtesy of Adafruit

Guide by Becky Stern

Overview

Make your own backup battery and recharge it with the sun! This is an upgrade project to our original Solar Charging Handbag and uses a PowerBoost 500 Basic, a solar Lipoly charger, slide switch, and 2000mAh rechargeable battery, all housed in a 3D printed enclosure.

 

battery_1

Before you begin, read through the following guides:

solarpack_2

parts_3

For this project, you will need:

3D Design Files

box_4

Download STLs

Table_5

Customize Design

The original solids are available to modify and download from our 123D Design project page.

123D Design

Assemble Circuit

circuit_6

When you solder the capacitor on the solar charger, fold the capacitor over so it makes a more compact shape.

solder_7

Solder the leads of the capacitor to the board.

leads_8

Solder the JST connector to the LOAD side of the solar charger as shown. The red wire goes to LOAD and the black wire goes to GND.

snip_9

Snip any excess wire on the back side of the board as well as the leads of the capacitor.

leads_10

Solder the USB port onto the PowerBoost.

USB_11

Prepare a slide switch by soldering on two short silicone-coated stranded wires to two adjacent pins, then apply and shrink some heat shrink tubing to protect the connections.

Insert the switch wires from the outside to the inside of the enclosure and seat the switch in its cutout, then solder the two wires to EN and GND (doesn’t matter which wire goes to which pin) on the inside of the enclosure.

wires_12

Plug the JST wire from the solar charger into the PowerBoost, plug the Lipoly battery into the BATT plug on the solar charger, and connect a miniB USB cable to your computer or an AC adapter to test out the circuit.

If toggling the slide switch turns the green PowerBoost LED on and off, you’re good to go!

Prepare Solar Panel

clamp_13

Follow Method 2 for replacing your solar panel's barrel jack on the appropriate page of the LiPoly Charger Guide: first slide on a large piece of heat shrink tubing, two smaller pieces (one on each wire). Tin the stripped wire leads and solder them together (red to red and black to black). Shrink the little heat shrink tubing pieces over the joints, then shrink the larger piece over the entire section for a finished look and added stability.

shrink_14

Test your circuit by plugging in the solar panel, then placing it in direct sunlight. The red charging light should be bright and solid, not flashing. To learn more about the charger, check out the LiPoly Charger Guide. You can also charge your battery using the mini USB jack. Plug your phone into the PowerBoost's USB port and see it charge up!

Enclosure

enclosure_15

Use #4-40 3/8 flat Phillips machine screws through the enclosure and mounting holes on the circuit boards to secure them inside, aligning the ports with the cutouts on the enclosure.

cutouts_16

The enclosure has countersunk screw holes, so the screws sit flush to the plastic surface.

Apply a piece of foam double-stick tape to the battery and stick it to the inside of the enclosure lid, within the rectangular outline.

tape_17

tape_18

tape_19

tape_20

Carefully plug the battery into the BATT port on the Lipoly battery charger. You may need to use tweezers or pliers to get it into the small space.

The above pictured version of this circuit uses a double-ended JST cable instead of one soldered directly to the LOAD pads on the PCB. There is no reason to do this unless you like practicing your wire splicing and have extra JST wires hanging around your desk (I'm guilty as charged!).

secure_21

Place the lid and secure it with four more machine screws.

lid_22

If the solar panel is plugged in and in bright sun, the battery will be charging. You can toggle the PowerBoost power with the slide switch, and you can peek inside the USB cutout to see the green light indicating power is on.

Wear it!

wear_23

Most of our large solar panels have four mounting screws that make it easy to affix to any bag. You can also use Velcro tape to make your solar panel quick-release!

pack_24

Tuck your power pack into your bag with the cable routed to your solar panel. You can charge while you walk outside or stash your bag in a sunny spot. Even leave your solar panel at home and just take the charged-up backup battery with you!

מק"ט יצרן # 390
EVAL BOARD FOR MCP73871
Adafruit Industries LLC
מק"ט יצרן # 1903
EVAL BOARD FOR TPS61090
Adafruit Industries LLC
5V 2A SWITCHING POWER SUPPLY W/
מק"ט יצרן # 1994
5V 2A SWITCHING POWER SUPPLY W/
Adafruit Industries LLC
מק"ט יצרן # 1329
CBL ASSY BARREL PL-GATOR 0.83'
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.