Maker.io main logo

SparkFun Qwiic Shield for Arduino Nano Hookup Guide

44

2020-05-29 | By SparkFun Electronics

License: See Original Project

Courtesy of SparkFun

Guide by EL DUDERINO

Introduction

The SparkFun Qwiic Shield for Arduino Nano allows you to add the SparkFun Qwiic ecosystem to development boards that use the Arduino Nano Footprint in an easy-to-assemble shield. It connects the I2C bus (GND, 3.3V, SDA, and SCL) on your Arduino Nano to four SparkFun Qwiic connectors. The Qwiic ecosystem allows for easy daisy chaining so, as long as your devices are on different addresses, you can connect as many Qwiic devices as you'd like.

SparkFun Qwiic Shield for Arduino Nano

Required Materials

To follow along with this guide, you will need an Arduino with the Nano footprint. This includes the all variants of the Arduino Nano and many other Arduino Nano-compatible boards! Here are just a few of the compatible boards.

  • Arduino Nano 33 BLE Sense

  • Arduino Nano Every

  • Arduino Nano 33 BLE

  • Arduino Nano 33 IoT with Headers

You will also need some headers to solder to both your Arduino Nano and Qwiic Shield:

Now you probably would not want the Qwiic Shield for Arduino Nano if you didn't have any Qwiic products to use with it, right? Well, if you don't have any Qwiic products, the following might not be a bad place to start.

You will need some of our Qwiic cables to connect your devices to the shield. Below are a few options:

Lastly, if you want to use a non-Qwiic I2C device, these adapters help to convert it to a Qwiic connector:

Required Tools

You will need a soldering iron, solder, and general soldering accessories to solder the header pins to the Qwiic shields.

Suggested Reading

If you aren't familiar with the Qwiic ecosystem, we recommend reading here for an overview:

qwiic_1

We would also recommend taking a look at the following tutorials if you aren't familiar with them:

  • How to Solder: Through-Hole Soldering: This tutorial covers everything you need to know about through-hole soldering.

  • I2C: An introduction to I2C, one of the main embedded communications protocols in use today.

  • Arduino Shields v2: An update to our classic Arduino Shields Tutorial! All things Arduino shields. What they are and how to assemble them.

Hardware Overview

The Qwiic Shield for Arduino Nano is pretty straight forward shield but has a few extra bits we'll cover in this section.

Qwiic Connectors

Just like our other Qwiic adapter boards, the Qwiic Shield for Arduino Nano comes with several Qwiic connectors. There are two horizontal Qwiic connectors on the edges of the board and two vertical ones in the center.

connectors_2

Logic Shifting Circuit and IOREF Jumper

The Qwiic Shield for Arduino Nano has a configurable logic shifting circuit depending on the voltage your Arduino Nano runs at. There is a jumper on the shield to set the IOREF voltage for the logic shifting circuit. The jumper defaults to 3.3V which works fine for 33 Nanos like the Arduino 33 Nano BLE but you will need to switch the jumper to 5V for Arduino Nanos that run at 5V like the Arduino Nano Every.

Jumper_3

Never worked with solder jumpers before just need some tips or a quick refresher? Check out our How to Work with Jumpers and PCB Traces tutorial.

pads_4

How to Work with Jumper Pads and PCB Traces APRIL 2, 2018

Handling PCB jumper pads and traces is an essential skill. Learn how to cut a PCB trace,

add a solder jumper between pads to reroute connections, and repair a trace with the green wire method if a trace is damaged.

I2C Jumper

The I2C jumper pulls the Qwiic SDA and SCL lines up to 3.3V through 4.7K resistors. The reference voltage set by the IOREF Jumper has no effect on the voltage of the pull up resistors. You can disable them by severing the trace in between the pads if you have many devices on your I2C bus.

I2C_5

Board Dimensions

The shield measures 1.7in. x 0.7in. (43.18mm x 17.78mm) and has four mounting holes with a 0.07in diameter that match those on the Nano footprint.

footprint_6

Hardware Assembly

All that is needed to get started using the Qwiic Shield for Arduino Nano is to solder your chosen headers to the shield and, if necessary, to your Arduino Nano. If you have never worked with an Arduino Shield before or need some tips, our Arduino Shields Tutorial provides detailed instructions on how to assemble and use them. Take care to match the markings on the Qwiic Shield to the appropriate pins on your Nano to avoid shorting anything out and possibly damaging your Nano. Also, some variants of the Nano like the Nano 33 BLE Sense have sensors or antennas that can be affected by the Qwiic Shield's placement on top such that you may want to consider placing the Qwiic Shield below your Arduino Nano.

Once you have soldered headers to your shield and connected it to your Nano, it's time to start connecting some Qwiic devices! Below you can see the Qwiic Shield attached to an Arduino Nano Every using some female and male headers with a couple of Qwiic devices attached.

devices_7

Resources and Going Further

For more information, take a look at the resources below.

If you are having trouble getting your Qwiic devices to connect using your newly assembled Qwiic Shield, you may want to take a look at these tutorials for help troubleshooting and reworking your shield.

מק"ט יצרן # 16130
SPARKFUN QWIIC SHIELD FOR ARDUIN
SparkFun Electronics
מק"ט יצרן # HDR100IMP40F-G-V-TH
CONN HDR 40POS 0.1 GOLD PCB
Chip Quik Inc.
מק"ט יצרן # 15712
GPS BREAKOUT NEO-M9N QWIIC U.FL
SparkFun Electronics
מק"ט יצרן # 15805
TEMPERATURE SENSOR TMP117 QWIIC
SparkFun Electronics
מק"ט יצרן # 15290
QWIIC KEYPAD - 12 BUTTON
SparkFun Electronics
מק"ט יצרן # 14427
QWIIC CABLE - 100MM
SparkFun Electronics
מק"ט יצרן # 14428
QWIIC CABLE - 200MM
SparkFun Electronics
מק"ט יצרן # 14426
QWIIC CABLE - 50MM
SparkFun Electronics
מק"ט יצרן # 14429
QWIIC CABLE - 500MM
SparkFun Electronics
מק"ט יצרן # 14425
QWIIC CABLE - BREADBOARD JUMPER
SparkFun Electronics
מק"ט יצרן # 14495
QWIIC ADAPTER
SparkFun Electronics
מק"ט יצרן # HDR100IMP40M-G-V-TH
CONN HEADER VERT 40POS 2.54MM
Chip Quik Inc.
מק"ט יצרן # 17261
FLEXIBLE QWIIC CABLE - FEMALE JU
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.