Maker.io main logo

Star Fragment IoT Lamp

63

2023-05-16 | By Adafruit Industries

License: See Original Project 3D Printing Addressable LEDs Programmers

Courtesy of Adafruit

Guide by Ruiz Brothers

Overview

Inspired by Star Fragments from video games such as Zelda: Breath of the Wild and Animal Crossing: ‎New Horizons, this fully 3D printed star shaped lamp uses a QT Py ESP32-S2 and NeoPixel LEDs to turn ‎on when the sun rises and off when it sets.‎

 

The CircuitPython code uses the Open-Meteo weather API to get location data for requesting the ‎sunrise and sunset times. This IoT project knows when to light up and turn off, effectively automating ‎a nightstand lamp.‎

remotes_1

The core of the star fragment is a dodecahedron that has 12 hollow spikes that snap fit together and ‎are 3D printed without any support material.‎

A 3D printed mount houses two NeoPixel stick PCBs and snap fits into the bottom of the ‎dodecahedron.‎

outside_2

outside_3

Parts from Adafruit

Following parts are used in this project.‎

  • QT Py ESP32-S2
  • ‎NeoPixel Driver BFF
  • ‎2x NeoPixel Sticks
  • ‎‎3-pin JST cable

parts_4

This project requires two 8x NeoPixel LED sticks.‎

CircuitPython

CircuitPython is a derivative of MicroPython designed to simplify experimentation and education on ‎low-cost microcontrollers. It makes it easier than ever to get prototyping by requiring no upfront ‎desktop software downloads. Simply copy and edit files on the CIRCUITPY drive to iterate.‎

CircuitPython Quickstart

Follow this step-by-step to quickly get CircuitPython running on your board.‎

Download the latest version of CircuitPython for this board via circuitpython.org

Click the link above to download the latest CircuitPython UF2 file.‎

Save it wherever is convenient for you.‎

reset_5

assets_6

Plug your board into your computer, using a known-good data-sync cable, directly, or via an adapter if ‎needed.‎

Click the reset button once (highlighted in red above), and then click it again when you see the RGB ‎status LED(s) (highlighted in green above) turn red (approximately half a second later). Sometimes it ‎helps to think of it as a "slow double-click" of the reset button.‎

For this board, tap reset and wait for the LED to turn purple, and as soon as it turns purple, tap reset ‎again. The second tap needs to happen while the LED is still purple.‎

Once successful, you will see the RGB status LED(s) turn green (highlighted in green above). If you see ‎red, try another port, or if you're using an adapter or hub, try without the hub, or different adapter or ‎hub.‎

If double-clicking doesn't work the first time, try again. Sometimes it can take a few tries to get the ‎rhythm right!‎

A lot of people end up using charge-only USB cables and it is very frustrating! Make sure you have a ‎USB cable you know is good for data sync.‎

If after several tries, and verifying your USB cable is data-ready, you still cannot get to the bootloader, ‎it is possible that the bootloader is missing or damaged. Check out the Install UF2 Bootloader page for ‎details on resolving this issue.‎

You will see a new disk drive appear called QTPYS2BOOT.‎

Drag the adafruit_circuitpython_etc.uf2 file to QTPYS2BOOT.‎

uf2install_7

The BOOT drive will disappear, and a new disk drive called CIRCUITPY will appear.

That's it!‎

boot_8

Create Your settings.toml File

If you've worked on WiFi projects with CircuitPython before, you're probably familiar with the ‎secrets.py file. This file is a Python file that is stored on your CIRCUITPY drive that contains all of your ‎secret WiFi information, such as your SSID, SSID password and any API keys for IoT services. ‎

As of CircuitPython 8, there is support for a settings.toml file. Similar to secrets.py, the settings.toml ‎file separates your sensitive information from your main code.py file.

Your settings.toml file should be stored in the main directory of your CIRCUITPY drive. It should not be in a folder.

settings.toml File Example

Here is an example on how to format your settings.toml file.‎

Download File‎

Copy Code
# Comments are supported
CIRCUITPY_WIFI_SSID="guest wifi"
CIRCUITPY_WIFI_PASSWORD="guessable"
CIRCUITPY_WEB_API_PORT=80
CIRCUITPY_WEB_API_PASSWORD="passw0rd"
test_variable="this is a test"
thumbs_up="\U0001f44d"

In a settings.toml file, it's important to keep these factors in mind:‎

  • Strings are wrapped in double quotes; ex: "your-string-here"
  • ‎Integers are not quoted and may be written in decimal with optional sign (+1, -1, 1000) or hexadecimal ‎‎(0xabcd).‎
    • Floats, octal (0o567) and binary (0b11011) are not supported.‎
  • Use \u escapes for weird characters, \x and \ooo escapes are not available in .toml files
    • Example: \U0001f44d for (thumbs up emoji) and \u20ac for € (EUR sign)
  • ‎Unicode emoji, and non-ASCII characters, stand for themselves as long as you're careful to save in ‎‎"UTF-8 without BOM" format‎‎

‎When your settings.toml file is ready, you can save it in your text editor with the .toml extension.‎

dot_9

Accessing Your settings.toml Information in code.py

In your code.py file, you'll need to import the os library to access the settings.toml file. Your settings ‎are accessed with the os.getenv() function. You'll pass your settings entry to the function to import it ‎into the code.py file.‎

Download File

Copy Code
import os

print(os.getenv("test_variable"))

output_10

In the upcoming CircuitPython WiFi examples, you'll see how the settings.toml file is used for ‎connecting to your SSID and accessing your API keys.‎

Code the Star Fragment Lamp

hero_11

Once you've finished setting up your QT Py ESP32-S2 with CircuitPython, you can access the code and ‎necessary libraries by downloading the Project Bundle.‎

To do this, click on the Download Project Bundle button in the window below. It will download to your ‎computer as a zipped folder.‎

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2023 Liz Clark for Adafruit Industries
# SPDX-License-Identifier: MIT

import os
import ssl
import time
import microcontroller
import board
import wifi
import socketpool
import adafruit_requests
import neopixel
import simpleio
from adafruit_ticks import ticks_ms, ticks_add, ticks_diff
from adafruit_io.adafruit_io import IO_HTTP

# latitude
lat = 42.36
# longitude
long = -71.06

# neopixel setup
NUMPIXELS = 30 # number of neopixels
BRIGHTNESS = 0.5 # A number between 0.0 and 1.0, where 0.0 is off, and 1.0 is max.
PIN = board.A3 # This is the default pin on the NeoPixel Driver BFF.

pixels = neopixel.NeoPixel(PIN, NUMPIXELS, brightness=BRIGHTNESS, auto_write=False)

# turn on NeoPixels on boot to check wiring
pixels.fill((255, 125, 0))
pixels.show()

# API request to open-meteo
weather_url = "https://api.open-meteo.com/v1/forecast?"
# pass latitude and longitude
# will return sunrise and sunset times
weather_url += "latitude=%d&longitude=%d&timezone=auto&daily=sunrise,sunset" % (lat, long)

# connect to SSID
wifi.radio.connect(os.getenv('CIRCUITPY_WIFI_SSID'), os.getenv('CIRCUITPY_WIFI_PASSWORD'))

pool = socketpool.SocketPool(wifi.radio)
requests = adafruit_requests.Session(pool, ssl.create_default_context())

pool = socketpool.SocketPool(wifi.radio)

# adafruit IO info
aio_username = os.getenv('aio_username')
aio_key = os.getenv('aio_key')
location = "America/New York"

# io HTTP for getting the time from the internet
io = IO_HTTP(aio_username, aio_key, requests)

def reset_on_error(delay, error):
print("Error:\n", str(error))
print("Resetting microcontroller in %d seconds" % delay)
time.sleep(delay)
microcontroller.reset()

# function for making http requests with try/except
def get_request(tries, ping):
for i in range(tries):
try:
n = ping
except Exception as error:
print(error)
time.sleep(10)
if i < tries - 1:
continue
raise
break
return n

# get the time on start-up
# pylint: disable=broad-except
try:
now = get_request(5, io.receive_time())
except Exception as e:
reset_on_error(10, e)
print(now)
today = now.tm_mday

# function to make a request to open-meteo
def sun_clock():
# make the API request
response = get_request(5, requests.get(weather_url))
# packs the response into a JSON
response_as_json = response.json()
# gets sunrise
_rise = response_as_json['daily']['sunrise'][0]
# gets sunset
_set = response_as_json['daily']['sunset'][0]
return _rise, _set

# initial API call
try:
sunrise, sunset = sun_clock()
except Exception as e:
reset_on_error(10, e)

print(sunrise)
print(sunset)

# the sunrise/sunset time is returned as a JSON aka a string
# this function chops up the string to get the hours and minutes as integers
def divide_time(z):
string_time = z.split("-")
clock_time = string_time[2].split("T")
int_time = clock_time[1].split(":")
event_time = time.struct_time(
(int(string_time[0]), int(string_time[1]), int(clock_time[0]), int(int_time[0]),
int(int_time[1]), 0, -1, -1, False)
)
# print(event_time)
return event_time

rise_time = divide_time(sunrise)
set_time = divide_time(sunset)

# function that tracks how many hours/minutes until sunrise or sunset
def sun_countdown(sun_event):
n = get_request(5, io.receive_time())
remaining = time.mktime(sun_event) - time.mktime(n)
r = remaining
# print(remaining)
# calculate the seconds remaining
secs_remaining = remaining % 60 # pylint: disable=unused-variable
remaining //= 60
# calculate the minutes remaining
minutes_until = remaining % 60
remaining //= 60
# calculate the hours remaining
hours_until = remaining % 24
remaining //= 24
return r, hours_until, minutes_until, n
try:
total_until_rise, hours_until_sunrise, mins_until_sunrise, now = sun_countdown(rise_time)
except Exception as e:
reset_on_error(10, e)
try:
total_until_set, hours_until_sunset, mins_until_sunset, now = sun_countdown(set_time)
except Exception as e:
reset_on_error(10, e)

# red and yellow color percentage for neopixels
percent_red = 0
percent_yellow = 0

print(total_until_set)
# check to see if the star fragment should be lit up on start-up
if total_until_set < 0:
print("star glow true")
star_glow = True
percent_red = 255
percent_yellow = 125
# turn neopixels on using RGB values
pixels.fill((percent_red, percent_yellow, 0))
pixels.show()
else:
print("star glow false")
star_glow = False
percent_red = 0
percent_yellow = 0
# turn neopixels on using RGB values
pixels.fill((percent_red, percent_yellow, 0))
pixels.show()

# ticks time tracker
clock = ticks_ms()

# tracker for initial start-up state
first_run = True

# 15 minutes in milliseconds
time_check = 900000
# state to tell if it's after midnight yet before sunrise
looking_for_sunrise = False

while True:
try:
# if it's daytime
if not star_glow:
# every 15 minutes...
if first_run or ticks_diff(ticks_ms(), clock) > time_check:
print("pinging Open-Meteo")
sunrise, sunset = sun_clock()
(total_until_set, hours_until_sunset,
mins_until_sunset, now) = sun_countdown(set_time)
print(now)
print("%d hour(s) until sunset" % hours_until_sunset)
print("%d minutes(s) until sunset" % mins_until_sunset)
print(sunset)
print(percent_red)
print()
# less than an hour until sunset...
if hours_until_sunset in (0, 23):
# check every minute
time_check = 300000
# map color to ramp up in brightness over the course of the final hour
percent_red = simpleio.map_range(mins_until_sunset, 59, 0, 0, 255)
percent_yellow = simpleio.map_range(mins_until_sunset, 59, 0, 0, 125)
# if the sun has set..
if total_until_set < 0:
percent_red = 255
percent_yellow = 125
time_check = 900000
star_glow = True
print("star is glowing")
# otherwise just keep checking every 15 minutes
else:
time_check = 900000
percent_red = 0
percent_yellow = 0
if first_run:
first_run = False
else:
# reset clock
clock = ticks_add(clock, time_check)
# if it's nighttime...
else:
if first_run or ticks_diff(ticks_ms(), clock) > time_check:
if today != now.tm_mday or (first_run and now.tm_hour < rise_time.tm_hour):
today = now.tm_mday
looking_for_sunrise = True
# begin tracking the incoming sunrise
if looking_for_sunrise:
print("pinging Open-Meteo")
sunrise, sunset = sun_clock()
(total_until_rise, hours_until_sunrise,
mins_until_sunrise, now) = sun_countdown(rise_time)
print(now)
print("%d hour(s) until sunrise" % hours_until_sunrise)
print("%d minutes(s) until sunrise" % mins_until_sunrise)
print(sunrise)
print(now)
print()
# less than an hour until sunset...
if hours_until_sunrise in (0, 23):
# check every minute
time_check = 300000
# map color to decrease brightness over the course of the final hour
percent_red = simpleio.map_range(mins_until_sunrise, 59, 0, 255, 0)
percent_yellow = simpleio.map_range(mins_until_sunrise, 59, 0, 125, 0)
# if the sun has risen..
if total_until_rise < 0:
percent_red = 0
percent_yellow = 0
time_check = 900000
star_glow = False
looking_for_sunrise = False
print("star is off")
# otherwise just keep checking every 15 minutes
# and keep neopixels on
else:
time_check = 900000
percent_red = 255
percent_yellow = 125
# otherwise just keep checking every 15 minutes
# and keep neopixels on
else:
now = get_request(5, io.receive_time())
print("not looking for sunrise")
print(now)
print()
time_check = 900000
percent_red = 255
percent_yellow = 125
if first_run:
first_run = False
else:
# reset clock
clock = ticks_add(clock, time_check)
# turn neopixels on using RGB values
pixels.fill((percent_red, percent_yellow, 0))
pixels.show()
except Exception as e:
reset_on_error(10, e)

View on GitHub

Upload the Code and Libraries to the QT Py ESP32-S2‎

After downloading the Project Bundle, plug your QT Py ESP32-S2 into the computer's USB port with a ‎known good USB data+power cable. You should see a new flash drive appear in the computer's File ‎Explorer or Finder (depending on your operating system) called CIRCUITPY. Unzip the folder and copy ‎the following items to the QT Py ESP32-S2's CIRCUITPY drive. ‎

  • lib folder
  • code.py

Your QT Py ESP32-S2 CIRCUITPY drive should look like this after copying the lib folder and the code.py ‎file.‎

circuitpy_12

Add Your settings.toml File

As of CircuitPython 8, there is support for Environment Variables. These Environmental Variables are ‎stored in a settings.toml file. Similar to secrets.py, the settings.toml file separates your sensitive ‎information from your main code.py file. Add your settings.toml file as described in the Create Your ‎settings.toml File page earlier in this guide. You'll need to include your CIRCUITPY_WIFI_SSID, ‎CIRCUITPY_WIFI_PASSWORD, aio_username, and aio_key in the file.‎

Download File

Copy Code
CIRCUITPY_WIFI_SSID = "your-wifi-ssid-here"
CIRCUITPY_WIFI_PASSWORD = "your-wifi-password-here"

aio_username = "your-Adafruit-IO-username-here"
aio_key = "your-Adafruit-IO-key-here"

How the CircuitPython Code Works

The Open-Meteo weather API uses latitude and longitude to determine your location when creating ‎an API request. At the top of the code, you can add your latitude and longitude coordinates by editing ‎the lat and long variables.‎

Download File

Copy Code
# latitude
lat = 42.36
# longitude
long = -71.06

weather_url is a string that holds the Open-Meteo API request. It passes the latitude and longitude ‎variables and requests the sunrise and sunset times.‎

Download File

Copy Code
# API request to open-meteo
weather_url = "https://api.open-meteo.com/v1/forecast?"
# pass latitude and longitude
# will return sunrise and sunset times
weather_url += "latitude=%d&longitude=%d&timezone=auto&daily=sunrise,sunset" % (lat, long)

Internet Connect!‎

The QT Py ESP32-S2 connects to your network by passing your SSID name and SSID password ‎information from the settings.toml file. io is instantiated as an Adafruit IO HTTP object by passing your ‎IO username and password from the settings.toml file as well. Adafruit IO is used to get the current ‎time.‎

Download File

Copy Code
#  connect to SSID
wifi.radio.connect(os.getenv('CIRCUITPY_WIFI_SSID'), os.getenv('CIRCUITPY_WIFI_PASSWORD'))

pool = socketpool.SocketPool(wifi.radio)
requests = adafruit_requests.Session(pool, ssl.create_default_context())

pool = socketpool.SocketPool(wifi.radio)

# adafruit IO info
aio_username = os.getenv('aio_username')
aio_key = os.getenv('aio_key')
location = "America/New York"

# io HTTP for getting the time from the internet
io = IO_HTTP(aio_username, aio_key, requests)

Error Checking

The reset_on_error() function takes an Exception error and resets the QT Py depending on the delay ‎time. ‎

The get_request() function uses a try/except loop to attempt an HTTP request. In the event of an ‎error, the request will be attempted again after a delay. Once the number of tries has been exceeded, ‎then the loop breaks.‎

Download File

Copy Code
def reset_on_error(delay, error):
print("Error:\n", str(error))
print("Resetting microcontroller in %d seconds" % delay)
time.sleep(delay)
microcontroller.reset()

# function for making http requests with try/except
def get_request(tries, ping):
for i in range(tries):
try:
n = ping
except Exception as error:
print(error)
time.sleep(10)
if i < tries - 1:
continue
raise
break
return n

These two functions are utilized together in a try/except loop for each HTTP request. If the try/except ‎loop exceeds the tries in get_request(), then reset_on_error() is called and the QT Py resets itself.‎

Download File

Copy Code
try:
now = get_request(5, io.receive_time())
except Exception as e:
reset_on_error(10, e)

When and Where Is The Sun?‎

The sun_clock() function makes the Open-Meteo API request and returns that day's sunrise and ‎sunset timestamp.‎

Download File

Copy Code
# function to make a request to open-meteo
def sun_clock():
# make the API request
response = get_request(5, requests.get(weather_url))
# packs the response into a JSON
response_as_json = response.json()
# gets sunrise
_rise = response_as_json['daily']['sunrise'][0]
# gets sunset
_set = response_as_json['daily']['sunset'][0]
return _rise, _set

However, the sunrise and sunset timestamps are returned as strings, which isn't very helpful for doing ‎math. The divide_time() function chops up the string and returns a struct_time object.‎

Download File

Copy Code
def divide_time(z):
string_time = z.split("-")
clock_time = string_time[2].split("T")
int_time = clock_time[1].split(":")
event_time = time.struct_time(
(int(string_time[0]), int(string_time[1]), int(clock_time[0]), int(int_time[0]),
int(int_time[1]), 0, -1, -1, False)
)
# print(event_time)
return event_time

Then, the sun_countdown() function calculates the time remaining until either sunrise or sunset.‎

Download File

Copy Code
# function that tracks how many hours/minutes until sunrise or sunset
def sun_countdown(sun_event):
n = get_request(5, io.receive_time())
remaining = time.mktime(sun_event) - time.mktime(n)
r = remaining
# print(remaining)
# calculate the seconds remaining
secs_remaining = remaining % 60 # pylint: disable=unused-variable
remaining //= 60
# calculate the minutes remaining
minutes_until = remaining % 60
remaining //= 60
# calculate the hours remaining
hours_until = remaining % 24
remaining //= 24
return r, hours_until, minutes_until, n

Before the loop, it's determined if the sun has already set. This sets the state for star_glow, which is ‎used in the loop to turn the NeoPixels on or off.‎

Download File

Copy Code
# check to see if the star fragment should be lit up on start-up
if total_until_set < 0:
print("star glow true")
star_glow = True
percent_red = 255
percent_yellow = 125
# turn neopixels on using RGB values
pixels.fill((percent_red, percent_yellow, 0))
pixels.show()
else:
print("star glow false")
star_glow = False
percent_red = 0
percent_yellow = 0
# turn neopixels on using RGB values
pixels.fill((percent_red, percent_yellow, 0))
pixels.show()

The Loop

In the loop, ticks_ms() is used to track time. Every 15 minutes, requests are sent to Open-Meteo and ‎Adafruit IO to retrieve the sunrise and sunset times and the current time. Depending on whether or ‎not star_glow is True determines if sunrise or sunset is tracked.‎

Download File

Copy Code
while True:
try:
# if it's daytime
if not star_glow:
# every 15 minutes...
if first_run or ticks_diff(ticks_ms(), clock) > time_check:
print("pinging Open-Meteo")
sunrise, sunset = sun_clock()
(total_until_set, hours_until_sunset,
mins_until_sunset, now) = sun_countdown(set_time)
print(now)
print("%d hour(s) until sunset" % hours_until_sunset)
print("%d minutes(s) until sunset" % mins_until_sunset)
print(sunset)
print(percent_red)
print()

Mapping Color to Time

When there is less than an hour until sunrise or sunset, Open-Meteo and Adafruit IO begin to be ‎pinged every 5 minutes. The NeoPixels begin to either dim or brighten during that hour countdown. ‎Their red and green values are mapped to the minutes remaining.‎

Once the sun event has been reached, the NeoPixels are set to fully yellow or fully off, the ‎time_check is reset to 15 minutes, and the state of star_glow is updated.‎

Download File

Copy Code
# less than an hour until sunset...
if hours_until_sunset in (0, 23):
# check every minute
time_check = 300000
# map color to ramp up in brightness over the course of the final hour
percent_red = simpleio.map_range(mins_until_sunset, 59, 0, 0, 255)
percent_yellow = simpleio.map_range(mins_until_sunset, 59, 0, 0, 125)
# if the sun has set..
if total_until_set < 0:
percent_red = 255
percent_yellow = 125
time_check = 900000
star_glow = True
print("star is glowing")

What Day Is It?‎

There is some additional logic in place to prevent errors while the star is glowing. Once the day changes ‎‎(aka once it's past midnight), the looking_for_sunrise state is set to True to begin checking Open-‎Meteo for the sunrise and sunset times for the new day.‎

Download File

Copy Code
if first_run or ticks_diff(ticks_ms(), clock) > time_check:
if today != now.tm_mday or (first_run and now.tm_hour < rise_time.tm_hour):
today = now.tm_mday
looking_for_sunrise = True
# begin tracking the incoming sunrise
if looking_for_sunrise:
print("pinging Open-Meteo")
sunrise, sunset = sun_clock()
(total_until_rise, hours_until_sunrise,
mins_until_sunrise, now) = sun_countdown(rise_time)

While the code waits for the new day, the time is checked every 15 minutes and the NeoPixels are ‎fully yellow.‎

Download File

Copy Code
# otherwise just keep checking every 15 minutes
# and keep neopixels on
else:
now = get_request(5, io.receive_time())
print("not looking for sunrise")
print(now)
print()
time_check = 900000
percent_red = 255
percent_yellow = 125

Circuit Diagram

The diagram below provides a general visual reference for wiring of the components once you get to ‎the Assembly page. This diagram was created using the software package Fritzing.‎

Adafruit Library for Fritzing

Use Adafruit's Fritzing parts library to create circuit diagrams for your projects. Download the library or ‎just grab individual parts. Get the library and parts from GitHub - Adafruit Fritzing Parts.‎

You'll forgo socket headers in the final assembly and connect the QT Py and BFF directly with header ‎pins.‎

diagram_13

Wired Connections

The QT Py is powered by a 5V 1A power supply wall adapter. ‎

NeoPixel Stick to NeoPixel Stick

  • DATA OUT to DATA In
  • GND to GND pin
  • ‎5V to 5V pin‎

NeoPixel Stick to BFF NeoPixel Drive

The power, data, and ground connections from the first NeoPixel stick connect directly to the 3-pin JST ‎port on the NeoPixel BFF board.‎

CAD Files

CAD Assembly

The two NeoPixel sticks are secured to the NeoPixel Stick Mount with hardware screws and nuts. The ‎NeoPixel mount snap fits into the bottom side of the star core. Eleven spikes snap fit into the star core. ‎The star bottom piece snap fits into the NeoPixel stick mount. The star fragment assembly rests onto ‎the stand. The stand is secured to the star case top cover with machine screws. The star case top and ‎bottom covers snap fit onto the star case frame. ‎

star_14

CAD Parts List

STL files for 3D printing are oriented to print "as-is" on FDM style machines. Parts are designed to 3D ‎print without any support material using PLA filament. Original design source may be downloaded ‎using the links below.‎

  • NeoPixel Stick Mount.stl
  • simple-case-bottom.stl
  • simple-case-frame.stl
  • simple-case-top.stl
  • Star-Bottom.stl
  • Star-Case-Bottom.stl
  • Star-Case-Frame.stl
  • Star-Case-Top.stl
  • Star-Core.stl
  • Star-Spike.stl
  • Star-Stand.stl

case_15

slide_16

Download STLs.zip

Download CAD Source

Transparent Filament

For best illumination, we suggest printing the Star-Core and NeoPixel Stick Mount parts in translucent / ‎transparent PLA filament.‎

The star spikes were 3D printed in a yellow-colored PLA filament.‎

bedsize_17

Build Volume

The parts require a 3D printer with a minimum build volume.‎

  • ‎138mm (X) x 132mm (Y) x 42mm (Z)‎

brim_18

Bed Adhesion

Applying brim to the star spikes can help improve bed adhesion. A minimum of 6 perimeters is ‎suggested to keep the part from coming off the bed of the 3D printer.‎

bed_19

Headers Assembly

Headers for QT Py and BFF

Trim the included strip of headers to create two 1x7 headers.‎

headers_20

Install Headers to QT Py

Insert the two strips of header pins to the bottom of the QT Py PCB.‎

install_21

Install NeoPixel Driver BFF

Place the NeoPixel Driver BFF board under the QT Py to get a sense of the correct orientation. ‎

install_22

Soldering Headers

Use a breadboard to help keep the two strips of header pins straight when soldering them to the QT ‎Py.‎

headers_23

Solder NeoPixel Driver BFF to QT Py

Carefully solder the header pins from the QT Py to the NeoPixel Driver BFF.‎

soldered_24

NeoPixel Wiring

Short Cable for NeoPixels

The two NeoPixel sticks will be daisy chained using a short 3-wire ribbon cable.‎

Peel three wires from the 10-wire ribbon cable to create a short 3-pin cable for connecting the two ‎NeoPixel sticks together.‎

short_25

JST Cable for NeoPixels

Separate three wires from the 10-wire ribbon cable to create a long cable extension for the 3-pin JST ‎cable. ‎

Cut the 3-wire ribbon cable to the desired length. Make sure it's a has a minimum length of 6in (15cm). ‎

A 3-pin JST cable will connect the NeoPixel sticks to the NeoPixel Driver BFF board.‎

cables_26

Solder Short Cable

Connect the short 3-wire ribbon cable to one of the NeoPixel sticks by soldering to the GND, 5VDC and ‎DOUT pads.‎

solder_27

Solder Short Cable (Continued)‎

Connect the other end of the short ribbon cable to the second NeoPixel stick by soldering to the GND, ‎‎5VDC and DIN pads.‎

The connections between the two boards are:‎

  • GND to GND
  • 5VDC to 5VDC‎D
  • OUT to DIN

solder_28

Soldered NeoPixel Sticks

Double check the short cable has been soldered to the correct pads.‎

soldered_29

Solder 3-pin JST Extension

Connect the long ribbon cable to the 3-pin JST cable by soldering the individual wires to the red, black ‎and white colored wires. ‎

Use pieces of heat shrink tubing to insulate the exposed wire.‎

soldering_30

‎3-pin JST Cable

Double check the soldered wires have a good and strong connection.‎

ext_31

Connect JST Cable to NeoPixels

Solder the three wires from the JST cable/extension to the NeoPixel stick with the DIN pad. Connect ‎red wire extension to 5VDC, black wire extension to GND and white wire extension to the DIN pad.‎

solder_32

Wired NeoPixel Sticks

Take a moment to double check the wired connections have been properly soldered.‎

soldered_33

Assembly

Hardware for NeoPixel Mount

You'll use the following hardware to secure the NeoPixel sticks to the 3D printed mount.‎

  • ‎2x M2 x 12mm long screws
  • ‎‎2x M2 hex nuts
  • ‎‎4x M2 washers‎

screws_34

Install Cable to NeoPixel Mount

Insert the 3-pin JST through the center opening of the 3D printed mount and pull it all the way through.‎

install_35

Mounting NeoPixel

Place both NeoPixel sticks onto the 3D printed mount and line up the mounting holes.‎

installing_36

Insert the M2 screws through the NeoPixel sticks and 3D printed mount with the washers fitted in ‎between. The washer will allow airflow to help with heat dissipation to prevent the 3D print from ‎warping. ‎

setup_37

Secure NeoPixels

Fasten M2 hex nuts onto the threads of the screws and use a screwdriver to secure them together.‎

secure_38

Assembled NeoPixel Holder

Take a moment to inspect the NeoPixel holder assembly and ensure it has been properly secured.‎

secured_39

Install NeoPixel Holder

Locate the bottom side of the 3D printed star core. It's the surface that touched the 3D printer's bed.‎

Insert the NeoPixel holder through the bottom side of the star core and firmly press it through the ‎edges.‎

install_40

Install Bottom Spike

Insert the JST cable through the hole on the side of the 3D printed bottom spike and pull it all the way ‎through.‎

Orient the bottom spike so the protruding lips are lined up with the NeoPixel holder.‎

Firmly press the bottom spike into the star core until the surfaces sit flush.‎

install_41

Install Top Spike

Insert one of the eleven spikes to the top side of the star core. Firmly press the spike into the star core ‎until the surfaces are flush with each other.‎

top_42

Install Another Spike

Proceed to install one of remaining spikes into another side of the star core ensuring the surfaces are ‎flush.‎

spike-2_43

Install Spikes (Continued)

Continue to install spikes by press fitting them into the remaining sides of the star core.‎

spike-5_44

 

Installed Spikes

Double check all of the spikes have been properly installed onto the star core.‎

installed_45

Connect JST to BFF

Grab the 3-pin JST plug from the NeoPixels and connect it to the NeoPixel Driver BFF.‎

connect_46

 

Connect USB to QT Py

Plug in a USB-C cable to the USB port on QT Py board.‎

connect_47

Power Test

Plug the other end of the USB cable into a 5V 1A (minimum, higher current rating is fine to use) USB ‎power supply to turn on the circuit. ‎

star-power_48

Simple Case Setup

Use the simple snap fit case if you prefer to use the star fragment off the stand.‎

Insert the JST plug from the NeoPixel through the smaller hole on the side of the case.‎

Insert the USB cable through the bigger hole on the side of the case.‎

case_49

case-set_50

 

Lamp Stand Setup

Insert the USB-C extension cable through the hole on the side of the lamp stand base. Use the ‎included hex nut to secure the cable.‎

lamp_51

lamp_52

Lamp Base Bottom Install

Line up the snap fit edges of the bottom cover with the lamp base. Firmly press bottom cover to snap ‎fit them together. ‎

bottom_53

bottom_54

Hardware for Lamp Stand

Use three M3 x 6mm long machine screws to secure the stand to the lamp base top cover.‎

stand_55

Secure Lamp Stand to Top Cover

Place the lamp stand over the base top cover and line up the three mounting holes.‎

Insert and fasten the M3 screws through the bottom of the top cover to secure the stand to the top ‎cover.‎

secure_56

Install NeoPixel Cable to Lamp Stand

Insert the NeoPixel cable through the lamp stand and pull it through the other end.‎

install_57

Connect NeoPixel and QT Py

Proceed to connect the 3-pin JST cable to the NeoPixel Driver BFF and the USB-C extension cable to ‎the QT Py.‎

connect_58

Install PCBs into Lamp Base

Place the QT Py and NeoPixel Driver BFF into the lamp case with the extension cable neatly coiled.‎

fit_59

Install Top Cover to Lamp Base

Line up the snap fit edges of the top cover with the lamp base and firmly press to snap fit them ‎together.‎

snap_60

Install Star Fragment to Lamp Stand

Pull on the cable from the NeoPixels through the openings on the bottom cover until the star ‎fragment can rest on the lamp stand.‎

Orient the star fragment so it can rest over the tapered edges of the lamp stand.‎

Optionally use glue to permanently adhere the star fragment to the lamp stand.‎

test_61

מק"ט יצרן # 4336
JST PH 3-PIN PLUG-PLUG CABLE
Adafruit Industries LLC
MEMORY CARD SDHC 16GB CLASS 10
מק"ט יצרן # 2693
MEMORY CARD SDHC 16GB CLASS 10
Adafruit Industries LLC
מק"ט יצרן # 1426
ADDRESS LED MODULE SERIAL RGB
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.