Maker.io main logo

Wakanda Forever Game

104

2023-04-18 | By Adafruit Industries

License: See Original Project Displays LED Strips

Courtesy of Adafruit

Guide by John Park

Overview

Code your own Black Panther: Wakanda Forever game using ‎MakeCode Arcade!‎

Start with this great tutorial, and then customize or build your own ‎totally new game using the excellent art assets provided.‎

The game build in this guide also includes optional NeoPixel ‎Vibranium Gauntlet blasts when run on the PyGamer!‎

 

game_2

Parts

If making a DIY NeoPixel Y-splitter, you'll need two JST PH 2mm 3-‎pin socket cables, and one JST PH 2mm 2-pin plug cable.‎

or:‎

Code the Game

code_3

Start Here

If you're new to MakeCode Arcade, check out this intro as well as ‎some of these Learn Guides on making games with MakeCode ‎Arcade.‎

You can also check out this great video playlist from Microsoft's ‎MakeCode team, as well as the MakeCode Arcade Game of the ‎Week series.‎

Wakanda Forever Game

Click the button below to open the game in the MakeCode Arcade ‎site in your web browser (it should open into a new window).‎

Wakanda Forever Game

You can play the game in the browser and then continue below if ‎you want to see how it's made and customize it.‎

Click on the Edit Code button in order to customize the code.‎

edit_4

code2_5

Extensions

Some extensions are used to add functionality to the program. From ‎the Advanced category section, in the Extensions item, the following ‎are added:‎

  • Sprite scaling to allow re-sizing of the character sprites

  • Background scroll to create multi-plane camera background ‎layers

  • Light to use NeoPixel strips

  • Feather to add the Feather pins necessary to plug NeoPixel ‎strips into the PyGamer hardware

feather_6

backward_7

light_8

feather_9

Title Sequence Function

A function called title sequence is used to place all of the opening ‎title blocks in a single place that can be called from the main startup ‎block when the game begins.‎

The text sprite blocks create the three lines of text, "Black Panther", ‎‎"WAKANDA", and "FOREVER".‎

The sound block creates an ascending alert tone.‎

tone_10

BG Layers Setup Function

Using the Background Scroll extension, a set of different background ‎layers are created -- these were extracted from the tutorial image ‎using copy, paste, and erase!‎

This gives the game the illusion of depth using the parallax effect. ‎

layers_11

NeoPixel Setup Function

Add the Light extension to MakeCode Arcade. ‎

First, open the Advanced category section and click on the ‎Extensions item.‎

Next, click on the light extension, which adds the blocks we need.‎

Click the Light category to see the available blocks. Now you can ‎click on the "..." category under Light to get the NeoPixel strip blocks.‎

Create a function called NeoPixel setup and add the strip blocks ‎shown here.‎

setup_12

setup_13

setup_14

setup_15

Vibranium Gauntlet Blast Function

This function will be called when the NeoPixel strand shoots a blast -‎‎- this is done by advancing the bright "photon" pixel by three and ‎doing so ten times. The strand has 30 LEDs, so this will blast forward ‎through the whole strip.‎

function_16

Character Setup Function

In this function, the two-character sprites are created and defined as ‎‎"player" and "enemy", which are tags that are used for other ‎behaviors later.‎

The character sprites are then scaled up in size to make them ‎appear bigger on screen.‎

Shuri's position is set at the start, and the "stay on screen" flag is ‎set on so she can't be moved off screen.‎

Namor is set to follow Shuri with a speed of 40.‎

Finally, Shuri is set to be controlled with the d-pad at a velocity of 100 ‎on x and 220 on y.‎

character_17

speed_18

On Start

The on start loop runs once at the beginning of the game to set up ‎or run a number of commands and functions.‎

The started flag is set to false in order to prevent a button from ‎firing projectiles until the game has started.‎

The title sequence function is run, followed by the BG setup ‎function.‎

Then, after a short pause, the title text sprites are removed from the ‎screen, and then a long text is shown that says "Battle Namor! But ‎don't get hit!!".‎

The character setup function is run, and Shuri's life counter is set to ‎‎10.‎

The started variable is set to true, and then the NeoPixel ‎setup and Vibranium Gauntlet blast functions are called.‎

start_19

Namor Projectile Loop

All forever loops are run continuously once the game has started. ‎This one is used to have Namor fire projectiles at Shuri at a ‎randomized interval.‎

loop_20

Namor Motion Constraint

Since the follow loop is running constantly to have Namor move ‎toward Shuri in both x and y, we want to limit that motion to only the ‎y axis. This is done here by setting Namor's x position to 138 ‎constantly.‎

constraint_21

Fire Button

Whenever the A button is pressed, the check is made to see if the ‎game has started (based on the state of the started variable).‎

Then, if that check passes, a projectile is emitted from Shuri's sprit, ‎and sent on the x-axis at a velocity of 225 vx.‎

When the projectile hits a wall or sprite it is destroyed.‎

Each time the projectile is fired the Vibranium Gauntlet blast ‎function is called to light up the NeoPixel strip.‎

fire_22

Shuri Hit

If Shuri is hit by Namor's projectile, her life count decrements by one, ‎a sound effect is played, and Namor's position is reset to a random ‎location on the y-axis.‎

hit_23

Namor Hit

When Namor is hit by Shuri's projectile, the score is incremented by 1, ‎a sound effect is played, and Namor's position is reset.‎

hit_24

Shuri Wins

When the score reaches 10, the player wins! Namor is destroyed, a ‎‎"We are safe!" text is displayed, and Shuri proclaims, "WAKANDA ‎FOREVER".‎

Then, the confetti effect plays, and the game is set to over with the ‎WIN condition.‎

wins_25

Next Steps

Ready to up your game? For an added challenge, now try to add ‎features, such as extra life power-ups, add new levels, and adjust the ‎difficulty!‎

Build the PyGamer Case

case_26

Here's how to assemble the laser cut acrylic case for the PyGamer. ‎The kit comes with seven pieces of acrylic, and four screws and nuts. ‎You've gotten button caps to pick from (you'll pick four), and you'll ‎also want to connect the speaker and battery for the full portable ‎experience.‎

assemble_27

Prep

If you haven't already, remove the clear plastic screen protector film ‎from the PyGamer display.‎

display_28

display_29

Paper Protection

Remove the protective paper backing from both sides of all the ‎acrylic pieces.‎

paper_30

paper_31

paper_32

Speaker

Plug the speaker into the speaker port on the PyGamer.‎

Then, remove the white oval plastic ring to expose the adhesive and ‎press the speaker to the PyGamer where the silkscreen oval outline ‎indicates.‎

speaker_33

speaker_34

speaker_35

Battery

Plug the battery into the on-board connector. Very carefully, bend ‎the wires so that the battery fits the spot shown.‎

battery_36

battery_37

battery_38

Button Caps

Pick four of the button caps and click them into place on the square ‎shafts of the buttons. Which color combo will you choose?!‎

buttons_55

buttons_56

buttons_57

Case Layers

The case assembly is pretty simple. Place the clear top side piece on ‎as shown.‎

Next, place the smoked gray piece on.‎

case_39

case_40

Spacers

Flip the board over, then place the four spacer pieces onto the back ‎as shown.‎

spacers_41

spacers_42

Backing

The last piece to go on is the thin bottom layer with the Feather ‎header cutouts.‎

backing_43

Fasteners

Push the four screws through from front to back, being sure they go ‎through the holes in all layers and the PyGamer.‎

Screw on the nuts to secure things. Hand tight is fine -- you don't ‎want to crack anything by using excessive force.‎

fasteners_44

fasteners_45

secure_46

secure_47

secure_48

That's all there is to it -- you're ready to play with your PyGamer in its ‎excellent, stylish case!‎

Play on PyGamer with Vibranium ‎Blast Strips

 

 

First, follow this page to load the game onto your PyGamer or ‎PyBadge.‎

Plug the NeoPixel strip into the 3-pin JST connector marked D3 as ‎shown here.‎

plug_49Wakanda Forever Game

Turn on the PyGamer and the game will start. Once you get past the ‎loading screens, the NeoPixels will light up.‎

turn_50

lights_51

Advance DIY Double Strand Hack

Double Blasters

Despite being listed in the NeoPixel strip pin list, the D2 JST plug ‎can't be used in MakeCode Arcade at the moment. However, there's ‎another way to use double Vibranium Gauntlet blaster strips! Since ‎NeoPixels can run in parallel, a DIY wire y-splice will do the trick. See ‎this guide for more on wire splicing.‎

Here, the ground, 3.3V and data pins from the D3 JST port have been ‎spliced to two adapter cables.‎

By plugging in a pair of strips to the adapter, you get twice the ‎NeoPixel action! They will run identically to each other, which works ‎well in this case.‎

blasters_52

blasters_53

blasters_54

מק"ט יצרן # 4242
PYGAMER FOR MAKECODE ARCADE, CIR
Adafruit Industries LLC
מק"ט יצרן # 3919
ADDRESS LED STRIP SERIAL RGB
Adafruit Industries LLC
מק"ט יצרן # 4046
JST PH 3-PIN SOCKET TO COLOR COD
Adafruit Industries LLC
מק"ט יצרן # 4336
JST PH 3-PIN PLUG-PLUG CABLE
Adafruit Industries LLC
מק"ט יצרן # 4227
SPEAKER 8OHM 1W TOP PORT 96DB
Adafruit Industries LLC
מק"ט יצרן # 4238
CASE ACRYLIC BLK
Adafruit Industries LLC
מק"ט יצרן # 4277
PYGAMER STARTER KIT
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.