Maker.io main logo

Face Expression Detection Robot with Arduino UNO Q

637

2026-01-08 | By ShawnHymel

3D Printing Arduino

The new Arduino UNO Q is a fascinating combination of microcontroller and single-board computer. With a Qualcomm QRB2210 microprocessor (MPU) and an STM32U585 microcontroller (MCU) on the same board, the UNO Q gives you the horsepower to run modern AI workloads while still offering real-time control on the MCU side.

To test this hybrid capability, I built a small robot: a pan/tilt camera head that uses a USB webcam for face tracking and facial-expression recognition (many thanks to Jorvon Moss for creating the mechanical pan/tilt design!). When the robot sees you, it turns to face the largest (ideally nearest) detected face and changes its LED ring color based on the expression it thinks you’re making. Under the hood, the Qualcomm side runs a YOLOv11-nano while the microcontroller drives the servos and LEDs. This results in a robotic “head” that follows you around and reacts to your mood.

I was inspired by Cyril Engmann’s LuxoPi, which he showcased at this year’s Hackaday Supercon. LuxoPi, based on Pixar’s iconic Luxo Jr., is a lamp-like robot that reacts to users' movements, touch, expressions, and sounds. I wanted to demonstrate one part of this, reacting to facial expressions, on low-power hardware, which opens the possibility of running the robot off smaller batteries.

All mechanical (STL) files and code for this project can be found here: https://github.com/ShawnHymel/face-expression-detection-robot.

Arduino UNO Q Overview

The Arduino UNO Q sits in a new space between traditional makers’ boards and more complex embedded Linux platforms. On paper, the specs look impressive:

  • Qualcomm Dragonwing QRB2210 CPU (quad-core Arm Cortex-A53 at 2 GHz)
  • Qualcomm Adreno 702 GPU
  • 2 or 4 GB RAM
  • Integrated Wi-Fi and Bluetooth
  • A low-power STM32U585 microcontroller tightly coupled on the same board
  • A generous amount of GPIO (many are broken out on the back side of the board)

It’s tempting to treat it as a drop-in replacement for any other small Linux SBC: you can boot to a graphical desktop, plug in a keyboard and monitor, and treat it like a tiny computer. However, in practice, the UNO Q shines in headless applications (projects where you do not need a monitor or keyboard).

The MPU is ideal for computationally heavy tasks such as:

  • Running AI/ML inference (ONNX, PyTorch, TensorFlow Lite, etc.)
  • Performing computer vision tasks via USB cameras
  • Hosting lightweight local web servers or dashboards
  • Handling image preprocessing, networking, or multi-threaded applications

Meanwhile, the MCU side gives you what Linux often struggles with: deterministic real-time control. It’s excellent for:

  • Driving servos, motors, or other actuators
  • Reading sensors
  • Managing LEDs or tight timing loops
  • Handling low-latency control tasks in parallel with high-compute workloads

The two processors communicate through Arduino’s new Bridge system, which allows you to delegate fast, real-time tasks to the MCU and heavy computational loads to the MPU. It essentially sets up a remote procedure call (RPC) framework between the two devices, allowing you to call functions from one to the other.

This architecture makes the UNO Q particularly well-suited for robotics, especially if you require complex algorithms, such as vision processing and machine learning, to run on an integrated, low-power board. The face-tracking, expression-recognizing pan/tilt robot is a natural fit, as the MPU can handle image capture and inference while the MCU handles motion and LEDs.

The rest of this post will walk you through building the mechanical mount, retraining the YOLO object detection model, deploying it to the UNO Q, and running the face expression detection script.

Required Hardware

If you wish to recreate this project, you will need:

Set Up Arduino UNO Q

Before you start, I recommend following these instructions to install App Lab, connect the Arduino UNO Q to your computer via USB, and go through the setup process to connect the UNO Q to your WiFi and update the firmware.

Hardware Connections

Print the STL files on your 3D printer. Assemble the pan/tilt mount as shown.

Image of Face Expression Detection Robot with Arduino UNO Q

Connect the power pins of the LED ring and both servos to 5V. Connect the following pins:

  • Data Input of the LED ring to Arduino pin 4
  • Pan servo signal pin to Arduino pin 9
  • Tilt servo signal pin to Arduino pin 10

Connect the USB hub to the Arduino UNO Q. Connect the webcam to a USB port on the hub. Connect a USB-C cable to power to the PD port on the USB hub.

Image of Face Expression Detection Robot with Arduino UNO Q

If you configured WiFi on the UNO Q, it should power up, connect to your WiFi network, and start an SSH server that you can log into. We’ll use that to upload our code and run our application.

Retrain Machine Learning Model

While you might be able to find an off-the-shelf model pre-trained to detect human facial expressions, let’s try retraining our own! This will demonstrate how you can start with a pretrained object detection model, use transfer learning to retrain it to perform a similar task, and then export it in the ONNX format.

Start by downloading this repository: https://github.com/ShawnHymel/face-expression-detection-robot

Assuming you have a CUDA-capable NVIDIA graphics card, you can use the pre-configured Docker image to run Jupyter Lab and PyTorch in a container. Build and run the image with:

Copy Code
docker build -f Dockerfile.gpu -t fed-training-gpu .
docker run --rm -it --gpus all --shm-size=2g -p 8888:8888 -p 6006:6006 -v "${PWD}/workspace:/workspace" fed-training-gpu

With the Jupyter Lab server running, you can click on the URL shown in the terminal (likely the one starting with http://127.0.0.1:8888/lab?token=...) to open a browser for Jupyter Lab.

In Jupyter Lab, open workspace/notebooks/training.ipynb. Follow the instructions as you run through each cell (press shift+enter to run the cell). Note that you will need to create an account on Roboflow and manually download the Human Face Expression dataset.

Image of Face Expression Detection Robot with Arduino UNO Q

During the training process, you can connect to TensorBoard by browsing to localhost:6006. You can watch the loss and mAP over time.

Image of Face Expression Detection Robot with Arduino UNO Q

Training will take 30+ minutes (depending on your GPU) and should ultimately produce a trained model at workspace/models/model_with_nms.onnx.

Deploy Model and Run Application

Now, we'll copy the firmware project to the UNO Q and run it. Copy workspace/models/model_with_nms.onnx to firmware/face-detection-robot/model_with_nms.onnx.

Open a terminal (to be used as your SSH connection to the UNO Q). Enter the following (replace <UNO_Q_IP_ADDRESS>  with the IP address of your UNO Q board):

Copy Code
ssh arduino@ssh arduino@<UNO_Q_IP_ADDRESS>

Enter yes if asked to accept the SSH key fingerprint. Enter your UNO Q password.

In that terminal, create a new project folder on the UNO Q:

Copy Code
mkdir -p ~/ArduinoApps/face-detection-robot

From your host computer, open up a new terminal, navigate into this directory, and run the following (replace <UNO_Q_IP_ADDRESS>  with the IP address of your UNO Q board):

Copy Code
scp -r firmware/face-detection-robot/ arduino@<UNO_Q_IP_ADDRESS>:~/ArduinoApps

Now, we can use the Arduino App CLI to run and control apps. To start your program, run the following in the SSH terminal (connected to your UNO Q):

Copy Code
arduino-app-cli app start ~/ArduinoApps/face-detection-robot

Browse to <UNO_Q_IP_ADDRESS>:7000 to see the web UI, which should show a low-quality version of what the camera sees, along with bounding boxes and some framerate metrics. Try walking in front of the camera and making faces!

Image of Face Expression Detection Robot with Arduino UNO Q

You can check the logs with:

Copy Code
arduino-app-cli app logs ~/ArduinoApps/face-detection-robot

You can stop the application with:

Copy Code
arduino-app-cli app stop ~/ArduinoApps/face-detection-robot

Going Further

You might notice that the model does not detect some of your facial expressions. For me, it found “surprise” and “happy” easily, but struggled with the others. This is likely due to a combination of several factors, including data and model complexity (we’re using the smallest available YOLOv11). I recommend trying the following to increase the model accuracy:

  • Gather real photos (and label them appropriately!) from your intended deployment environment (e.g., your face in your office or home with a variety of lighting). Mix them in with the other training data.
  • Play with the hyperparameters used for training: try training for more epochs, adjust the learning rate schedule (especially for the fine-tuning step), or freezing different numbers of layers.

Object detection can be tricky, and lighting (or other environmental factors) can kill your accuracy. I hope this demo gets you started developing other edge AI and robotics projects with the Arduino UNO Q!

If you’d like to learn more about edge AI, check out this video.

מק"ט יצרן # 2853
ADDRESS LED RING SERIAL RGBW
Adafruit Industries LLC
מק"ט יצרן # SER0039
SERVOMOTOR RC 5V 9G METAL GEAR
DFRobot
מק"ט יצרן # 127B-USBC-MULTIPORT
RJ45 USB MULTIPORT ADAPTER
StarTech.com
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.