Maker.io main logo

Getting Started With STM32 and Nucleo Part 4-Working with ADC and DMA

3,943

2019-09-30 | By Maker.io Staff

As we continue the series with STM32, let’s take a look at how to use the analog-to-digital converter (ADC). At first, we set up a single conversion that samples the voltage from a potentiometer and transmits the raw value over UART. We can then read this information on a serial terminal.

We run into problems, however, when we want to sample analog voltages at a much faster rate. So, we introduce the concept of direct memory access (DMA) to help pipe data from the ADC (or any other peripheral) to memory.

We can also use the DMA controller the other way, too. We start by showing an example of reading a large buffer of test data out over UART via DMA. From there, we build a quick demo of filling a circular buffer with ADC readings with the DMA controller. We’ll simply peek at the buffer contents in the STM32CubeIDE debugger to show how the DMA can act without CPU intervention.

Related Items

Related Projects

Related Videos

Additional Resources

Download STM32CubeIDE: https://www.st.com/en/development-tools/stm32cubeide.html

STM32 HAL documentation (click on family from graphic and then Resources tab): https://www.st.com/en/embedded-software/stm32cube-mcu-mpu-packages.html

FreeRTOS documentation: https://www.freertos.org/

CMSIS-RTOS documentation: http://www.keil.com/pack/doc/CMSIS/RTOS2/html/index.html

Recommended Reading

מק"ט יצרן # NUCLEO-L476RG
NUCLEO-64 STM32L476RG EVAL BRD
STMicroelectronics
מק"ט יצרן # AK672M/2-2
CBL USB2.0 A PLG-MIN B PLG 6.56'
Assmann WSW Components
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.