Private LTE Based on CBRS

Digi's 3.5 GHz band is a dependable alternative to Wi-Fi and public networks

Image of Digi's Private LTE Based on CBRSDigi's private LTE networks are based on the same protocols as public networks. Small cells that are on site are operated by a managed service provider, the owner, or an enterprise customer. This is typically at a lower cost than a public network and has better reliability and performance. This network can reach through building walls and other obstacles that can potentially block a Wi-Fi signal. It occupies 150 MHz in the 3.5 GHz C-band, or Band 48. Traditionally, this band was only used for US military and fixed satellites. Digi is a member of the CBRS Alliance, which is a non-profit organization that develops and promotes CBRS technology.

A major benefit of using private LTE is that it is a secure, exclusive network in an uncrowded spectrum. This is important for highly-regulated industries such as finance and healthcare. The SIM-level device security ensures that devices have a unique identifier and are properly authenticated, allowing network administrators tight control of what devices are on the network. Another key benefit is the quality of service. Typically, cellular technology provides a better quality of connection than Wi-Fi. It gives the network administrator control of how data traffic is prioritized. Using the small cells, there is no connection loss with private LTE as there can be with Wi-Fi. Enterprise customers will have lower data transfer costs with private versus public LTE. This is important when there are high data volumes.

Features
  • Private
  • Secure
  • Flexible
  • Resilient
  • Lower cost
Applications
  • Mine sites
  • Seaports
  • Hospitals
  • College and corporate campuses
  • Factories

Private LTE Based on CBRS

תמונהמק"ט יצרןתיאורכמות זמינהמחירהצגת הפרטים
NETWORKING WR64 ACCESSORY KIT76002069NETWORKING WR64 ACCESSORY KITמיידית - 0See Page for Pricingהצגת הפרטים
NETWORKING WR64 POWER SUPPLY76002076NETWORKING WR64 POWER SUPPLYמיידית - 0See Page for Pricingהצגת הפרטים
WR54 ACCESSORY KIT - SINGLE LTE76002084WR54 ACCESSORY KIT - SINGLE LTEמיידית - 0$1,708.53הצגת הפרטים
WR54 ACCESSORY KIT - DUAL LTE76002085WR54 ACCESSORY KIT - DUAL LTEמיידית - 0$2,013.51הצגת הפרטים
TX64-A141 ACCESSORY KIT76002087TX64-A141 ACCESSORY KITמיידית - 0$5,194.46הצגת הפרטים
ROUTER, LTE, WI-FI, WORLDWIDETX54-A106ROUTER, LTE, WI-FI, WORLDWIDEמיידית - 3$4,292.68הצגת הפרטים
ROUTER LTE DUAL WI-FI, WORLDWIDETX54-A112ROUTER LTE DUAL WI-FI, WORLDWIDEמיידית - 1$5,473.20הצגת הפרטים
ROUTER LTE, WI-FI, NA, FIRSTNETTX54-A146ROUTER LTE, WI-FI, NA, FIRSTNETמיידית - 1$5,374.85הצגת הפרטים
ROUTER DUAL LTE, WI-FI WORLDWIDETX54-A206ROUTER DUAL LTE, WI-FI WORLDWIDEמיידית - 0$5,637.20הצגת הפרטים
RTR DUAL LTE WI-FI NA FIRSTNETTX54-A246RTR DUAL LTE WI-FI NA FIRSTNETמיידית - 8$7,112.90הצגת הפרטים
DUAL CAT18 1ST NET DUAL WIFI GBLTX64-A141DUAL CAT18 1ST NET DUAL WIFI GBLמיידית - 15$10,496.02הצגת הפרטים
2020-05-19 תאריך הפרסום