Graphene at DigiKey
Kennedy Labs is an excellent source for graphene, other 2D materials, and more
DigiKey is partnering with Kennedy Labs to offer graphene and other two dimensional (2D) materials to academic, industrial, and research customers looking to harness these disruptive technologies and deliver new functionality, miniaturization, gain efficiency, and lower cost in new product designs and systems.
Kennedy Labs is a manufacturer of 2D materials, heterostructures, and products enhanced by them, such as conductive inks, pastes, epoxies, and lubricants. Through their partnership, Kennedy Labs and DigiKey bring mono, bi, and tri layer CVD graphene films on copper, silicon, quartz, flexible plastic, and suspended on grids, along with various kinds and grades of graphene powders such as graphene oxide (GO), reduced graphene oxide (rGO), and graphene nanoplatelets (GnPs) to the market. Gallium oxide on sapphire and graphene on hexagonal boron nitride (hBN) on silicon substrates are available now and new 2D materials are being added as they become available.
2-D Basics: Materials for Designing the Future
In their simplest form, 2D materials are single atom layers of a particular material. Graphene, a single atomic layer of graphite, was the first such 2D to be discovered, but many other 2D materials have been discovered since then. Because of their atomic sizes, 2D materials possess amazing properties that their bulk forms do not, and they will help to usher in a new age of cutting-edge performance and miniaturization benefits to microelectronics. For example, graphene is the thinnest and lightest material known with incredible strength coming in around 300 times stronger than steel. It is also the best man-made thermal conductor and has a conductive density 1,000,000 times greater than copper.
Kennedy Labs' partnership with DigiKey has allowed them to bring the highest quality graphene development products in a range of sizes, substrates, and forms to the market. With readymade graphene on different substrates such as copper, quartz, poly, and silicon, designers can jump right in to the world of 2D material development. Kennedy Labs also offers graphene in other forms and compounds as well. For example, graphene infused ink, thermal grease, powder, thermal spreading substrates, and pastes for user enjoyment and thermal experimentation. Stay tuned for more to come from Kennedy Labs.
Kennedy Labs' Graphene and 2D Design Challenge
In order to stimulate design discussion and collaboration, Kennedy Labs invites anyone to participate in their Graphene and 2D Design Challenge. Applicants are immediately eligible for product discounts, direct factory support and/or custom development.
To enter the Kennedy Labs' Graphene and 2D Design Challenge:
- Download and complete the form
- Email form as attachment to 2DMaterials@digikey.com
- DigiKey and Kennedy Labs will review each submission carefully
Graphene
| תמונה | מק"ט יצרן | תיאור | כמות זמינה | מחיר | הצגת הפרטים | |
|---|---|---|---|---|---|---|
![]() | ![]() | KL2G-1010-SIO2/SI | 2 LAYER GRAPHENE 10MM2 SIO2 SUB | מיידית - 4 | $488.62 | הצגת הפרטים |
![]() | ![]() | KLG-RGO-1G | REDUCED GRAPHENE OXIDE POWDER | מיידית - 0 | $816.55 | הצגת הפרטים |
![]() | ![]() | KLG-1010-18CU | MONO LYR CVD GRAPHENE X4 ON CU | מיידית - 0 | $226.27 | הצגת הפרטים |
![]() | ![]() | KLG-1010-18CU+PMMA | CVD GRAPHENE X4 ON CU PMMA | מיידית - 0 | $249.23 | הצגת הפרטים |
![]() | ![]() | KLG-100100-18CU | MONO CVD GRAPHENE ON CU 4" X1PCS | מיידית - 0 | $1,308.45 | הצגת הפרטים |
![]() | ![]() | KLG-100100-18CU+PMMA | CVD GRAPHENE ON CU 4" PMMA X1 | מיידית - 3 | $1,367.48 | הצגת הפרטים |
![]() | KLG-1010-SIO2/SI | CVD GRAPHENE ON SIO2/SI X 4PCS | מיידית - 6 | $718.17 | הצגת הפרטים | |
![]() | ![]() | KLG-1010-18Q | CVD GRAPHENE ON QUARTZ X 4PCS | מיידית - 0 | $816.55 | הצגת הפרטים |
![]() | KLG-1010-175PET | CVD GRAPHENE ON PET SUB X 4PCS | מיידית - 4 | $705.06 | הצגת הפרטים | |
![]() | ![]() | KLG-1010-POLY | CVD GRAPHENE ON POLY SUB X1 PCS | מיידית - 3 | $405.82 | הצגת הפרטים |
![]() | ![]() | KL3G-1010-SIO2/SI | 3 LAYER CVD GRAPHENE SIO2/SI SUB | מיידית - 6 | $816.55 | הצגת הפרטים |
![]() | ![]() | KLG-2UM-3MMTEMAUGRID | SUSPENDED MONOLAYER GRAPHENE | מיידית - 10 | $980.52 | הצגת הפרטים |
![]() | KLG-SKIT | GRAPHENE DISCOVERY KIT 10X10 MM | מיידית - 14 | $1,636.39 | הצגת הפרטים | |
![]() | KLG-AKIT | GRAPHENE DISCOVERY KIT 1 WAFER | מיידית - 6 | $2,772.54 | הצגת הפרטים | |
![]() | ![]() | KLG-RGO-200MG | REDUCED GRAPHENE OXIDE 200MG | מיידית - 8 | $324.65 | הצגת הפרטים |
![]() | KLG-RGO-C-500MG | REDUCED GRAPHENE OXIDE 500MG | מיידית - 2 | $488.62 | הצגת הפרטים | |
![]() | ![]() | KLG-GOFD-1 | DRY GRAPHENE OXIDE PASTE 200MG | מיידית - 0 | $512.40 | הצגת הפרטים |
![]() | ![]() | KLG-GOPO-8 | GRAPHENE OXIDE POWDER, 1000 MG J | מיידית - 0 | $368.92 | הצגת הפרטים |
![]() | ![]() | KLG-GOPA-2 | GRAPHENE OXIDE PASTE - 50% GO, 5 | מיידית - 1 | $819.83 | הצגת הפרטים |
![]() | ![]() | KLG-GOPA-4 | GRAPHENE OXIDE PASTE, 10% GO, 5 | מיידית - 5 | $819.83 | הצגת הפרטים |