CODEGRIP Remote Programming and Debugging Solution
MikroElektronika’s remote programming and debugging solution allows multiple developers to access and work simultaneously from separate devices
MikroElektronika's CODEGRIP is a complete solution designed for remote programming and debugging of various microcontroller devices (MCUs) that use the Arm® Cortex®-M architecture through a Wi-Fi connection. It effectively bridges the differences among numerous MCUs across different vendors, enabling the programming and debugging of an extended array of MCUs. CODEGRIP's unique attributes, such as its wireless capabilities and USB-C connectivity, simplify the programming and debugging of numerous Arm Cortex-M-based microcontrollers, making the process smooth and user-friendly. The USB-C connector provides enhanced performance and reliability over the traditional USB Type A/B connectors. Additionally, the wireless feature transforms how the development board is used, offering a new level of convenience and flexibility in development tasks.
The latest update for the CODEGRIP programmer brings significant enhancements to the development experience. Wi-Fi programming speeds have increased by over 50%, improving operations such as target connection, chip sector/mass erase, as well as flash writing and verification. This boost makes programming quicker and more efficient than ever before. Additionally, staying current with industry standards, MikroElektronika offers expanded support to include 272 MCUs from STMicroelectronics and Microchip. These updates ensure that developers have the tools they need to stay innovative and competitive in a rapidly evolving tech landscape.
Features
- Remote debugging feature
- Multiple developers can access and work simultaneously from separate devices
- Easily connect IoT devices, helping simplify processes and accelerate time to market
CODEGRIP Updates - Click to Enlarge
CODEGRIP Remote Programming and Debugging Solutions
| תמונה | מק"ט יצרן | תיאור | כמות זמינה | מחיר | הצגת הפרטים | |
|---|---|---|---|---|---|---|
![]() | ![]() | MIKROE-3460 | WI-FI WIRELESS CODEGRIP ARM | מיידית - 31 | $980.52 | הצגת הפרטים |
![]() | ![]() | MIKROE-3461 | WI-FI WIRELESS CODEGRIP STM32 | מיידית - 1 | $750.97 | הצגת הפרטים |
![]() | ![]() | MIKROE-4544 | CODEGRIP FOR PIC | מיידית - 1 | $750.97 | הצגת הפרטים |
![]() | ![]() | MIKROE-5162 | UNI CODEGRIP | מיידית - 1 | $1,800.35 | הצגת הפרטים |