Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
PSA101-Slide13

There are three factors that can influence pressure sensitive adhesive performance and the designer’s choices. The first is the surface in which the adhesive is bonded to. For optimal bond formation, the pressure sensitive adhesive must flow into the minute valleys of the substrate. This requires matching the surface energy of the adhesive to the substrate.

PTM פורסם ב: