Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
heat-pipe-slide13

The wick is necessary to return the liquid from the condenser to the evaporator. Wick types can be homogeneous or composite. Homogeneous wicks are constructed of one type of material or machining technique. ATS offers cost effective sintered copper powder and axial groove. Sintered wicks have the added advantage of being able to handle high heat fluxes and deployment in any orientation.

PTM פורסם ב:
PTM Updated on: 2016-02-05