Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List Associated Content
Thermal Interface Materials (TIMs)

Thermal interface materials (TIMs) enhance the thermal conductivity of heat sinks by reducing the thermal resistance between the component and the heat sink. TIMs fill in the air gaps that are left between the surface of the heat sink and the device, which act as insulators preventing heat from being conducted into the base of the heat sink. Common thermal interface materials include Gap Pads, Thermal Grease, Thermal Tape, and Phase-Change Materials.

PTM פורסם ב: