Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
Image of Advantech AIW-166K Series of Wireless Kits - What Does it Provide

Wi-Fi 6E is an extension of the Wi-Fi 6 (802.11ax) standard that adds support for the 6GHz band, in addition to the 2.4GHz and 5GHz bands. Some benefits of the Wi-Fi 6E include increased capacity: Wi-Fi 6E adds more available channels, which increases the capacity of the network and reduces congestion, improved performance: with more available channels, Wi-Fi 6E can provide faster data transfer speeds and lower latency, which is especially beneficial for high-bandwidth applications such as streaming video and online gaming, increased reliability: The 6GHz band is less crowded than the 2.4GHz and 5GHz bands, which means that Wi-Fi 6E networks are less likely to experience interference from other wireless devices, better security: Wi-Fi 6E includes built-in security features such as WPA3 encryption, which can help protect the network from unauthorized access and finally improved battery life: Wi-Fi 6E is designed to be more power-efficient than previous versions, which can help extend the battery life of mobile devices. Overall, Wi-Fi 6E results in a more reliable and faster wireless experience.

PTM פורסם ב: