Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Wastewater Process Monitoring

For wastewater process monitoring, many sensors such as temperature, flow rate, and PH sensors are used to monitor the water quality. The ESRP-PCS-ADAM6717 measures the sensor signals through its onboard I/O and collects data from pumps and meters via Modbus. The data is then converted and pushed to the cloud. The IEC-61131-3 Softlogic is also supported by the ADAM module, so users can use the PLC programming languages such as ladder and function blocks to manage logic control.

PTM פורסם ב: