Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
Image of Advantech WISE-750 Vibration AI Gateway - Application Sensors

There are three monitoring modes in WISE-750-02A1E. In the machine learning mode, users can leverage the Renesas machine learning IC and monitor machine condition based on AI algorithms. In the feature extraction mode, users can set alarm criteria based on the feature value. For example, users can follow the guideline of ISO 10816-3 which is one of the standards for evaluating the machine heath-based on RMS value. Lastly, in the datalogger mode, if the customer wants to build their own PHM algorithm the WISE-750-02A1E can also export the raw data and feature values for further analysis.

PTM פורסם ב: