Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
Image of Allegro Microsystems Magnetic High-Current Sensors - Hall Coreless Frictionless Design Busbar

Like the core-based current sensors, the customer can get help for the design of the coreless-based current sensors. Allegro has released a busbar tool as the one on the left. In this web application, the customer can then calculate the coupling factor of a busbar with the ACS37612 current sensor using a 3D magnetic model. Depending on the inputs, the tool will give the customer the maximum measurable current (up to 50kA), the busbar sensitivity (up to 4.3mV/A), the coupling factor (up to 850mG/A), the current density (up to 166.88A/mm2) and the effective airgap (up to 2.66mm). There is also a view app note button on this site to understand how to design a busbar for the ACS37612.

PTM פורסם ב: