Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
Surveillance-Slide7

A brand new field that Intel® is working in with a partner named Sensity is on-chip FPGA real-time video analytics. The raw processing power of the FPGA provides a unique platform on which to implement almost any analytical function for processing and monitoring video streams in a surveillance application. This type of IP function can be used in machine vision or intelligent surveillance/security applications. These algorithms could be incorporated into the DVR or camera side of the network as well. Triggers from these real-time analyzed events could be used to increase or decrease network bandwidth, control DVR recording events or enhance camera sensitivity/resolution or frame rates.

PTM פורסם ב: