Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
Image of American Hakko FX100-04 RF Induction Heat Soldering Station - Conversion

Hakko’s FX1001-51 handpiece is powered by RF heating and is compatible with other RF induction heat soldering stations. There is no calibration required or system settings needed. The kit includes the handpiece, iron holder with the traditional cleaning sponge, and brass coils. Also included are two extra grips and a heat pad which protects the operator when removing the tips.

PTM פורסם ב:
PTM Updated on: 2022-01-10