Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
FX-951 Soldering Station Slide 4

The temperature setting is done by using the up, down and asterisk buttons on the face of the unit. After inserting the control card, the hundreds digit will flash indicating that a temperature can be entered. After the hundreds has been entered, the tens digit can be entered and then the units digit thereafter following the same steps. When the desired temperature is displayed, press the asterisk button to enter. Once all the temperatures are set, the heater control will begin.

PTM פורסם ב: