Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
Battery-Slide9

In summary, an Ametherm thermistor is required with following ratings: 5.0 Ohms at 25ºC and 250 Joules. AS32 5R020 (5 Ohms at 25ºC, 300 Joules, 20A max steady state current) would be suitable. Please note: Steady state current is not calculated because in this example, the current goes through the contactor.

PTM פורסם ב: