Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Inrush-Slide12 five six

In summary, Ametherm’s Inrush Current Limiters are used to reduce the inrush current that occurs when an electrical device is switched on. High inrush current is the result of the maximum instantaneous input current drawn by an electrical device during the initial power up. As technology continues to advance, most systems run efficiently and maintain a low impedance which in turn contributes to high inrush current. Additionally, devices that require alternating current such as electric motors or transformers can draw several times their steady state current at switch on. Although this additional draw of inrush often lasts less than ½ of a normal 60Hz cycle, that is enough time to cause possible damage to the equipment. Check out Ametherm’s Website for more information.

PTM פורסם ב: