Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
NTC-Slide16

The next factor to consider is whether the application needs to be curve matched or point matched. This will allow for the calculation of the needed nominal resistance value at a given temperature. Ametherm offers an entire range of nominal resistance values for the NTC Thermistors. The standard reference temperature is 25°C, but buyers and designers can request different temperatures. A word of caution: if the desired resistance is not available in the combination of product type and material component, then a decision must be made as to which characteristic takes priority: product type/size, material preference or resistance ratio.

PTM פורסם ב: