Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
LM2594-slide4

Shown on this slide is the typical schematic diagram for a 5V fixed output buck converter, using the LM2597 switching regulator. The additional supervisory features, such as shutdown/soft-start, can be seen. Note the inductor value of 100 microhenries is the same value used in the preceding LM2494 5.0V example.

PTM פורסם ב: