Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List Associated Content
Air Quality Engineering Development Kit

Telaire offers an air quality development kit for both the SM-UART-04L PM2.5 laser dust sensor and the SM-PWM-01C dust sensor. The SM-UART-04L is served by the Telaire AAS-LDS-UNO. This evaluation kit also works with the Telaire T9602 temperature and humidity sensor, T6713 CO2 sensor module, and other sensors from Amphenol. The SM-PWM-01C is served by the Telaire AAS-AQS-UNO. This evaluation kit also works with the Telaire T9602 temperature and humidity sensor and the Telaire T6713 CO2 sensor module. They are both based on an Arduino development platform with open-source code. Sample codes are available on www.github.com.

PTM פורסם ב: