Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
Choosing the Right Sensor

Selecting the right sensor depends on the application. If the monitored environment experiences periodic exposure to background CO2 levels, the optimal solution will be a single channel NDIR sensor utilizing ABC Logic™. This sensor will provide in-situ automated re-calibration for the life of the sensor, improving performance and reducing cost of ownership. If the monitored environment is continually occupied or not expected to see diurnal CO2 concentration cycles (such as hospitals, detention facilities, and indoor agricultural structures), a dual channel NDIR is necessary. Without periodic exposure to background CO2 levels, firmware-based statistical algorithms cannot be reliably deployed for drift compensation. While the hardware-based reference inherent in the dual channel NDIR sensors can provide excellent drift compensation, recalibration will eventually be required for these NDIR sensors in order to retain factory performance specifications.

PTM פורסם ב: