Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
chip in glass
Thermometrics’ long standing chip-in-glass technology is a proven leader in reliability and stability within the NTC thermistor industry, providing a 14004 Ω nominal resistance at 37°C and 25/50 Beta of 3500K. The AB thermistor assembly’s performance, coupled with Amphenol Advanced Sensors’ exceptional customer support, has spanned from the first AB assembly shipment in 1974 to over one million AB assembly shipments per year. Each AB thermistor assembly is provided with six feet long, 38 gauge nickel alloy bifilar leads, with a heavy build polyester enamel insulation as standard.
PTM פורסם ב: