Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Product List
Mil-DTL-Slide4

To build an MS coded part number, begin with the MS identifier in position one and enter the shell style into the second slot. The next designation for the desired service class is entered and is followed by the desired shell size.  Slot five designates the insert arrangement which is followed by an entry to select either pin or socket type contacts. Finally, insert the desired insert rotation with W,X,Y, Z or leave this slot blank for normal rotation.

PTM פורסם ב: