Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
HD-BNC-Slide5

The spacing of the HD-BNC™ is a highly compact, dense solution that was meant to meet the growing demands of the broadcast industry. HD-BNC™ can be configured with a centerline spacing of 8mm minimum compared to the BNC at 15.5, and to the 1.0/2.3 DIN at 10mm. This allows for density improvements of 400% over standard BNC. 

PTM פורסם ב: