Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
AS5047 Rotary Position Sensor Slide 4

Like other members of the 47 series, the AS5047P features ams OSRAM's DAEC™ (dynamic angle error compensation) technology, which produces outstanding angle measurement accuracy even at very high rotation speeds. The 47 series magnetic sensors’ high-speed performance and ABI incremental outputs make them ideal as robust replacements for optical encoders. The total system cost of a design based on the 47 series is also typically lower than that of an equivalent optical encoder or resolver. In the AS5047P sensor, the maximum rated measurement speed has been increased from 14,500 rpm to 28,000 rpm, enabling it to support many high speed rotating shaft applications that previously could only be addressed with optical encoders.

PTM פורסם ב: