Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
Instrumentation Amplifier Primer Slide 9

To address the input impedance issue of the difference amplifier, another two op amps are added as input buffers. In addition another three resistors are added. These extra resistors allow the addition of more gain in this pre-amp stage. This allows important parameters like offset, noise, and CMRR to improve with gain.

PTM פורסם ב: