Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
AmplifierProblem-Slide9

The problem is as follows: in order for the part to work correctly, one of the internal nodes needs to pull up to 6V, but the power supply is only 5V. So the internal node will saturate at 4.69V and cannot achieve its 6V desired voltage. The second stage is working correctly, but only sees a difference voltage of 2.96V at its inputs, so its output is 2.96V.

PTM פורסם ב: