Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
TUE-Slide11

Here is a graph depicting actual measured outputs from the DAC. Note how the output may change over temperature. At room temperature the offset is at its worst but there is no real gain error. Looking at the same DAC output at -40°C, the offset error might be fine but there is a gain error component that is at its worst. Finally, after being heated, it may behave with another differring transfer function.

PTM פורסם ב: