Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
HF-Slide9

The HF “52” handle is sealed per IP67 and provides two momentary pushbutton functions in addition to the three proportional axis. The two momentary pushbuttons are protected under an elastomer boot.

PTM פורסם ב: