Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
WSW Components Line of Board-Level Transistor Heat Sink Overview Slide 2

A heat sink is made from metal, typically aluminum alloy that is stamped or extruded into a desired form. Heat sinks are designed to increase the surface area of the device in contact with the cooling medium surrounding it, such as the air. In electronic systems, a heat sink is a passive heat exchanger component that cools a device by absorbing excess heat from an electronic component and dissipating it into the surrounding air.

PTM פורסם ב: