Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
picoPower-Slide3

The power budget, shown in the figure above, uses the duty cycle between active and sleep mode to show the average current consumption of an application. The average current consumption enables determination of battery life-time calculations as well as other power supply considerations. This budget will indicate whether active or sleep power consumption is the most critical for a given application. In most low power applications, the power budget points to sleep power consumption as the most critical parameter.

PTM פורסם ב: