Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Studio Development Environment Overview Part 1 Slide 14

Another interesting addition to the latest Atmel Studio 6 is the terminal window, which is an integrated extension installed by default. There is more information about the Atmel Studio extension manager in a separate Product Training Module here at Digikey. The Terminal Window opens a channel through the computer’s serial port, and connects to the target using a simple serial port or USB-to-serial adapter. It also lets the user save the communication in a file, as documentation of board test run, and calibration data generated by the target microcontroller.

PTM פורסם ב: