Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
AltEnergy-Slide6

AVX offers capacitors based on a new material system that is ideal in the output of DC/DC converters, regulators, or power supplies. Oxicaps are a niobium based capacitor that is electrically more efficient than small aluminum Electrolytics. OxiCaps are smaller, lighter, noise free, and can replace a larger aluminum electrolytic (because of their low inductance and ESR). These devices will also not burn when operated up to their category voltage.

PTM פורסם ב: