Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List

VCAS-Slide9

Another example of a very common application is on interfaces such as CAN bus. This particular schematic shows a CAN bus and highlights the additional auto grade devices AVX offers (AEC-Q200 qualified MLCC capacitors and Niobium Oxide capacitors). It should be noted that proper selection of the MLV may allow additional components to be eliminated on the design (see C2, C3 etc).

PTM פורסם ב: